Skip to main content
SEEED STUDIO · PAPER DEEP-DIVE

GR00T N1: How a Dual-System Architecture Supports Generalist Humanoid Control

GR00T N1: An Open Foundation Model for Generalist Humanoid Robots

  • Humanoid robots
  • Dual-system architecture
  • Data pyramid
  • Flow matching
arXivRead the paper

GR00T N1.7: Adaptation and Fine-Tuning​

This reading covers the original GR00T N1 paper. For hands-on work with GR00T N1.7 (nvidia/GR00T-N1.7-3B), follow the existing reBot course:

The N1 experimental settings discussed below belong to the original paper. Use the N1.7 tutorials for version-specific training and deployment configuration.

Prerequisites​

From ACT to GR00T N1: The Learning Loop Is the Same​

If you have used LeRobot + ACT, this workflow is familiar:

Human teleoperation
↓
Collect camera / state / action data
↓
Organize an episode dataset
↓
Train a policy
↓
Observation → Action chunk → On-robot execution

GR00T N1 still answers the same question:

Given what the robot sees, its current state, and the user's request, how should it move next?

ACT typically learns one robot and a task family from demonstrations. GR00T N1 seeks general priors from multiple robots, human videos, and synthetic data before adapting to a particular real robot.

GR00T N1 Paper Deep-Dive: 1.1 From ACT to GR00T N1: The Learning Loop Is the Same (image-11)

ACT starts with one concrete skill; GR00T N1 first learns a foundation across bodies and tasks, then learns to use the current robot.

Observation, State, Action, and Embodiment​

The three terms introduced with ACT retain their meaning:

  • Observation: external sensor information, such as head, wrist, and multi-view RGB images.

  • State: the robot's configuration, including joint angles, gripper opening, end-effector pose, waist, or neck state.

  • Action: requested controls, potentially joint targets, increments, end-effector poses, or gripper commands.

Embodiment includes more than appearance. It combines body and control definitions:

Robot structure
+ Sensors
+ State definition
+ Action definition
+ Control frequency and mode
= One embodiment

A single Franka, a bimanual system, and a GR-1 humanoid have different state/action dimensions. Sharing a model across these bodies is a central challenge.

VLA, Action Chunking, and Flow Matching​

GR00T N1 Paper Deep-Dive: 1.3 VLA, Action Chunking, and Flow Matching (image-09)

A VLA adds task language to visual policy inputs. Language identifies which object to manipulate, where it should go, and whether behavior matches the request; it is not decorative context.

An action chunk, as in ACT, predicts a short future sequence rather than one action. GR00T N1 sets H = 16.

Flow matching can be understood as refining random actions into an executable chunk under image, language, and state conditioning. The paper uses only K = 4 inference updates.


Abstract​

General-purpose robots need capable bodies and intelligent models. Humanoids are promising for human environments, but understanding new situations, handling real-world variation, and quickly learning new tasks require foundation models trained on large, diverse data.

GR00T N1 is an open foundation model for humanoids with a dual-system VLA architecture. A vision-language module, System 2, interprets images and instructions; a diffusion Transformer, System 1, generates smooth actions in real time. The modules are closely connected and jointly trained end to end.

Training mixes real trajectories, human videos, and synthetic data. GR00T N1 exceeds the compared imitation-learning baselines on simulation benchmarks across embodiments and learns language-conditioned bimanual tasks efficiently on the Fourier GR-1 humanoid.

Three ideas organize the paper:

  1. Dual-system VLA: one component interprets, another acts.

  2. Heterogeneous data: use human videos, simulation, and generated videos alongside robot demonstrations.

  3. Cross-embodiment sharing: different bodies share core capabilities instead of receiving entirely independent models.


Hardware, Models, Data, and Data Islands​

The introduction identifies three necessary elements:

  • Hardware determines physical capability. Humanoids are appealing because human environments are designed for human bodies.

  • Models must handle open-ended tasks, not one fixed behavior.

  • Data determines exposure to environments, objects, tasks, and bodies.

Language and vision models can learn from the internet, but robotics lacks an equivalent internet of actions. Real data is costly and slow to collect, and robots differ in joints, sensors, and controls.

Putting datasets together can still leave data islands: files share a database but not semantics or action spaces.

The paper therefore asks not only how to design a policy but also how to unify its training corpus.

The Data Pyramid​

GR00T N1 Paper Deep-Dive: 3.2 The Data Pyramid (image-12)

LevelDataRelative quantityRelationship to the robot
BottomWeb data + human videosLargestRich action concepts without direct robot commands.
MiddleSimulation + neural trajectoriesLargeScalable and controllable, but with simulation or generation bias.
TopReal-world robot dataSmallestClosest to execution, most expensive to collect.

Moving upward reduces quantity but increases specificity to the target embodiment.

Human videos: which actions and tasks exist Simulation / generation: how those tasks can vary Real robot data: how this body should execute them


GR00T N1 Architecture​

System 2 Understands; System 1 Acts​

GR00T N1 Paper Deep-Dive: 4.1 System 2 Understands; System 1 Acts (image-17)

The architecture borrows a dual-system analogy from cognition:

  • System 2: Eagle-2 VLM, interpreting images, language, and tasks.

  • System 1: diffusion Transformer (DiT), generating continuous actions quickly.

These are not independent programs: cross-attention connects them tightly and training optimizes them jointly.

Eagle-2 contains a language model and image encoder. Images enter at 224 × 224, producing 64 tokens per frame. The authors use intermediate layer-12 VLM features rather than final features, improving speed and downstream success in their experiments.

System 2 operates at about 10 Hz on an NVIDIA L40, while the action system can output closed-loop controls at a higher rate. High-level interpretation need not be recomputed every millisecond, while motion must remain continuous.

Connecting Different Robots to One DiT​

GR00T N1 Paper Deep-Dive: 4.2 Connecting Different Robots to One DiT (image-13)

There are two kinds of modules:

  • Shared core: VLM and DiT share visual, language, and behavioral knowledge across robots.

  • Embodiment-specific interfaces: state encoder, action encoder, and action decoder translate platform dimensions and control semantics to and from shared features.

ModuleFunctionWhy embodiment-specific?
State encoderEncode current state as tokens.State fields and dimensions differ.
Action encoderEncode noisy actions and generation time.Action dimensions differ.
Action decoderConvert DiT features into controls.Joint, end-effector, and gripper control modes differ.

Commentary: Cross-robot learning is not just zero-padding vectors to equal length. Equal dimensions are meaningless without knowing which joint, pose, or command each value represents.

Flow-Matching Action Chunks​

At time t, predict a sequence rather than one action:

A_t = [a_t, a_(t+1), ..., a_(t+H-1)]
H = 16

Training starts with real chunk A_t, Gaussian noise ε, and flow time τ, constructing:

A_t^τ = τ A_t + (1 - τ) ε
  • Near τ=0, the chunk resembles noise.

  • Near τ=1, it resembles real actions.

The DiT reads visual-language features, state features, and noisy actions to learn an update direction. The paper writes the loss as:

L_fm(θ)
= E_τ [ || V_θ(φ_t, A_t^τ, q_t) - (ε - A_t) ||² ]

Here φ_t denotes VLM features and q_t robot-state features.

Inference has no real future action, so it begins from noise and performs four forward-Euler updates:

A_t^0 ~ N(0, I)

A_t^(τ+1/K)
= A_t^τ + (1/K) V_θ(φ_t, A_t^τ, q_t)

K = 4

GR00T-N1-2B has 2.2B total parameters, including about 1.34B in the VLM. On L40, generating a 16-step chunk takes about 63.9 ms.


Data and Training​

Using Videos without Robot Actions​

Robot trajectories directly supervise images, states, and actions. Human and generated videos contain images but no robot joint commands.

GR00T N1 adds action-like supervision in two ways.

Latent actions learn discrete behavioral codes from visual changes, rather than exact joint angles: concepts like moving left, grasping, or pushing.

GR00T N1 Paper Deep-Dive: 5.1 Using Videos without Robot Actions (image-01)

These can span embodiments: human hands and robot grippers have different joints but can both move an object left in the image.

An inverse dynamics model (IDM) infers actions between observations:

Observation_t + Observation_(t+1)
↓
IDM
↓
Pseudo Action Label

Latent actions resemble unitless behavioral vocabulary; IDM outputs resemble pseudo-action labels. Neither makes videos perfect physical demonstrations. They make image-only data usable for pre-training.

Neural Trajectories and Simulation: More Variation from Fewer Demonstrations​

Video generation starts from real robot images and varies language prompts to synthesize tasks, object positions, and trajectories. These are neural trajectories.

GR00T N1 Paper Deep-Dive: 5.2 Neural Trajectories and Simulation: More Variation from Fewer Demonstrations (image-00)

The authors expand 88.4 hours of internal teleoperation into 827.3 hours of generated video, nearly tenfold. Generation can move objects impossibly, distort contacts, or deform the robot, so language-model and rule-based filters remove low-quality samples before latent actions or IDM provide supervision.

GR00T N1 Paper Deep-Dive: 5.2 Neural Trajectories and Simulation: More Variation from Fewer Demonstrations (image-08)

Simulation instead executes in a physics engine. Methods such as DexMimicGen retarget object-centric demonstrations to new scenes, producing about 780,000 simulated trajectories, roughly 6,500 hours.

Difference:

  • Neural trajectories provide visual and semantic variation but limited physical reliability.

  • Simulation provides exact actions and physics interactions but retains a sim-to-real gap.

Pre-Training and Post-Training​

Teleoperation data comes from Manus, VIVE, Apple Vision Pro, Leap Motion, and other devices, retargeted to the robots.

GR00T N1 Paper Deep-Dive: 5.3 Pre-Training and Post-Training (image-05)

GR00T N1 Paper Deep-Dive: 5.3 Pre-Training and Post-Training (image-15)

Post-training is neither training from scratch nor immediate zero-shot control of arbitrary robots. It adapts the foundation to a target camera setup, state, action interface, and task.

SettingPre-trainingPost-training
Batch size16,384128 or 1,024
Gradient Steps200,00020,000-60,000
Main dataMultiple embodimentsOne embodiment / task
PurposeGeneral priorsAdaptation to a specific body and task

GR00T-N1-2B pre-training uses about 50,000 H100 GPU hours. The dataset totals 8,375.7 hours and 592.9M frames.

One-sentence view: Pre-training supplies broad experience of worlds and bodies; post-training teaches the model to use this particular robot.


Experiments and Results​

How Is Effectiveness Tested?​

Simulation and physical tests examine pre-training priors and adaptation with limited data, rather than only fitting training tasks.

GR00T N1 Paper Deep-Dive: 6.1 How Is Effectiveness Tested? (image-10)

Simulation benchmarks include:

  • RoboCasa Kitchen: 24 kitchen tasks.

  • DexMimicGen Cross-Embodiment Suite: nine cross-robot manipulation tasks.

  • GR-1 Tabletop: 24 humanoid tabletop tasks.

Real GR-1 tests include pick-and-place, articulated objects, industrial manipulation, and multi-robot cooperation.

GR00T N1 Paper Deep-Dive: 6.1 How Is Effectiveness Tested? (image-03)

Main comparisons are BC-Transformer and Diffusion Policy. GR00T N1 differs not just in size and architecture but in heterogeneous cross-embodiment pre-training, so results reflect data and training as well.

Do Priors Help with Little Data?​

Simulation post-training uses 30, 100, or 300 demonstrations per task. Main trends are:

  • Priors help most when task data is scarce.

  • With more data, a dedicated Diffusion Policy narrows the gap, but GR00T N1 retains strong data efficiency.

  • In some settings, about 10% of task data approaches Diffusion Policy trained with all data.

GR00T N1 Paper Deep-Dive: 6.2 Do Priors Help with Little Data? (image-16)

The practical implication is:

A foundation model's value is not needing no data; it is learning effectively from a pre-trained starting point when your data is limited.

Do Neural Trajectories Improve Real Behavior?​

Ablations compare real data alone, generated videos labeled with latent actions, and generated videos with IDM pseudo-actions.

GR00T N1 Paper Deep-Dive: 6.3 Do Neural Trajectories Improve Real Behavior? (image-02)

Synthetic trajectories improve some tasks, with IDM often connecting more directly to real action spaces than latent codes. More generation is not automatically better: physical errors and pseudo-label bias enter training too.

The authors also observe spontaneous left-to-right handovers in a pre-trained model that can disappear after narrow task post-training.

GR00T N1 Paper Deep-Dive: 6.3 Do Neural Trajectories Improve Real Behavior? (image-04)

This illustrates catastrophic forgetting: focused fine-tuning can raise a target score while overwriting broader pre-trained capabilities.


Limitations, Practical Implications, and Summary​

What Remains Unsolved?​

  • Mostly short tabletop tasks. Long-duration navigation, whole-body motion, and joint planning remain future work.

  • Limited spatial reasoning. Recognizing an object does not imply precise 3D, contact, or force understanding.

  • Synthetic physical inconsistencies. Plausible-looking video does not ensure executable motion.

  • Forgetting during post-training. Adaptation should be evaluated for generalization retention as well as target success.

Connecting to LeRobot Practice​

The engineering appendix extends the LeRobot dataset format. Storing numbers is insufficient; their meanings must be defined.

ContentInformation to specify
VideoCamera names, views, resolution, frame rate, and time alignment.
StateThe joint or pose represented by each dimension.
ActionAbsolute or incremental targets; joint or end-effector controls.
LanguageInstructions associated with each episode.
RotationRotation matrix, Euler angles, quaternion, or 6D representation.

modality.json adds these semantics, addressing whether the model understands the seventh number, not just whether it can open the file.

For readers with ACT datasets, the additional considerations are:

StageACT practiceAdditional foundation-VLA considerations
CollectionAlign cameras, state, and actions.Stable language annotations.
DataConsistency within one robot.Semantic consistency across embodiments.
TrainingLearn a policy from demonstrations.Post-train a foundation checkpoint.
InferenceImage + state → action chunkImage + language + state → action chunk
EvaluationOn-robot successSuccess, generalization, and retention of pre-trained capabilities
Loading Comments...