Skip to main content
Stage 3 · Chapter 10 · Theory

10. LeRobot and reBot Arm System Architecture

Chapter 10 of the Seeed Physical AI Beginner's Course — what LeRobot is, leader/follower arm division of labor, the Robot and Teleoperator plugin architecture, the camera/CAN/arm data flow, and DM vs RS configuration differences.

10.1 What Is LeRobot and Why Do We Need It?​

Motivation

10.1 What Is LeRobot and Why Do We Need It?

In Chapter 9 we established the conceptual framework of imitation learning: demonstration, data, model, closed loop. But to actually run this pipeline, you immediately encounter a host of trivial yet specific problems:

  • How to align timestamps between camera frames and joint angles?
  • What format should be used to store images, states, and actions for dozens of Episodes?
  • How to share and download trained models on Hugging Face Hub?
  • How can the three codebases — data collection, training, and inference — share the same arm control logic?
Reinventing the wheel

If everyone reinvented the wheel, robot learning would remain a game for only a few labs. LeRobot is the open-source framework Hugging Face built to solve this — it implements proven imitation learning algorithms (ACT, smolVLA, GR00T, etc.) in PyTorch, defines a standard robot dataset format, and provides a complete command-line toolchain from teleoperation and data collection to training and real-robot deployment.

10.2 Leader Arm and Follower Arm​

Arms

10.2 Leader Arm and Follower Arm

  • The first step of imitation learning is "human demonstrates to the robot." The question is: how does a human "teach" a 750 mm-reach arm to do precise grasping motions? Physically guiding it by hand is both dangerous and produces non-smooth data.
  • The answer is master-slave teleoperation: use a structurally similar, lightweight, flexible demonstration arm as the "input device" — the human moves the leader, and the follower follows in real time.
Leader arm and follower arm
  • Leader Arm (leader / teaching arm): the arm the human holds and moves. It only reads positions — it reads its own joint angles in real time and sends them to the computer. It doesn't need to output force, so it can use a lightweight, low-cost servo solution.
  • Follower Arm (follower / execution arm): the arm that actually does the work. It receives joint angles from the Leader and drives its high-power joint motors to follow, completing the actual grasping.

This is like the relationship between the control stick in a crane cab and the crane arm itself. The operator moves the lightweight stick (Leader), while the heavy lifting is done by the arm outside (Follower). Every movement of the stick is real-time "translated" into movements of the crane arm.

10.3 Plugin Architecture​

Plugins

10.3 Plugin Architecture: Robot Plugin and Teleoperator Plugin

LeRobot's first design principle: the framework doesn't know any specific hardware; it only defines interfaces. Hardware connects as plugins.

Robot PluginTeleoperator Plugin
RoleExecutor: receives actions, reports stateInput: only reads human motion intent
Data DirectionBidirectional (read + write)Unidirectional (read-only)
Core Methodsget_observation(), send_action()get_action()
In the reBot systemB601 Follower slave armreBot 102 Leader master arm

One-sentence distinction: The Robot handles "doing," the Teleoperator handles "reading."

Plugin architecture

10.4 Data Flow Overview: Cameras, CAN, and the Arm​

Data flow

10.4 Data Flow Overview: Cameras, CAN, and the Arm

In one control cycle, what data flows, in what format, through which path? One computer connects three types of peripherals, corresponding to three data paths:

Data flow overview

10.5 Four Workflows: Four Uses of the Same System​

Workflows

10.5 Four Workflows: Four Uses of the Same System

Understanding the hardware and data flow, when you look at the four workflows in later chapters of this stage, you'll find they use the same plugins and same configuration; only the LeRobot tools called differ:

WorkflowLeRobot Tool
Teleoperationlerobot-teleoperate
Data Collectionlerobot-record
Traininglerobot-train
Inference & Deploymentlerobot-record (with a policy) or an inference script
  • Teleoperation and data collection use the same hardware chain — the only difference is whether data is recorded.
  • Inference deployment and data collection are structural mirror images: during collection, actions come from the Leader (human); during inference, actions come from the model (checkpoint). Everything else (camera reading, State feedback, CAN commands, safety limits) is identical. This is the benefit of a plugin architecture — changing the decision-maker doesn't require changing the system.
  • Teleoperation and inference deployment: both have all hardware active and control the arm online; the difference is "who makes decisions" — in teleoperation, the decision-maker is the human; in inference, it's the model.

10.6 DM vs. RS Configuration Differences​

Config

10.6 DM vs. RS Configuration Differences

Comparison ItemB601-DMB601-RS
PC ConnectionDamiao USB2CAN Serial BridgeSocketCAN-compatible USB-CAN Adapter
Device Name/dev/ttyACM* (Serial Bridge)can0 (SocketCAN Network Interface)
--robot.typeseeed_b601_dm_followerseeed_b601_rs_follower
--robot.port/dev/ttyACM0 (depending on actual enumeration)can0 (depending on actual enumeration)
--robot.can_adapterdamiaosocketcan

One sentence summarizing the relationship between the two versions: same skeleton, two sets of "hearts and nerves." The mechanical structure, joint naming, and upper-level software workflows are identical; all differences are in the motors and CAN communication chain — which is also the most commonly misconfigured parameter in all LeRobot commands.

This means that all subsequent teleoperation, data collection, training, and evaluation commands are identical for both arms — you only need to replace the corresponding arm name.

Loading Comments...