Skip to main content
Stage 3 · Chapter 14 · Theory & Practice

14. Dataset Structure and Quality Inspection

Chapter 14 of the Seeed Physical AI Beginner's Course — what is actually stored on disk, the four quality standards, playback and image inspection, and what to do when problems are found.

14.1 Dataset Structure: What's Actually Stored on Disk​

Structure

14.1 Dataset Structure: What's Actually Stored on Disk

The dataset recorded in Chapter 13, seeed_rebot_b601_rs/test, looks like this on disk:

~/.cache/huggingface/lerobot/seeed_rebot_b601_rs/test/
├── data/
│ └── chunk-000/
│ └── file-000.parquet ← All numeric frames (state / action / timestamps)
├── videos/
│ ├── observation.images.front/
│ │ └── chunk-000/
│ │ └── file-000.mp4 ← Overhead camera: 50 videos concatenated
│ └── observation.images.wrist/
│ └── chunk-000/
│ └── file-000.mp4 ← Wrist camera: same
└── meta/
├── info.json ← Info: version, fps, total frames, feature definitions
├── stats.json ← Stats: mean/variance/extremes per feature
├── tasks.parquet ← Task description table
└── episodes/
└── chunk-000/
└── file-000.parquet ← Profile card for each Episode

Three storage formats, each for one data type:

FormatWhat It StoresWhy
MP4 videoAll image frames from both camerasImages take up >90% of dataset size; video compression saves 1–2 orders of magnitude vs. per-frame images.
Parquet tablePer-frame numeric values: state, action, timestamps, indicesColumnar storage; reading "all values of joint 3" doesn't require loading the whole file.
Meta infoStructure definitions, statistics, tasks, episode indexLoaders and training programs read this first to know how to interpret the other two.

14.2 What Counts as "Good" Data: Four Quality Standards​

Quality

14.2 What Counts as "Good" Data: Four Quality Standards

To judge whether a dataset is ready for training, look at four dimensions:

Four quality standards

14.3 Playback and Image Inspection​

Inspection

14.3 Playback and Image Inspection

For visualization playback use lerobot-dataset-viz; for real-robot playback use lerobot-replay. For real-robot playback, use Episode 0, one in the middle, and the last one: the first checks workflow correctness, the middle checks state drift, the last most easily reveals fatigue-related quality decline.

During playback, check against these criteria:

  • Both camera feeds present; no black screens, artifacts, or frozen streams.
  • Clear, well-exposed images; block and gripper always visible.
  • Actions synchronized with images: at the moment the gripper closes, it should be touching the block.
  • Starts in standard starting pose, ends satisfying end conditions.

14.4 What to Do When Problems Are Found​

Fixes

14.4 What to Do When Problems Are Found: Delete, Supplement, or Re-record the Whole Set

Three paths when issues are found:

  • A few bad Episodes (e.g., Episodes 3 and 17 are blurry) → delete those 2, then record 2 more.
  • Batch-wide problems (e.g., half have changed lighting, entire batch has audio-video desync) → don't patch, re-record the whole set. A patched-together dataset hurts the model more than having less data.

Two facts about deletion: after deletion, the tool automatically rebuilds the dataset — episodes are renumbered consecutively, stats.json recalculated; you don't need to manually fix anything. Whether deleting or supplementing, the tool regenerates the meta.

Loading Comments...