Skip to main content
Stage 3 · Chapter 16 · Practice

16. Training Your First ACT Policy

Chapter 16 of the Seeed Physical AI Beginner's Course — batch size, learning rate and steps, checkpoint management, starting training, monitoring loss and GPU status, and resuming interrupted training.

⚡ No-code · No environment setup

Skip the setup — run the reBot Arm and LeRobot from one app

SenseCraft Robotics is Seeed's no-code platform for the SO-ARM101, reBot Arm 102 + B601-RS and B601-DM. Connect the arms, calibrate, collect demonstrations, train and run inference from a guided interface — no Python environment, no terminal.

  • ✅ 6-step guided workflow
  • ✅ Cloud training — no local GPU
  • ✅ Windows / macOS client
  • ✅ SO-ARM101 · B601-RS · B601-DM

16.1 Three Key Configs: Batch Size, Learning Rate, Steps​

Configs

16.1 Three Key Configs: Batch Size, Learning Rate, Steps

In the terminal, run nvidia-smi to check your GPU and VRAM; consumer GPUs (e.g., 3050) can also train.

Batch Size​

If you have VRAM headroom, increase it to speed up convergence, but don't force it beyond available VRAM.

ConfigScenario
8 GB VRAM or lessCan train; use small batch size: 8 GB → batch size 4, 4 GB → batch size 2.
12 GB+ VRAMComfort zone; use default batch size; if VRAM is large, set batch size=16
Only integrated GPU / no NVIDIA GPUTrain on a cloud server

Learning Rate​

The "step size" per update. ACT comes with presets: AdamW optimizer, learning rate 1e-5, weight decay 1e-4, visual backbone at 1e-5. Policy presets are enabled by default (use_policy_training_preset), so these values apply automatically; you don't need to write anything. Too large a step causes loss oscillation or divergence; too small doubles training time. Don't touch it for your first training — these are tuned values from the original paper and extensive practice.

  • If you change Batch Size or Steps, no need to adjust learning rate.
  • If fine-tuning/resuming from a trained checkpoint, reduce learning rate to 1e-6–3e-6 (3–10x smaller).
  • If train loss barely drops (flatlined), don't raise LR yet; first add steps/data, then try 2e-5.

Add the following code; change both together to the same value:

--policy.optimizer_lr=1e-6 \
--policy.optimizer_lr_backbone=1e-6

Training Steps​

For 50 Episodes, if you don't want to read the steps explanation below, just run it at 80,000 (50 Episodes).

Steps scale proportionally: if batch size is halved, samples seen per step are halved; to give the model the same number of passes (epochs), steps must double. E.g., default batch size=8, steps=80000; batch size=4 → steps=160000; batch size=2 → steps×4; batch size=16 → steps÷2.

You can also set more steps — during training you can press Ctrl+C to stop at any time, choosing whether to stop based on loss and other parameters; the model generated so far is saved automatically.

  • Total frames ≈ total length of the video recordings.
  • epoch (one pass) = the student watches the entire recording from start to finish.
  • steps = how many segments the student watched in total.
Training steps

16.2 Saving and Managing Checkpoints​

Checkpoints

16.2 Saving and Managing Checkpoints

No manual saving needed: a checkpoint is saved every 20,000 steps (save_freq), plus a final one at the end. So it's fine to set a large step count — you can pick the model from lower steps and discard under-trained or over-fitted ones.

outputs/train/act_grab_cube_v1/
├── train_config.json ← Full config for this run (needed to resume)
└── checkpoints/
├── 0020000/pretrained_model/ ← Model archive at each step count
├── 0040000/pretrained_model/
├── ...
└── last/pretrained_model/ ← Last checkpoint, used in Chapter 17
  • Disk usage: each checkpoint is a complete model weight file; dozens of them add up. Once training stabilizes, early/mid checkpoints can be deleted, keeping only last.
  • During inference, --policy.path points to checkpoints/last/pretrained_model.

16.3 Starting Training​

Training

16.3 Starting Training

All checks passed — start (in the conda lerobot environment):

lerobot-train \
--dataset.repo_id=seeed_rebot_b601_rs/test \
--policy.type=act \
--output_dir=outputs/train/act_rebot_test \
--job_name=act_rebot_test \
--policy.device=cuda \
--wandb.enable=false \
--policy.push_to_hub=false \
--steps=100000
tip

If using an RTX 50-series GPU, add --dataset.video_backend=pyav to work around missing APIs in the torchvision preview.

If VRAM is insufficient or you want to set more at once, add --batch_size to set batch size.

Parameter notes:

ParameterMeaning
--dataset.repo_idDataset name from Chapter 13 (use local name directly; for Hub use ${HF_USER}/xxx)
--policy.type=actPolicy type; can also use diffusion, smolvla, etc. This stage uses ACT
--output_dirDirectory for all training outputs
--job_nameName for this run, used in logs to distinguish runs
--policy.device=cudaTrain on GPU
--wandb.enable=falseDisable wandb online dashboard (register and enable if you want; not required)
--policy.push_to_hub=falseDon't upload to Hub yet; wait until Chapter 17 evaluation is satisfactory
--stepsTraining steps
--batch_sizeBatch size

Time estimate: 100k steps on a consumer GPU typically takes a few hours, depending on GPU and batch size.

16.4 Monitoring Loss and GPU Status​

Monitoring

16.4 Monitoring Loss and GPU Status

After pressing Enter, the terminal starts scrolling training logs. LeRobot prints a summary line every 200 steps (controlled by --log_freq), like this:

step: 10000  smpl: 80K  ep: 35.6  loss: 1.832  grdn: 12.4  lr: 1.0e-05  updt_s: 0.21  data_s: 0.003  eta: 3:42:10

Field by field (field names may vary slightly between versions):

FieldMeaningWhat to Look For
stepCurrent stepCompare with --steps to check progress
epEpochs trainedCorresponds to "how many times watched the recording"
lossTraining lossFast drop early, slow decline later, small fluctuations is normal shape
grdnGradient normSudden spike to hundreds/thousands indicates unstable training
lrCurrent learning rateConfirm it's the expected value
updt_s / data_sPer-step update/data-loading timeLarge data_s means data loading is the bottleneck
etaEstimated time remainingDecide whether to go eat or sleep

Normal trends for these metrics, in three categories:

  • Should keep declining — loss. The decline has three phases: initial steep drop, mid gradual decline, late small fluctuations at a low level, overall flattening. This "fast then slow then flat" curve is a healthy convergence curve. Two abnormal shapes to watch: never drops (data/config problem — check camera keys); drops then bounces back (training divergence — halve LR and retrain).
  • Should overall converge with allowed jitter — grdn (gradient norm). The overall trend follows loss downward and stabilizes, but spikes are normal — an occasional spike that recovers is fine; what's dangerous is continuous amplification, wave after wave higher — that's a divergence precursor; handle as above: lower LR.
  • Should stay constant — lr, updt_s, data_s, GPU utilization. lr stays at your set value throughout, just for your confirmation; per-step time (updt_s/data_s) and watch -n 1 nvidia-smi GPU utilization should both be stable — persistently low or fluctuating utilization means the GPU is waiting for data; the bottleneck is data loading, not the GPU.
Loss curve
GPU utilization

16.5 Resuming Interrupted Training​

Resume

16.5 Resuming Interrupted Training

If training loses power, network, or terminal mid-run, no need to start over — as long as at least one checkpoint has been saved (i.e., training has run past 20,000 steps):

lerobot-train \
--config_path=outputs/train/act_rebot_test/train_config.json \
--resume=true
  • Resume uses the saved config: resumed training uses the config saved in train_config.json; command-line parameters are ignored. To change parameters (e.g., steps, batch size), start a new run; don't use resume.
  • Continue from latest checkpoint: optimizer state and step count are restored; the loss curve continues seamlessly.
Loading Comments...