Skip to main content
Stage 3 · Chapter 17 · Theory & Practice

17. Real-Robot Inference, Evaluation, and Data Iteration

Chapter 17 of the Seeed Physical AI Beginner's Course — inference data flow, preprocessing and de-normalization, starting inference, action chunk execution, safety, success-rate evaluation, generalization testing, failure analysis, and failure-driven data collection.

17.1 Inference Data Flow​

Flow

17.1 Inference Data Flow: Understand in One Diagram

Inference data flow

17.2 Preprocessing and De-normalization​

Preprocessing

17.2 Preprocessing and De-normalization

During training the model eats normalized data; during inference you must follow the same rules for both input and output:

DirectionProcessingStatistics Used
Into modelImage resize + ImageNet mean/std; state minus mean, divided by std (z-score)Training dataset's meta/stats.json
Out of modelAction multiplied by std, plus mean; restore to real joint anglesSame as above
Preprocessing and de-normalization

17.3 Starting Real-Robot Inference​

Inference

17.3 Starting Real-Robot Inference

Use lerobot-record to load the policy; robot and camera parameters are identical to collection:

RS version:

lerobot-record \
--robot.type=seeed_b601_rs_follower \
--robot.port=can0 \
--robot.can_adapter=socketcan \
--robot.cameras='{ front: {type: opencv, index_or_path: 0, width: 640, height: 480, fps: 30, fourcc: "MJPG"}, side: {type: opencv, index_or_path: 2, width: 640, height: 480, fps: 30, fourcc: "MJPG"} }' \
--robot.id=follower1 \
--display_data=false \
--dataset.repo_id=seeed/eval_test18 \
--dataset.single_task="Grab the crayfish into the box" \
--dataset.num_episodes=10 \
--dataset.episode_time_s=60 \
--dataset.reset_time_s=10 \
--policy.path=outputs/train/act_rebot_test/checkpoints/last/pretrained_model \
--policy.push_to_hub=false

DM version:

lerobot-record \
--robot.type=seeed_b601_dm_follower \
--robot.port=/dev/ttyACM0 \
--robot.can_adapter=damiao \
--robot.cameras='{ front: {type: opencv, index_or_path: 0, width: 640, height: 480, fps: 30, fourcc: "MJPG"}, side: {type: opencv, index_or_path: 2, width: 640, height: 480, fps: 30, fourcc: "MJPG"} }' \
--robot.id=follower1 \
--display_data=false \
--dataset.repo_id=seeed/eval_test18 \
--dataset.single_task="Grab the crayfish into the box" \
--dataset.num_episodes=10 \
--dataset.episode_time_s=60 \
--dataset.reset_time_s=10 \
--policy.path=outputs/train/act_rebot_test/checkpoints/last/pretrained_model \
--policy.push_to_hub=false
  • --dataset.num_episodes=10: run 10 episodes.
  • --dataset.episode_time_s=60: max 60 seconds per episode. Set it based on task duration — e.g., grasping a crayfish into a box takes ~20-30 seconds, so set 30-40 to leave margin. If you want to test the model without waiting, set it very long (e.g., 300), since there's a gap between episodes.
  • --dataset.reset_time_s=10: 10 seconds between episodes for you to reset objects (during evaluation, keep initial state as consistent as possible).

17.4 Action Chunk Execution​

Execution

17.4 Action Chunk Execution

  • One inference outputs a 100-step action chunk; only the first n steps are executed open-loop (n_action_steps), then re-observe — predictions further out are less reliable.
  • When temporal ensembling is enabled (temporal_ensemble_coeff), the action at each timestep is a weighted average of multiple predictions, with near-zero jitter.
  • If the real robot looks "stuttery," it's likely the computation gap between chunks — old chunk finished, new one not yet computed. Increasing n_action_steps can help, at the cost of weaker disturbance resistance.

17.5 Safety: Limits, Speed Limits, E-Stop​

Safety

17.5 Safety: Limits, Speed Limits, E-Stop

  • Always use ESC to stop; don't use Ctrl+C. Before stopping, let the arm finish the current action chunk or manually return it to a safe pose to avoid stopping mid-air in a loaded position.
  • Always be ready to cut power; if the arm behaves abnormally, emergency power-off is needed.

17.6 Evaluation: Success Rate and Completion Time​

Evaluation

17.6 Evaluation: Success Rate and Completion Time

Fix starting conditions, run 20 consecutive tests, record each one.

  • Success rate = successes ÷ 20. For a first trained model, >50% is a normal start, >80% is excellent.
  • Completion time: check stability — are the successful runs similar in duration? Inconsistent speed means the policy is "hesitating."
  • Failed runs — don't just record a ✗ — note the failure mode.

17.7 Generalization Testing​

Generalization

17.7 Generalization Testing

After testing under standard conditions, vary conditions one by one and see how much success rate drops (ACT with 50 Episodes won't have great generalization; we recommend adding data).

TestMethodExpectation
Position generalizationPlace block outside the five pencil points but within training coverageShould barely drop; if it drops, position diversity is insufficient
Mild disturbancePlace unrelated objects on the tableA visually clean-trained model should be unaffected
Major distribution shiftBrand-new objects, mirrored reflective surfaceFailure is expected; no need to fix

The point of generalization testing isn't to prove how strong the model is, but to map out its capability boundary — use freely within the boundary; supplement data and gradually expand it beyond.

17.8 Failure Type Analysis​

Failures

17.8 Failure Type Analysis

Failure TypeMost Likely CauseCountermeasure
Can't reach: moves toward wrong positionInsufficient data coverage at that position (out of distribution)Supplement demonstrations in that area
Unstable grasp: touches but can't hold/dropsGripper closing timing learned imprecisely; too few grasp-moment demonstrationsAdd high-quality demonstrations of the grasp moment
Random motion throughout; actions are absurdTraining didn't converge at all, or scene/lighting changed significantlyCheck whether data collection scene and lighting match inference
tip

Rule out config issues first, then suspect data issues — random motion is a config disease; can't-reach is a data disease.

17.9 Data Iteration: Failure-Driven Data Collection​

Iteration

17.9 Data Iteration: Failure-Driven Data Collection

The final step of the loop — turn failures into data:

  1. Categorize: identify failure type and corresponding scene.
  2. Supplement: record 10-20 new demonstrations for the failure scene — can't reach? record at that position; unstable grasp? record the grasp moment. Consciously expand the grasp boundary gradually — e.g., place blocks at points 5-10 cm beyond the original cross to expand the dataset.
  3. Retrain: retrain with the new dataset.
Data iteration

With this, the closed loop from the start of the chapter is fully complete: teleoperation, collection, inspection, training, inference, evaluation, iteration — this pipeline is reused as-is for any new task. That is the core deliverable of Stage 3.

Loading Comments...