Skip to main content
Stage 4 · Chapter 20 · Practice

20. Preparing the reBot VLA Dataset

Chapter 20 of the Seeed Physical AI Beginner's Course — prerequisites, checking the LeRobot dataset, adding language task descriptions, configuring state/action/camera keys, creating meta/modality.json, setting the embodiment tag, verifying joint order and dimensions, and multi-task organization.

⚡ No-code · No environment setup

Skip the setup — run the reBot Arm and LeRobot from one app

SenseCraft Robotics is Seeed's no-code platform for the SO-ARM101, reBot Arm 102 + B601-RS and B601-DM. Connect the arms, calibrate, collect demonstrations, train and run inference from a guided interface — no Python environment, no terminal.

  • ✅ 6-step guided workflow
  • ✅ Cloud training — no local GPU
  • ✅ Windows / macOS client
  • ✅ SO-ARM101 · B601-RS · B601-DM

GR00T uses the LeRobotDataset v2/v3 format on LeRobot, and additionally requires meta/modality.json to describe the semantic split of state, action, video, and annotation. This chapter assumes you have already collected ACT data on the reBot Arm via lerobot-record; next we will upgrade it to VLA training data.

Preparing the reBot VLA dataset

20.1 Prerequisites​

Prerequisites

20.1 Prerequisites

Prerequisites
ItemRequirement
HardwarereBot Arm B601-RS or B601-DM calibrated (see table below)
SoftwareLeRobot installed; recommended pip install "lerobot[groot,training]"
DataAt least 50 successful demonstrations for one task; for multi-task, ≥ 30 per task
CameraTraining and inference use the same key names, resolution, and count

Model variant reference (only change these three in all subsequent lerobot-record / lerobot-rollout):

Versionrobot.typerobot.portrobot.can_adapterWiki
B601-RSseeed_b601_rs_followercan0socketcanGetting Started with LeRobot
B601-DMseeed_b601_dm_follower/dev/ttyACM0damiaoGetting Started with LeRobot

Before using RS, configure CAN: sudo ip link set can0 type can bitrate 1000000 && sudo ip link set can0 up. The teleop side is always rebot_arm_102_leader, commonly on port /dev/ttyUSB0.

Reference documents:

20.2 Checking the LeRobot Dataset​

Check dataset

20.2 Checking the LeRobot Dataset

Checking the LeRobot dataset

Dataset Directory Structure​

Local datasets are located by default at:

~/.cache/huggingface/lerobot/<repo_id>/
├── data/
│ └── chunk-000/
│ └── episode_*.parquet
├── videos/
│ └── chunk-000/
│ └── observation.images.<camera_name>/
├── meta/
│ ├── info.json
│ ├── episodes.jsonl
│ ├── tasks.jsonl ← language task descriptions
│ ├── stats.json
│ └── modality.json ← required by GR00T, create or verify manually

Quick Check with Python​

from lerobot.datasets.lerobot_dataset import LeRobotDataset

dataset = LeRobotDataset("seeed_rebot_b601_rs/pick_cube") # RS example; for DM use seeed_rebot_b601_dm/pick_cube
print(dataset)
print("Feature keys:", dataset.features.keys())
print("Frame 0 state shape:", dataset[0]["observation.state"].shape)
print("Frame 0 action shape:", dataset[0]["action"].shape)

Required Checklist​

Check itemExpected value (reBot B601-RS / B601-DM single arm)
observation.state dimension(7,) - 6 joints + 1 gripper
action dimension(7,) - aligned with state
Video keyse.g. observation.images.front, observation.images.side
FPSUsually 30
tasks.jsonlEvery task_index has a corresponding language description
Failed episodesDeleted or marked out to avoid polluting training
warning

If state/action is not 7-dimensional, the robot configuration during recording was wrong; go back to lerobot-record to troubleshoot. Do not force-edit modality.json to pad dimensions.

20.3 Adding Language Task Descriptions​

Language

20.3 Adding Language Task Descriptions

Adding language task descriptions

VLA training requires language conditioning. There are two ways:

Each episode is recorded with --dataset.single_task. The following uses B601-RS as an example (Wiki); DM users replace type / port / can_adapter with seeed_b601_dm_follower, /dev/ttyACM0, damiao.

# RS: bring up CAN first
sudo ip link set can0 down 2>/dev/null
sudo ip link set can0 type can bitrate 1000000
sudo ip link set can0 up

lerobot-record \
--robot.type=seeed_b601_rs_follower \
--robot.port=can0 \
--robot.id=follower1 \
--robot.can_adapter=socketcan \
--robot.cameras="{ front: {type: opencv, index_or_path: 0, width: 640, height: 480, fps: 30, fourcc: "MJPG"}, side: {type: opencv, index_or_path: 2, width: 640, height: 480, fps: 30, fourcc: "MJPG"}}" \
--teleop.type=rebot_arm_102_leader \
--teleop.port=/dev/ttyUSB0 \
--teleop.id=rebot_arm_102_leader \
--display_data=true \
--dataset.repo_id=${HF_USER}/rebot_vla_pick_cube \
--dataset.num_episodes=50 \
--dataset.single_task="put the black cube on the blue tray" \
--dataset.push_to_hub=false \
--dataset.episode_time_s=30 \
--dataset.reset_time_s=20

Method B: Backfill meta/tasks.jsonl​

If existing ACT data lacks language, edit meta/tasks.jsonl:

{"task_index": 0, "task": "put the black cube on the blue tray"}
{"task_index": 1, "task": "put the screwdriver into the toolbox"}

In a multi-task dataset, different episodes are associated with different descriptions via the task_index field. All episodes of the same task should share the same task_index.

Language Annotation Guidelines​

  1. Verb-first, describing the target action: "grasp...", "place...", "push...".
  2. Be specific about object names: "black cube" is better than "object".
  3. Keep sentence patterns consistent: for multi-task, use the same template, e.g. always "put X on Y".
  4. Either Chinese or English works, but the language should be consistent between training and inference.
  5. Avoid multiple phrasings for one data point (especially during early fine-tuning).

20.4 Configuring State Keys and Action Keys​

State & Action

20.4 Configuring State Keys and Action Keys

Configuring state keys and action keys

The 7-dimensional vector of the reBot Arm B601-RS / B601-DM is concatenated in the following joint order (consistent with the LeRobot driver):

IndexKey name (semantic)Meaning
0shoulder_panShoulder rotation
1shoulder_liftShoulder lift
2elbow_flexElbow flexion
3wrist_flexWrist flexion
4wrist_yawWrist yaw
5wrist_rollWrist roll
6gripperGripper open/close

In GR00T's modality.json, the above 7 dimensions are split into two semantic keys:

  • single_arm: indices 0-5 (6 joints)
  • gripper: index 6 (gripper)
note

Python slicing is half-open: "end": 6 means up to index 5, and "start": 6, "end": 7 means index 6.

20.5 Configuring Camera Keys​

Camera

20.5 Configuring Camera Keys

Configuring camera keys

GR00T maps original camera keys in the dataset to standard key names via the video field of modality.json.

Common reBot camera layouts​

Dataset key (original_key)Modality standard keyRecommended use
observation.images.frontfrontBracket-mounted wide view
observation.images.sidesideWrist close-up

Example: if the camera keys during recording are front and side:

"video": {
"front": {
"original_key": "observation.images.front"
},
"side": {
"original_key": "observation.images.side"
}
}

Key principles:

  1. original_key must exactly match the actual key in the dataset.
  2. The standard keys on the left side of modality (front, side) will be used uniformly during training and inference.
  3. A single camera can train, but two cameras usually perform better.
  4. Recommended resolution is uniformly 640x480, consistent with recording parameters.

Find the local camera index:

lerobot-find-cameras opencv

20.6 Creating meta/modality.json​

modality.json

20.6 Creating meta/modality.json

Creating meta/modality.json

Create modality.json in the dataset's meta/ directory. Below is the complete example for the reBot Arm B601 single-arm 7-dimensional joint space (identical for RS / DM):

{
"state": {
"single_arm": {
"start": 0,
"end": 6
},
"gripper": {
"start": 6,
"end": 7
}
},
"action": {
"single_arm": {
"start": 0,
"end": 6
},
"gripper": {
"start": 6,
"end": 7
}
},
"video": {
"front": {
"original_key": "observation.images.front"
},
"side": {
"original_key": "observation.images.side"
}
},
"annotation": {
"human.task_description": {
"original_key": "task_index"
}
}
}

Field Description​

FieldPurpose
state / actionDefine the index range of each segment in the concatenated vector
videoMap LeRobot video keys to GR00T standard camera names
annotationAssociate task_index with tasks.jsonl. reBot uses human.task_description; LIBERO / SimplerEnv use human.action.task_description
warning

If the dataset has only one task and no task_index field, first ensure lerobot-record wrote tasks.jsonl, otherwise GR00T cannot read the language condition.

20.7 Setting the Embodiment Tag​

Embodiment tag

20.7 Setting the Embodiment Tag

Setting the embodiment tag

For custom robots like the reBot Arm, use the same setting for both training and inference:

embodiment_tag = new_embodiment

Meaning:

  • Tells GR00T to use the new-embodiment projection layer, not reusing the pretrained humanoid state/action dimensions.
  • LeRobot training parameter: --policy.embodiment_tag=new_embodiment.
  • The fine-tuned checkpoint saves the corresponding modality config, which is automatically loaded at inference time.
warning

Do not use pretraining tags such as LIBERO_PANDA, DROID, SIMPLER_ENV_GOOGLE on reBot data — their state/action dimensions and semantics do not match reBot. There is also no official tag called libero_sim.

20.8 Checking Joint Order and Data Dimensions​

Verify

20.8 Checking Joint Order and Data Dimensions

Checking joint order and data dimensions

This is the most common cause of "training loss decreases but the real robot does not move at all." Please verify item by item:

Step 1: Print dataset meta​

import json
from pathlib import Path

meta_dir = Path.home() / ".cache/huggingface/lerobot/seeed_rebot_b601_rs/pick_cube/meta"
print(json.dumps(json.loads((meta_dir / "info.json").read_text()), indent=2))
print((meta_dir / "modality.json").read_text())

Step 2: Verify modality slicing​

import numpy as np
from lerobot.datasets.lerobot_dataset import LeRobotDataset

ds = LeRobotDataset("seeed_rebot_b601_rs/pick_cube")
s = ds[0]["observation.state"].numpy()
mod = json.loads((meta_dir / "modality.json").read_text())

arm = s[mod["state"]["single_arm"]["start"]:mod["state"]["single_arm"]["end"]]
grip = s[mod["state"]["gripper"]["start"]:mod["state"]["gripper"]["end"]]
print("single_arm:", arm.shape) # expect (6,)
print("gripper:", grip.shape) # expect (1,)

Step 3: Visualize the data​

lerobot-dataset-viz --repo_id=seeed_rebot_b601_rs/pick_cube --episode-index=0

Observe:

  • Are images synchronized with joint motion?
  • Does the gripper dimension change when the gripper opens/closes?
  • Does the language description match the visual content?

Step 4: Statistical checks​

print(ds.meta.stats["observation.state"])
print(ds.meta.stats["action"])

If some dimension has min == max (no variation), that joint did not move in the data; consider excluding it from training or recollecting.

20.9 Multi-task Dataset Organization​

Multi-task

20.9 Multi-task Dataset Organization

Multi-task dataset organization

To train "one model, multiple language tasks", two approaches are recommended:

{"task_index": 0, "task": "put the black cube on the blue tray"}
{"task_index": 1, "task": "put the screwdriver into the toolbox"}
{"task_index": 2, "task": "push the red cup to the left side of the table"}

Cycle through --dataset.single_task while recording, or record in batches and merge into the same dataset.

Method B: Merging multiple datasets​

LeRobot supports multi-dataset training (depending on version); the simpler approach is to use one repo_id during recording and distinguish tasks by task_index.

Data Volume Recommendations​

ScenarioRecommendation
Single-task starter50 episodes
Single-task stable100-200 episodes
Multi-task (3 tasks)≥ 30 episodes each
Position generalization≥ 10 episodes per position variant

20.10 Data Quality Checklist​

Checklist

20.10 Data Quality Checklist

Data quality checklist

Before uploading to Hub or starting training, confirm:

  • observation.state and action are both 7-dimensional float32
  • meta/modality.json exists and index slicing is correct
  • Every task_index in meta/tasks.jsonl has a non-empty description
  • Camera key names match between modality.json and the dataset
  • No all-zero / idle waste episodes
  • Cameras fixed, objects in view, stable lighting
  • Angle units unified (the reBot low-level motor API uses degrees; the LeRobot driver internally converts to radians; the dataset and training/inference must stay consistent)
  • Plan to use new_embodiment for embodiment_tag

Push to Hugging Face Hub (optional)​

huggingface-cli login
lerobot-record ... --dataset.push_to_hub=true
# or upload manually
huggingface-cli upload ${HF_USER}/rebot_vla_pick_cube ~/.cache/huggingface/lerobot/seeed_rebot_b601_rs/pick_cube

20.11 Chapter Summary​

Summary

20.11 Chapter Summary

  • GR00T needs standard LeRobot data + meta/modality.json.
  • reBot's 7-dimensional vector is split into single_arm(6) + gripper(1); RS / DM have the same dimensions, only driver parameters differ.
  • Language is connected via tasks.jsonl + annotation.human.task_description.
  • Camera key names must align across recording, modality, and inference.
  • The next chapter uses the prepared data to start lerobot-train --policy.type=groot.
Loading Comments...