Skip to main content
Stage 4 · Chapter 22 · Theory & Practice

22. GR00T Inference and Real-Robot Deployment

Chapter 22 of the Seeed Physical AI Beginner's Course — the end-to-end loop, decoupling inference and control, single-machine vs distributed, camera/state/language inputs, action chunk output, latency, action buffering and RTC, safety limits, evaluation, and the stage project.

⚡ No-code · No environment setup

Skip the setup — run the reBot Arm and LeRobot from one app

SenseCraft Robotics is Seeed's no-code platform for the SO-ARM101, reBot Arm 102 + B601-RS and B601-DM. Connect the arms, calibrate, collect demonstrations, train and run inference from a guided interface — no Python environment, no terminal.

  • ✅ 6-step guided workflow
  • ✅ Cloud training — no local GPU
  • ✅ Windows / macOS client
  • ✅ SO-ARM101 · B601-RS · B601-DM

Chapter 21 covered fine-tuning and the basic real-robot commands; this chapter zooms in on inference deployment: how the inference side and control side are decoupled, how to choose between single-machine and distributed, how inputs/outputs are aligned, and latency, async buffering, safety limits, and task evaluation. Finally, the stage project "place the test tube into the left rack" runs through the entire pipeline.

GR00T inference and real-robot deployment

22.1 What Does the End-to-End Loop Look Like?​

End-to-end loop

22.1 What Does the End-to-End Loop Look Like?

End-to-end loop

A successful VLA real-robot episode can be abstracted as a fixed-frequency control loop:

User language instruction L (e.g. place the test tube into the left rack)
|
v
+---------------------------------------+
| Control Client (Robot Control) |
| 1. Capture cameras: front + side |
| 2. Read joint state (7-dim) |
| 3. Pack observation -> send to infer |
+-------------------+-------------------+
| images + state + task
v
+---------------------------------------+
| Inference side (GR00T Policy/Server)|
| VLM + DiT -> action_chunk (H x 7) |
+-------------------+-------------------+
| action chunk
v
+---------------------------------------+
| Control side executes |
| Write motors step by n_action_steps |
| (optional RTC: async prefetch next) |
+---------------------------------------+
StageKey constraint
CameraKey names, resolution, and count match training (front bracket wide view / side wrist)
State7-dim order matches modality.json; angle unit is consistent between training and inference
Language--task sentence pattern close to training annotations
Actionn_action_steps ≤ training chunk_size (N1.7 commonly 40)

22.2 Decoupling the Inference Side and Control Side​

Decoupling

22.2 Decoupling the Inference Side and Control Side

Decoupling the inference side and control side

Splitting the system into two sides keeps real-time control and heavy computation from dragging each other down:

Control side responsibilities​

  • Capture images and joint state at a fixed frequency (e.g. 30 Hz)
  • Assemble the observation packet {images, state, task}
  • Receive action_chunk and dispatch step by step to the reBot driver
  • Execute e-stop, soft limits, and timeout protection

Corresponding tools: lerobot-rollout / lerobot-record (with --policy.path).

Inference side responsibilities​

  • Load policy.path (fine-tuned checkpoint) and base_model_path=nvidia/GR00T-N1.7-3B
  • Decode the reBot action space with embodiment_tag=new_embodiment
  • Return an action chunk of shape about (H, 7) (H determined by training chunk_size)

Corresponding form: by default the in-process groot policy; advanced use can be a standalone HTTP/gRPC service (refer to the deployment examples in the Isaac GR00T repository).

Decoupling principle: the control side is unaware of the model's internal structure; the inference side does not directly operate motors. The interface contract is only "observation in, action chunk out."

22.3 Single-Machine vs. Distributed Deployment​

Deployment

22.3 Single-Machine vs. Distributed Deployment

Single-machine vs distributed deployment

The GPU workstation connects cameras, CAN/serial, and the arm at the same time:

lerobot-rollout \
--policy.path=${MODEL_PATH} \
--policy.base_model_path=nvidia/GR00T-N1.7-3B \
--policy.embodiment_tag=new_embodiment \
--device=cuda \
--robot.type=seeed_b601_rs_follower \
...

Pros: no network round-trip, simple joint debugging. Cons: a GPU host must be on-site.

Distributed deployment (advanced)​

NodePlacement
GPU machineInference Server (loads GR00T)
On-site / IPCControl Client (cameras + reBot driver)

Suitable scenarios: lab GPU separated from production arm, multiple arms sharing one inference pool.

ComparisonSingle-machineDistributed
LatencyMainly inference timeInference + network RTT
ComplexityLowNeed serialization, timeout, reconnect conventions
ScalabilityOne machine, one armOne service, multiple clients

Selection advice: first get the stage project running on a single machine; after confirming success rate, split to distributed.

22.4 Camera, State, and Language Inputs​

Inputs

22.4 Camera, State, and Language Inputs

Camera, state, and language inputs

Each inference call requires three conditional inputs, all of which are essential (or consistent with what was declared during training):

1. Camera (Vision)​

Key nameMountPurpose
observation.images.front -> frontBracket wide viewScene and target localization
observation.images.side -> sideWristClose-up aiming, grasp/place

Recommended resolution 640x480; training and inference must match.

2. State​

reBot Arm: single_arm 6-dim + gripper 1-dim = 7 dimensions, order consistent with Chapters 19/20. The control side reads the latest joint angles each control cycle before sending to inference.

3. Language​

Injected via --task / dataset.single_task. Example:

Place the test tube into the left rack.

Requirements:

  • Same language and sentence-style as training tasks.jsonl / human.task_description.
  • Clear object reference ("left rack" must be visually distinguishable).
  • Do not suddenly switch to a complex composite instruction never seen in training.

22.5 Action Chunk Output​

Output

22.5 Action Chunk Output

Action chunk output

A single GR00T inference does not output an instantaneous joint command, but an action chunk:

action_chunk.shape ~= (H, 7)
H = chunk_size / action_horizon # N1.7 fine-tuning commonly 40
each row 7-dim = 6 joints + gripper

Control-side execution strategy:

ParameterSuggestionDescription
chunk_size40 at trainingDetermines how far ahead the model can predict; do not arbitrarily enlarge at inference
n_action_stepsStart with 20Steps actually executed this round, must be ≤ chunk_size
Execution frequencyClose to recording fps (e.g. 30 Hz)Too fast or too slow deviates from the training distribution

If relative actions are enabled (use_relative_actions), the control side must restore them to absolute joint commands using the same rules as training; the gripper is usually excluded from relative.

22.6 Network and Inference Latency​

Latency

22.6 Network and Inference Latency

Network and inference latency

End-to-end latency roughly:

T_e2e ~= T_capture + T_pack + T_net + T_infer + T_unpack + T_actuate
ComponentTypical sourceMitigation
T_captureCamera exposure/USBMJPG, fixed resolution, avoid extra preprocessing
T_inferVLM + DiTbf16, batch=1, Flash Attention
T_netDistributed RTTGigabit, same datacenter, compress observations
T_actuateCAN/serial write cycleKeep control frequency close to training

Rules of thumb:

  • Single-machine: bottleneck is usually T_infer; use smaller n_action_steps + RTC to mask stalls.
  • Distributed: if RTT is unstable, first turn off RTC for synchronous debugging, then gradually enable async.
  • Do not solve latency by "enlarging chunk_size" — the window is fixed by training.

22.7 Action Buffering and Asynchronous Inference​

Buffering

22.7 Action Buffering and Asynchronous Inference

Action buffering and asynchronous inference

Action Queue​

The control side writes received action_chunk into a queue and pops it per control cycle. If the next chunk has not arrived before the queue empties, the arm will pause or reuse the last action — which is exactly what async inference avoids.

RTC (Real-Time Chunking)​

While executing the current chunk, the backend requests the next chunk with the latest observation:

lerobot-rollout \
... \
--policy.n_action_steps=20 \
--inference.type=rtc \
--inference.rtc.enabled=true \
--inference.rtc.execution_horizon=20 \
--inference.queue_threshold=0
ParameterSuggestion
n_action_steps / execution_horizonStart at 20, then tune for jitter
queue_thresholdRecommend ≤ 5; too large stacks stale actions

If jitter/twitch appears, first set --inference.rtc.enabled=false, confirm the synchronous path is healthy, then enable RTC.

22.8 Real-Robot Safety Limits​

Safety

22.8 Real-Robot Safety Limits

Real-robot safety limits

VLA output carries no physical guarantees, so safety must be enforced by the control layer:

LayerMeasure
HardwareE-stop button, power cut, cable management to prevent tangling
Driver / firmwareJoint soft/hard limits, current/torque protection
Software controlVelocity/acceleration clipping, workspace box, hold or move to safe pose on timeout
Experiment flowLower gain/speed on first inference; human in the loop; clear unrelated obstacles from the table

Debug checklist:

  1. Before loading the policy, use manual/teleop to confirm limits are effective.
  2. On policy rollout, first use a short --duration to confirm no runaway.
  3. On abnormal motion, e-stop immediately, record the current task, camera frames, and state, then review data and modality.

22.9 VLA Task Evaluation​

Evaluation

22.9 VLA Task Evaluation

VLA task evaluation

Evaluation methods​

MethodToolPurpose
Online eval recordinglerobot-record + --policy.pathSave fail/success episodes for replay
Real-time deploymentlerobot-rolloutTest latency, RTC, long-horizon stability

Suggested metrics​

MetricDescription
Success rateUnder fixed initial conditions and instructions, successes / total (recommend ≥ 20 runs)
Completion timeSeconds from start to placement done
Collision / e-stop rateRatio of non-task collisions or manual interventions
Instruction robustnessDoes a slightly rephrased instruction for the same task still succeed (within training distribution only)

Failure attribution order​

  1. Are camera key names / resolution consistent with training?
  2. Does the language sentence pattern deviate from annotations?
  3. Joint order and units.
  4. embodiment_tag, relative-action switch.
  5. Insufficient data coverage -> return to Chapter 20 to collect more.

22.10 Stage Project: Place the Test Tube into the Left Rack​

Stage project

22.10 Stage Project: Place the Test Tube into the Left Rack

Stage project

Project goal​

ItemContent
User inputPlace the test tube into the left rack.
System inputWide-view front + wrist side + current 7-dim state
Expected outputThe arm completes pick tube -> move to left rack -> place -> release gripper

Implementation steps​

  1. Data (if not already covering this task)

    • Collect ≥ 50 successful demonstrations; annotate uniformly using the above sentence pattern.
    • Write meta/modality.json (front / side, single_arm + gripper, human.task_description).
  2. Fine-tuning (Chapter 21)

    • embodiment_tag=new_embodiment, chunk_size=40.
    • Obtain checkpoints/last/pretrained_model.
  3. Single-machine deployment inference (B601-RS example; for DM change type / port / can_adapter)

export MODEL_PATH="outputs/train/${REPO_ID}/checkpoints/last/pretrained_model"

# RS CAN
sudo ip link set can0 down 2>/dev/null
sudo ip link set can0 type can bitrate 1000000
sudo ip link set can0 up

lerobot-rollout \
--strategy.type=base \
--policy.path=${MODEL_PATH} \
--policy.base_model_path=nvidia/GR00T-N1.7-3B \
--policy.embodiment_tag=new_embodiment \
--policy.n_action_steps=20 \
--robot.type=seeed_b601_rs_follower \
--robot.port=can0 \
--robot.id=follower1 \
--robot.can_adapter=socketcan \
--robot.cameras="{ front: {type: opencv, index_or_path: 0, width: 640, height: 480, fps: 30, fourcc: "MJPG"}, side: {type: opencv, index_or_path: 2, width: 640, height: 480, fps: 30, fourcc: "MJPG"}}" \
--task="Place the test tube into the left rack." \
--duration=90 \
--device=cuda \
--display_data=true \
--inference.type=rtc \
--inference.rtc.enabled=true \
--inference.rtc.execution_horizon=20 \
--inference.queue_threshold=0
  1. Evaluation
    • Fix the table layout, repeat ≥ 20 times, record success rate.
    • Archive failure episodes with lerobot-record; analyze whether the error is in localization, grasping, or placement.

Acceptance criteria​

  • Given the instruction "Place the test tube into the left rack.", the task can be executed end-to-end.
  • front / side match training, no mean is infinity-style key errors.
  • E-stop and soft limits work; motion can be cut off manually on abnormal behavior.
  • Record success rate and decide the next step is more data or tuning n_action_steps / RTC.

22.11 Chapter Summary​

Summary

22.11 Chapter Summary

  • Decoupling: the control side handles capture and execution, the inference side handles VLA forward pass; the interface is observation -> Action Chunk.
  • Deployment: start single-machine, then go distributed as needed; distributed needs extra attention to network latency.
  • Inputs: cameras + state + language must align strictly with training.
  • Output: consume the action chunk by n_action_steps; RTC uses a queue to mask inference time.
  • Safety: limits, e-stop, and speed clipping are enforced by the control layer.
  • Evaluation: success rate + failure attribution; the stage project validates the "language -> real-robot action" closed loop.

You have now completed the full path from VLA theory, data, fine-tuning, to GR00T real-robot deployment. For future iteration, prioritize collecting data for failure scenarios rather than blindly lengthening training steps.

Loading Comments...