Skip to main content

Stage 8 · Chapter 38 · Practice

38. Running the reBot Arm in Isaac Sim

Chapter 38 of the Seeed Physical AI Beginner's Course — running the reBot Arm in Isaac Sim: installing and starting Isaac Sim, the scene structure, USD basics, importing the arm with the URDF Importer, checking links, joints, visuals and collisions, configuring the articulation root and joint drives, stiffness and damping, the gripper linkage, the ground and workbench, Python control, and four practice demos.

This chapter explains the model import and basic control of the reBotArm-RS arm in NVIDIA Isaac Sim. Isaac Sim uses USD (Universal Scene Description) as its scene format, which differs fundamentally from MuJoCo's MJCF. Joint name mapping, gripper unit conversion, communication frequency, and safety design are covered in detail in Chapter 39 and will not be repeated here; this chapter focuses only on Isaac Sim-specific concepts and operations.

Let users master the reBot Arm's model import, Articulation configuration, and basic joint control in Isaac Sim.

38.1 Installing and Starting Isaac Sim​

Isaac Sim is based on the NVIDIA Omniverse platform and requires an RTX GPU. There are two ways to run it:

  1. Desktop application: download the Isaac Sim installer from the NVIDIA website and launch the GUI directly.
  2. Python scripts: run headless in a terminal through the isaaclab or isaacsim Python packages.

After launch you enter the Isaac Sim interface: on the left is the Stage Tree, on the right is the Property panel,

and in the middle is the 3D viewport.

# Launch via a Python script (Isaac Sim 4.x+)
./python.sh my_script.py

Key point: Isaac Sim is essentially an Omn Kit application; all functionality is exposed through the Python API (omni.isaac.* / isaacsim.*), and GUI operations and script operations are equivalent.

38.2 Understanding the Isaac Sim Scene Structure​

Isaac Sim's scene is rooted at the Stage (USD stage), and every object is a Prim (scene primitive).

Understanding three levels is enough:

Stage (root)
└── Prim (an object, e.g., arm, ground, workbench)
└── child Prims (e.g., each link)
└── Properties (e.g., joint, mesh, material)

Differences from MuJoCo:

ConceptMuJoCo (MJCF)Isaac Sim (USD)
Scene root<mujoco>Stage
Object<body>Prim
Joint<joint>Joint Prim (attached under a link)
Actuator<actuator>Joint Drive (USD property)
Collision<geom confluence>Collision API (attached to a mesh)

MuJoCo defines actuators as independent elements; Isaac Sim attaches "drive" as a Drive property directly on the joint. This is the most fundamental architectural difference between the two engines.

38.3 USD Model Basics​

USD (Universal Scene Description) is a scene description format developed by Pixar; Isaac Sim uses it in place of URDF/MJCF.

USD vs URDF​

This repository already has the RS arm's URDF file:

Isaac Sim does not use URDF directly; instead it converts it to USD through the URDF Importer.

FeatureURDFUSD
FormatXMLBinary/text
Layered overridesNot supportedSupports Layer references and overrides
Collision/visual separation<visual> / <collision> tagsCollision API / Mesh API
Joint driveNone (requires external controller)Joint Drive property built in
Physics engine couplingNot coupledCan bind PhysX properties

Key USD concepts​

  • Reference: one USD file references another, similar to MuJoCo's <include>.
  • Override: modify properties on top of a reference without changing the original file.
  • Payload: a lazily loaded reference, used for large-scene optimization.
  • Variant: different variants of the same model (e.g., "with gripper" and "without gripper").

Summary of the reBot Arm's structure (from URDF parsing):

base_link
└── joint1 (revolute, -2.8~2.8 rad) → link1
└── joint2 (revolute, 0~3.14) → link2
└── joint3 (revolute, 0~3.14) → link3
└── joint4 (revolute, -1.57~1.57) → link4
└── joint5 (revolute, -1.57~1.57) → link5
└── joint6 (revolute, -3.14~3.14) → link6
└── j_gripper_end (fixed) → gripper_end
├── gripper_joint1 (prismatic, 0~0.05) → gripper_left
└── gripper_joint2 (prismatic, 0~0.0715) → gripper_right

Six revolute joints plus one fixed joint connect the end-effector, and two prismatic joints drive the left and right gripper fingers.

38.4 Importing the reBot Arm USD​

URDF Importer​

Isaac Sim has a built-in URDF Importer tool; the menu path is:

Isaac Utils → Workflows → URDF Importer

Or use the Python API:

from isaacsim.import_config.urdf import ImportConfig
from omni.importer.urdf import _urdf

import_config = ImportConfig()
import_config.merge_fixed_joints = False # keep the fixed joint structure
import_config.make_default_prim = True
import_config.create_physics_scene = False # do not recreate if a scene already exists
import_config.fix_base = True # fix the arm base
import_config.default_drive_type = _urdf.UrdfJointTargetType.JOINT_DRIVE_POSITION

_urdf.import_urdf(urdf_path, output_usd_path, import_config)

Key choices when importing​

  1. merge_fixed_joints: set to False to keep the j_gripper_end fixed joint; otherwise

gripper_end is merged into link6. Keeping it is more intuitive; merging is more efficient.

  1. fix_base: set to True to fix base_link to the world so the arm does not fall due to gravity.
  2. default_drive_type: choose position drive (POSITION), so target angles can be sent directly after import.

Mesh file paths​

The STL meshes referenced by the URDF are in the meshes_rs/ directory. The importer automatically resolves the package://rebotarm_bringup/description/meshes_rs/ prefix. If the import fails, check the ROS_PACKAGE_PATH environment variable or manually change the mesh paths to absolute paths.

After import, check the structure in the Stage Tree:

/rebotarm_rs          ← root Prim
/base_link
/link1
/link2
...
/gripper_end
/gripper_left
/gripper_right

Principle: Isaac Sim converts the URDF's <joint> into USD Joint Prims. A revolute joint becomes a PhysicsRevoluteJoint, a prismatic joint becomes a PhysicsPrismaticJoint, and a fixed joint becomes a PhysicsFixedJoint. The joint's axis, limits, and other attributes are mapped directly onto USD properties.

38.6 Checking Visual and Collision​

The URDF's <visual> and <collision> are annotated with different APIs in USD:

from pxr import UsdPhysics

# check collision bodies
for prim in stage.Traverse():
if prim.HasAPI(UsdPhysics.CollisionAPI):
print("Collision:", prim.GetPath())

# check visual meshes
for prim in stage.Traverse():
if prim.IsA(UsdGeom.Mesh):
print("Mesh:", prim.GetPath())

Principle: Isaac Sim does not mark pure-visual bodies with <geom contype="0" conaffinity="0"> like MuJoCo. In USD, every mesh is renderable by default; only meshes with a CollisionAPI participate in physics collision. This means the same mesh can be both visual and collision, or purely visual.

38.7 Configuring the Articulation Root​

This is the most important concept in Isaac Sim, with no direct counterpart in MuJoCo.

What is an Articulation Root​

The Articulation Root tells PhysX: "these joints and links form an articulated system; solve it uniformly with the Featherstone

algorithm, rather than treating them as independent rigid bodies connected by constraints."

Without an Articulation Root:
base_link ←constraint→ link1 ←constraint→ link2 ...
each parent-child link pair is a separate constraint solver; with many joints this becomes unstable.

With an Articulation Root:
[Articulation Root] → base_link → link1 → link2 → ...
the whole kinematic chain is solved in one pass with the Featherstone algorithm, numerically stable.

How to configure it​

Add the PhysicsArticulationRootAPI on base_link:

from pxr import UsdPhysics

base_link = stage.GetPrimAtPath("/rebotarm_rs/base_link")
UsdPhysics.ArticulationRootAPI.Apply(base_link)

Principle: the Articulation Root must be placed on the root link of the kinematic chain. For the reBot Arm that is base_link. If placed on the wrong link, PhysX truncates the chain and downstream joints lose their drive. The URDF Importer usually adds the Articulation Root automatically, but if you edit the USD manually, check that it is still there.

38.8 Configuring Joint Drives​

Drive principle​

MuJoCo uses <motor> or <position> actuators, with drive torques computed externally in Python. Isaac Sim's Drive is a PD controller built into the joint; the torque is computed inside PhysX:

tau = kp * (target_pos - current_pos) + kv * (target_vel - current_vel) + feedforward
#This is almost the same PD control formula as MuJoCo's physics mode; the difference is that Isaac Sim puts the PD loop inside the engine, while MuJoCo computes it in Python and writes it into `data.ctrl`.

How to configure it​

from pxr import UsdPhysics

joint_path = "/rebotarm_rs/base_link/link1/joint1"
joint = UsdPhysics.Joint.Get(stage, joint_path)

drive = UsdPhysics.DriveAPI.Get(joint, "angular") # revolute joints use angular, prismatic use linear
drive.GetTargetPositionsAttr().Set([0.0]) # target angle
drive.GetTargetVelocitiesAttr().Set([0.0]) # target velocity
drive.GetStiffnessAttr().Set(80.0) # kp
drive.GetDampingAttr().Set(5.0) # kv
drive.GetMaxForceAttr().Set(36.0) # torque limit

Correspondence with the real-robot gains​

Isaac Sim Drive's Stiffness and Damping correspond to the real arm's MIT-mode kp and kd.

You can directly use the real-robot configuration values (see [rebotarm_hardware.yaml]/ReBot_Arm_DigitalTwin_RS/rebotarm_ros2/src/rebotarm_bringup/config/rebotarm_hardware.yaml)):

# Real-robot RS MIT gains
mit_kp: [80.0, 150.0, 150.0, 50.0, 50.0, 50.0]
mit_kd: [5.0, 10.0, 10.0, 5.0, 4.0, 4.0]

Fill these values into each joint's Drive properties, and the simulation behavior will be close to the real robot.

38.9 Setting Joint Stiffness and Damping​

Tuning principles for stiffness and damping:

  1. Stiffness too low: the joint is soft, reaches the target angle slowly, and sags visibly under load.
  2. Stiffness too high: the joint is too hard, may oscillate, and PhysX becomes numerically unstable.
  3. Damping too low: oscillates after reaching the target, with obvious overshoot.
  4. Damping too high: motion is sluggish, like moving in syrup.

Recommended starting values (corresponding to the real robot):

JointStiffness (kp)Damping (kd)Max Force
joint180536
joint21501036
joint31501036
joint450514
joint550414
joint650414

Tuning strategy: start with low values to make sure there is no oscillation, then gradually increase stiffness until the response is fast enough, then increase damping to eliminate residual oscillation. Do not start with high values.

38.10 Configuring the Gripper Linkage​

The Isaac Sim way​

Isaac Sim has no equality constraint; it uses Mimic Joint for linkage. The URDF's <mimic> tag is converted during import:

# The mimic in URDF (if the URDF does not have it, you need to add it manually in USD)
# <mimic joint="gripper_joint1" multiplier="1.43" offset="0"/>

The current RS URDF has no <mimic> tag, so the linkage needs to be configured manually after import. Two methods:

Method 1: PhysX Mimic Joint API

from pxr import UsdPhysics

left_joint = UsdPhysics.Joint.Get(stage, ".../gripper_joint1")
UsdPhysics.MimicAPI.Apply(left_joint)
mimic = UsdPhysics.MimicAPI(left_joint)
mimic.GetReferenceJointRel().SetTargetPath(".../gripper_joint2")
mimic.GetMultiplierAttr().Set(1.43) # 0.0715 / 0.05 = 1.43

Method 2: send commands synchronously in Python control

If you do not use the Mimic API, simply send the same target to both gripper joints in the control code:

# The left and right gripper strokes differ: left 0-0.05m, right 0-0.0715m
# When sending commands, scale by each stroke ratio
left_target = target_ratio * 0.05
right_target = target_ratio * 0.0715

Principle: MuJoCo's equality is a hard constraint at the physics-engine level, Isaac Sim's Mimic API is also an engine-level linkage, while Method 2 is a software linkage at the control level. Method 1 is more stable; Method 2 is more flexible.

38.11 Adding the Ground and Workbench​

Ground​

Isaac Sim has a built-in ground generation tool:

from isaacsim.core.api import World

world = World(stage_units_in_meters=1.0)
world.scene.add_default_ground_plane() # add a Z=0 ground collision plane

add_default_ground_plane() creates a plane Prim with a CollisionAPI; the default friction coefficient is

0.5. In MuJoCo the ground is <geom type="plane"/>; in Isaac Sim it is a plane mesh with collision.

Workbench​

Add a Box as the workbench:

from isaacsim.core.api.objects import DynamicCuboid

table = DynamicCuboid(
prim_path="/World/table",
name="table",
position=np.array([0.5, 0.0, 0.4]), # table top height 0.4m
scale=np.array([0.6, 0.6, 0.02]), # 60cm x 60cm x 2cm
color=np.array([0.5, 0.4, 0.3]),
)

A simple task object​

red_cube = DynamicCuboid(
prim_path="/World/red_cube",
name="red_cube",
position=np.array([0.5, 0.0, 0.42]),
scale=np.array([0.03, 0.03, 0.03]), # 3cm cube
color=np.array([1.0, 0.0, 0.0]),
)

Principle: Isaac Sim attaches collision and dynamics properties directly to object Prims. DynamicCuboid automatically creates a collision body and a rigid-body API; FixedCuboid only creates a collision body without a rigid body. This is more concise than MuJoCo, where you have to write <geom contype> and <body> separately in XML.

38.12 Controlling the Arm with Python​

Articulation API​

Isaac Sim wraps the whole arm's control interface with the Articulation class, so you do not need to operate joint by joint:

from isaacsim.core.api import World
from isaacsim.core.primitives import Articulation

world = World()
world.scene.add_default_ground_plane()

robot = Articulation(prim_path="/rebotarm_rs")
world.reset()

# get joint information
num_joints = robot.num_joints
joint_names = robot.get_dof_names()

Principle: Articulation internally calls PhysX's Articulation API to get/set all joint states in one go. It corresponds to MuJoCo's way of operating joints through the data.qpos and data.ctrl arrays, but wraps it in a Python object interface.

38.13 Practice Demos​

Demo 1: Loading the reBot Arm USD​

Principle: when Isaac Sim loads a USD file, it builds the Stage tree, and PhysX creates an articulated body for the Prim subtree with an Articulation Root. Visual meshes are linked to the rendering layer; meshes with a CollisionAPI are linked to the physics layer.

from isaacsim.core.api import World
from isaacsim.core.primitives import Articulation
import numpy as np

world = World(stage_units_in_meters=1.0)
world.scene.add_default_ground_plane() # ground

# add the workbench
from isaacsim.core.api.objects import FixedCuboid
table = FixedCuboid(
prim_path="/World/table", name="table",
position=np.array([0.5, 0.0, 0.4]),
scale=np.array([0.6, 0.6, 0.02]),
)

# add the task object
from isaacsim.core.api.objects import DynamicCuboid
cube = DynamicCuboid(
prim_path="/World/red_cube", name="red_cube",
position=np.array([0.5, 0.0, 0.42]),
scale=np.array([0.03, 0.03, 0.03]),
color=np.array([1.0, 0.0, 0.0]),
)

# load the arm (assuming the USD has been imported)
robot = Articulation(prim_path="/rebotarm_rs")
world.reset()

# verify the loading result
print("Number of joints:", robot.num_joints)
print("Joint names:", robot.get_dof_names())

Expected result: the 3D viewport shows the arm model standing on the ground workbench, with the red cube on the table. The Stage Tree shows the complete hierarchy from base_link to gripper_right.

Demo 2: Reading Joint States​

Principle: Articulation reads the articulated body's joint state arrays from PhysX every frame. Position and velocity are outputs of PhysX's internal solver, not read from external sensors—just like MuJoCo's data.qpos / data.qvel, they are simulation states.

world.step(render=True)  # first advance one physics frame

# joint positions (radians)
positions = robot.get_joint_positions()
print("Joint positions:", positions)

# joint velocities
velocities = robot.get_joint_velocities()
print("Joint velocities:", velocities)

# joint names and count
joint_names = robot.get_dof_names()
print("Joint names:", joint_names)
print("Number of joints:", robot.num_joints)

# end-effector pose (world frame)
ee_position, ee_orientation = robot.get_local_pose() # end link pose

Principle note: get_joint_positions() returns a NumPy array whose order matches get_dof_names(). The Articulation Root determines which joints belong to this articulated body; joints outside the articulated body cannot be read.

Demo 3: Joint Position Control​

Principle: after setting the Drive's target position, the PD controller inside PhysX computes the torque every frame and drives the joint. You only need to send the target once; the engine completes the arrival process itself. This differs from MuJoCo's physics mode, where Python computes PD torques every frame and writes them into data.ctrl—Isaac Sim puts the PD loop inside the engine.

# target pose (radians): zero all joints
target_positions = np.array([0.0, 0.0, 0.0, 0.0, 0.0, 0.0])

# Method 1: set the target through the Drive API
robot.set_joint_position_targets(target_positions)

# advance the simulation and let the PD controller drive to the target
for _ in range(100):
world.step(render=True)

# check whether it has arrived
current = robot.get_joint_positions()
error = np.abs(current[:6] - target_positions)
print("Arrival error:", error)

You can also send a non-zero target to move the arm to a specified pose:

wave_pose = np.array([0.0, 0.5, 1.0, 0.0, 0.5, 0.0])  # raise the arm and wave
robot.set_joint_position_targets(wave_pose)
for _ in range(200):
world.step(render=True)

Principle note: set_joint_position_targets only updates the Drive's target position property; it does not

apply force directly. The actual torque is determined by Stiffness and Damping, and the arrival speed depends on these two parameters and

Max Force.

Demo 4: Gripper Control​

Principle: the gripper's two prismatic joints (gripper_joint1 and gripper_joint2) have different strokes (0.05 m and 0.0715 m) but must move in sync. The principle is to map the same open/close ratio to the target positions of both joints simultaneously.

GRIPPER_LEFT_RANGE = 0.05      # gripper_joint1 stroke
GRIPPER_RIGHT_RANGE = 0.0715 # gripper_joint2 stroke

def set_gripper(robot, open_ratio: float):
"""open_ratio: 0=fully closed, 1=fully open"""
open_ratio = max(0.0, min(1.0, open_ratio))
left_target = open_ratio * GRIPPER_LEFT_RANGE
right_target = open_ratio * GRIPPER_RIGHT_RANGE

# assume the gripper joints come after the arm joints
joint_names = robot.get_dof_names()
arm_joints = 6 # the first 6 are arm joints

positions = robot.get_joint_positions()
positions[arm_joints] = left_target # gripper_joint1
positions[arm_joints + 1] = right_target # gripper_joint2
robot.set_joint_position_targets(positions)

for _ in range(50):
world.step(render=True)

# open the gripper
set_gripper(robot, 1.0)

# close the gripper
set_gripper(robot, 0.0)

# half open
set_gripper(robot, 0.5)

Principle note: here software linkage at the control level replaces the physics constraint. If the Mimic API is configured (Method 1 in 38.10), you only need to control one joint and the other follows automatically. The current example uses software synchronization, which is more intuitive and suitable for teaching.

Key points of two-finger synchronization

The left and right gripper strokes differ but the motion directions are the same (both open outward), so use the same open_ratio to scale

each stroke limit. If the two joints' axis directions were opposite (one positive and one negative), you would also need to negate,

but in the reBot Arm's URDF, both gripper joints have axis 0 0 1, so the directions are consistent.

38.14 Summary​

The core conceptual differences between Isaac Sim and MuJoCo:

  1. Model format: USD replaces MJCF, supporting layered references and overrides.
  2. Articulated body: the Articulation Root is an Isaac Sim-specific concept, handing the whole kinematic chain to the Featherstone algorithm for uniform solving. MuJoCo has no such concept; all bodies naturally live in one tree.
  3. Drive method: Drive is a PD controller built into the joint, computing torque inside PhysX. MuJoCo's <motor> actuator computes torque externally in Python and writes it into data.ctrl.
  4. Gripper linkage: Isaac Sim uses the Mimic API or software synchronization; MuJoCo uses the equality constraint.
  5. Collision annotation: USD uses the CollisionAPI to distinguish collision bodies from pure-visual bodies; MuJoCo uses the contype / conaffinity attributes.

Once you master these differences, the content on joint mapping, unit conversion, communication, and safety design in Chapter 39 can be directly applied to the Isaac Sim scene.


Loading Comments...