Skip to main content

Stage 8 · Chapter 39 · Practice

39. Synchronizing the Real and Simulated Arms

Chapter 39 of the Seeed Physical AI Beginner's Course — Real-to-Sim synchronization: mapping the real arm's joint states into MuJoCo in real time, DM and RS unit conversion, communication frequencies, UDP versus ROS2, state refresh and latency, gripper state synchronization, the safety design of the sync program, and two demo workflows.

Using the actual source code of the reBotArm-RS project as an example, this chapter explains how to synchronize the joint states of the real arm to the MuJoCo simulation environment in real time. All code references point to the real files in this repository and can be read side by side.

39.1 What is Real-to-Sim​

Real-to-Sim means transmitting the joint angles, velocities, torques, and other states of the real physical arm to the simulation environment in real time, so that the virtual arm reproduces the real arm's motion synchronously. It is the opposite direction of Sim-to-Real: Sim-to-Real trains policies in simulation and then deploys them to the real robot, while Real-to-Sim maps the real-robot state into the virtual model.

Typical uses of Real-to-Sim:

  1. Digital twin: observe the real arm's pose in real time on a web page without looking at the physical device.
  2. Recording and playback: record the real arm's motion as trajectory data and replay it repeatedly in simulation for debugging.
  3. Safety monitoring: the simulation environment can overlay capabilities the real arm lacks, such as collision detection and workspace visualization.
  4. Teaching reproduction: manually drag the real arm (gravity compensation mode) while the simulation model follows synchronously, used to collect teaching data.

In this project, the core chain of Real-to-Sim is:

Real RobStride motors → SocketCAN can0 → MotorBridge SDK state cache
→ HardwareManager._get_arm_state() → ROS JointState topic (60 Hz)
→ MuJoCo Sync node subscribes → MuJoCo qpos update → virtual arm moves

Key source files:

  • Hardware state reading and caching: hardware_manager.py
  • ROS joint state publishing: ros_publishers.py
  • MuJoCo sync node: mujoco_sync.py
  • Simulation-side fake driver: fake_rs_driver.py

39.2 DM and RS Joint Unit Conversion​

DM (Damiao motors) and RS (RobStride motors) both use radians for angle units, but the gripper units differ significantly—

this is an error-prone link in synchronization.

Arm joints​

The six arm joints of both DM and RS use radians, and the MuJoCo model also uses radians (<compiler angle="radian"/>),

so the arm joints need no unit conversion.

Gripper unit differences​

The gripper involves four different quantities with different units:

QuantityRangeUnitUse
RS gripper motor angle0-5radReal-robot SDK commands and feedback
Web/task gripper opening width0-0.0715mUser command semantics
ROS single-finger state0-0.045mVisual displacement after mapping by the state publisher
MuJoCo gripper displacement0-0.05mSimulation joint7 slide stroke

39.3 Communication Frequencies​

There are multiple links with different frequencies in the Real-to-Sim chain; understanding their relationships is the basis for troubleshooting latency and lag.

LinkFrequencyDescription
RS real-robot control loop125 HzThe MIT commands finally sent to the motors
Sync hardware feedback polling20 HzQuery RobStride states and refresh the cache
ROS joint state publishing60 HzPublish the JointState topic from the cache
MuJoCo simulation sync250 HzSimulation step frequency
Browser receiving MuJoCo statesUp to 25 Hzrosbridge subscription throttled to 40 ms
Browser renderingAbout 60 HzrequestAnimationFrame

Key points to understand:

  • The web page sends commands at up to 60 Hz, which does not mean the motors are only controlled at 60 Hz. After the RS controller receives a new target, it keeps generating and sending MIT commands with its own 125 Hz loop.
  • Hardware feedback refreshes the cache at 20 Hz, and ROS publishes from the cache at 60 Hz. The real-time MIT loop does not do synchronous CAN parameter queries.
  • MuJoCo steps at 250 Hz, but its input comes from the 60 Hz ROS topic, so MuJoCo keeps the last target between adjacent inputs.

39.4 UDP, Socket, or ROS2 Communication​

This project chooses ROS2 topics as the communication layer for Real-to-Sim, rather than UDP or raw Sockets. Understanding the reason for this choice helps make correct architecture decisions in other scenarios.

Why ROS2​

  1. Topic abstraction: sensor_msgs/JointState is a standard message type; publishers and subscribers do not need to agree on the data format.
  2. QoS policies: qos_profile_sensor_data provides BEST_EFFORT reliability and a small depth, suitable for high-frequency sensor data.
  3. Many-to-many communication: one joint-state topic can be subscribed by MuJoCo sync, the web page, logging, and multiple other nodes at once.
  4. Ecosystem integration: rosbridge can bridge ROS topics directly to WebSocket, so the web page needs no extra communication layer.

Topic topology​

/rebotarm/joint_states          ← published by the real-robot controller (60 Hz)
↓
MuJoCo Sync node subscribes
↓
/rebotarm/mujoco/joint_states ← published by the MuJoCo sync node (250 Hz)
↓
rosbridge WebSocket → browser

The MuJoCo sync node's subscription and publication are defined in mujoco_sync.py:

self.subscription = self.create_subscription(
JointState, input_topic, self._joint_state_callback, qos_profile_sensor_data,
)
self.publisher = self.create_publisher(
JointState, output_topic, qos_profile_sensor_data,
)

Namespace isolation​

The real robot and the simulation use different namespaces to avoid topic conflicts:

EnvironmentDefault namespaceLaunch script
Real robot/rebotarmscripts/start_rs_hardware.sh
Fake Driver + MuJoCo/rebotarm_rsscripts/start_rs_sim.sh
MuJoCo following the real robot/rebotarm (following)scripts/start_rs_mujoco_follow.sh

In the Real-to-Sim scenario, the MuJoCo sync node subscribes to the real robot's /rebotarm/joint_states, and its own

namespace is also set to rebotarm, but it only subscribes and never sends motor commands, so it does not conflict with the real-robot controller.

DDS discovery range​

rs_env.sh restricts the DDS discovery range to the local host, avoiding nodes losing each other after Wi-Fi roaming:

export ROS_AUTOMATIC_DISCOVERY_RANGE="${REBOTARM_ROS_DISCOVERY_RANGE:-LOCALHOST}"

Applicable scenarios of UDP vs ROS2​

FeatureROS2 topicsUDP
LatencyMillisecond-level, with DDS middleware overheadLowest, microsecond-level
ReliabilityConfigurable BEST_EFFORT / RELIABLEMust implement yourself
Multiple subscribersNatively supportedMust implement broadcasting yourself
Debugging toolsros2 topic echo / hzMust implement yourself
Applicable scenariosMulti-node collaboration, needs the ecosystemPoint-to-point ultra-low latency

This project's latency requirements (60 Hz states, human-eye-acceptable) are far from needing UDP; ROS2 topics are the most natural choice.

39.5 State Refresh and Latency​

Separating the async cache from the feedback frequency​

hardware_manager.py is designed around separating the hardware feedback polling frequency from the

ROS publish frequency:

# JointStatePublisher in ros_publishers.py
period = 1.0 / max(float(rate_hz), 1.0) # publish at 60 Hz
self._feedback_poll_period = 1.0 / max(float(feedback_poll_rate_hz), 1.0) # feedback at 20 Hz

def publish(self) -> None:
now = time.monotonic()
request_feedback = now - self._last_feedback_poll >= self._feedback_poll_period
if request_feedback:
self._last_feedback_poll = now
pos, vel, effort = self._hardware.get_joint_state(request_feedback=request_feedback)

Among the 60 Hz publish frames, one third (20 Hz) triggers a synchronous CAN read, and the remaining frames return directly from the cache. This both keeps the ROS topic refresh rate high and prevents the CAN bus from being occupied by feedback polling.

Stale timeout on the MuJoCo side​

The MuJoCo sync node has a stale_timeout parameter (default 1.0 second). If no new JointState message is received within this time, the simulation stops updating:

def _update(self) -> None:
if self.last_input_time == 0.0:
return
if (self.stale_timeout > 0.0
and time.monotonic() - self.last_input_time > self.stale_timeout):
return

This prevents the simulation from continuing to move with stale data after the real robot disconnects.

Latency layering and troubleshooting​

When synchronization lags or is not responsive, measure layer by layer along the chain rather than tuning a single parameter:

  1. Real-robot feedback layer: use ros2 topic hz /rebotarm/joint_states to confirm it is stably at 60 Hz.
  2. MuJoCo sync layer: confirm whether last_input_time keeps updating.
  3. Web reception layer: the rosbridge subscription throttle may keep the browser side below 25 Hz.
  4. Display interpolation layer: the browser interpolates 32-120 ms between adjacent measurements.

For the detailed data flow and troubleshooting methods, see DATA_FLOW_RS_ZH.md.

39.6 Gripper State Synchronization​

Gripper synchronization is more complex than the arm joints, because it involves unit conversion and MuJoCo's equality-constraint linkage.

MuJoCo gripper model​

In rs_arm.xml, the gripper consists of three joints:

<joint name="joint7" type="slide" axis="0 1 0" range="0 0.05"/>
<joint name="joint_left" type="slide" .../>
<joint name="joint_right" type="slide" .../>

<equality>
<joint joint1="joint7" joint2="joint_left" polycoef="0 1 0 0 0"/>
<joint joint1="joint7" joint2="joint_right" polycoef="0 1 0 0 0"/>
</equality>

joint7 is the driving joint, and joint_left and joint_right follow it 1:1 through the equality constraint. When syncing, you only need to set joint7's qpos; the left and right fingers follow automatically.

Sync code​

When the MuJoCo sync node receives a JointState message, it first converts the gripper units, then sets the qpos of the three joints during the update:

def _joint_state_callback(self, msg: JointState) -> None:
if "gripper_joint1" in values:
self.target_gripper = self._visual_to_mujoco_gripper(
values["gripper_joint1"], _RS_ROS_VISUAL_OPEN_M
)

def _update_kinematic(self) -> None:
self.data.qpos[self.gripper_qpos_addr] = next_gripper # joint7
self.data.qpos[self.left_qpos_addr] = next_gripper # joint_left
self.data.qpos[self.right_qpos_addr] = next_gripper # joint_right

Note: in kinematic mode, the three joints are written with the same value directly; in physics mode, only joint7_motor is driven, and the left/right fingers follow automatically through the equality constraint.

39.7 Safety Design of the Synchronization Program​

Hardware confirmation gate​

start_rs_hardware.sh requires explicit confirmation before starting the real-robot controller, to prevent accidental operation from moving the arm:

if [[ "${REBOTARM_RS_HARDWARE_CONFIRM:-}" != "I_UNDERSTAND_RS_WILL_MOVE" ]]; then
echo "Hardware launch blocked." >&2
exit 2
fi

But the MuJoCo follow script start_rs_mujoco_follow.sh does not need this confirmation, because it only subscribes to the real-robot topics and does not send motor commands or open SocketCAN:

Process mutex lock​

start_rs_hardware.sh uses flock for process mutex on hardware launch, preventing two controllers from competing for the motors at the same time:

exec 9>"${REBOTARM_HARDWARE_LOCK}"
if ! flock -n 9; then
# identify and safely terminate the previous launch
stop_processes "the previous RS hardware launch" "${REBOTARM_LOCK_HOLDERS[@]}"
fi

It can also recognize controllers paused with Ctrl+Z, send SIGCONT first and then SIGINT, and finally clean up leftover Fast DDS shared memory.

State machine arbitration​

hardware_manager.py uses a state machine to reject unsafe commands:

def _begin_lowlevel_streaming(self, required_mode: str) -> None:
if not self._enabled:
raise RuntimeError("rejecting low-level command while arm is disabled")
if self._gravity_comp_active or self.state_machine == "GRAVITY_COMP":
raise RuntimeError("rejecting low-level command during gravity compensation")
if self.state_machine == "SAFE_HOMING":
raise RuntimeError("rejecting low-level command during safe home")

The states include: IDLE, LOWLEVEL_STREAMING, TRAJ_RUNNING, GRAVITY_COMP, SAFE_HOMING. Each state accepts only specific command types and rejects everything else.

Safe homing​

Before disabling, if the arm is not near the zero pose (any joint's absolute angle exceeds 2 degrees, or velocity exceeds 0.15 rad/s), the controller first enters the SAFE_HOMING state: clears old targets, closes the gripper, performs homing, verifies arrival, and only then disables the motors. For the detailed flow, see Section 5 of DATA_FLOW_RS_ZH.md.


39.8 Practice Demos​

Demo 1: Synchronizing the Real Arm to MuJoCo​

Overall chain​

Real reBot Arm (RobStride motors)
↓ CAN bus
Python SDK (motorbridge + reBotArm_control_py)
↓ read encoder feedback
ROS controller (rebotarmcontroller)
↓ publish JointState topics
MuJoCo sync node (mujoco_sync.py)
↓ kinematics mode directly writes qpos
MuJoCo virtual arm

DEMO launch​

The 6 RobStride motors (joints 1–6) and 1 gripper motor on the arm continuously report their encoder states (position, velocity, torque, status codes) over the SocketCAN can0 bus at 1 Mbps. This layer is pure hardware and involves no software.

Before launching, configure the CAN interface:

sudo ip link set can0 down 2>/dev/null || true
sudo ip link set can0 type can bitrate 1000000
sudo ip link set can0 up

Launch the real-robot controller:

# Terminal 1: real-robot controller
REBOTARM_RS_HARDWARE_CONFIRM=I_UNDERSTAND_RS_WILL_MOVE ./rebotarm start rs

# Terminal 2: MuJoCo follow (same as Demo 1)
./scripts/start_rs_mujoco_follow.sh

# Terminal 3: web page
./rebotarm start web

Demo 2: Gravity-Compensation Manual Teaching Synchronization​

Overall chain​

Click "Start gravity comp" on the web page
↓ rosbridge → ROS Service
The real-robot controller enters gravity compensation mode (GRAVITY_COMP)
↓ Pinocchio computes gravity torques + low-gain MIT holding
The user manually drags the real arm
↓ motor encoders report new angles
The controller publishes JointState (60 Hz, same as normal motion)
↓
The MuJoCo follow node subscribes → the virtual arm reproduces in real time
Meanwhile the web 3D model also displays the feedback in real time

Key difference from Demo 1: the real robot is no longer passively driven by position targets; it enters gravity compensation mode—the user drags the real arm by hand, the encoder feedback keeps changing, JointState is published as usual, and both MuJoCo and the web page follow. The MuJoCo follow part fully reuses Demo 1's script and needs no extra configuration.

Step 1: Web operation — start gravity compensation​

Prerequisites​

Three terminals, respectively launching the real robot, MuJoCo follow, and the web page:

# Terminal 1: real-robot controller
REBOTARM_RS_HARDWARE_CONFIRM=I_UNDERSTAND_RS_WILL_MOVE ./rebotarm start rs

# Terminal 2: MuJoCo follow (same as Demo 1)
./scripts/start_rs_mujoco_follow.sh

# Terminal 3: web page
./rebotarm start web

Open http://localhost:3002 in the browser, and follow these steps:

  1. Select the namespace: choose "RS real robot (/rebotarm)" as the control target;
  2. Connect: fill the ROS WebSocket with ws://localhost:9090 and click connect;
  3. Open the control lock: check the control lock checkbox;
  4. Enable: click the "Enable" button and wait until the status shows enabled;
  5. Start gravity comp: click the "Start gravity comp" button.

Step 2: The real-robot controller enters gravity compensation​

Several key design points:

  • Gain smooth transition: use smoothstep to gradually transition within transition_duration (default 0.5 s) from the stiff gains [80,150,150,50,50,50] / [5,10,10,5,4,4] to the compliant gains kp=2.0 / kd=1.0 (RS config). smoothstep has zero derivatives at both ends, avoiding an abrupt stiffness drop at the switch instant.
  • Target follows the measured angle: q_target is smoothly interpolated from the holding angle at startup to the real-time measured angle. After the transition completes, q_target = q, i.e., the target always equals the current angle—wherever the user drags, the arm follows.
  • Gravity feedforward: every cycle, recompute compute_generalized_gravity with the cached angles (no CAN read) and add it to the MIT torque. The motors only need to output a tiny position-error force; the tau mainly cancels gravity.
  • Cache instead of real-time CAN reads: _read_gravity_comp_positions(request=False) takes angles from the 20 Hz-refreshed cache; the 125 Hz loop does no synchronous CAN parameter queries, avoiding blocking.
Safety rules during gravity compensation​

While the state machine is in GRAVITY_COMP, the controller rejects all web joint commands, TCP dragging, trajectory playback, and gripper commands. Only the "Stop gravity comp" button and disable requests can interrupt it.


Complete data flow​

User clicks "Start gravity compensation" on the web page
→ rosbridge WebSocket
→ /rebotarm/gravity_compensation/start service
→ HardwareManager.start_gravity_compensation()
→ per-joint switch to MIT + gravity feedforward
→ 125 Hz compliant control loop
The user manually drags the real robot
→ encoder feedback → SocketCAN → state cache
→ /rebotarm/joint_states (60 Hz)
→ web mirror (Three.js model follows)
→ MuJoCo Sync (virtual arm follows)
MuJoCo virtual arm + web 3D model + real arm reproduced in real time​

39.9 Summary​

The core of Real-to-Sim synchronization is passing the real-robot joint states to the simulation environment at an appropriate frequency and format. The practical points of this project

are:

  1. Map joints by name, not by array order.
  2. The gripper involves four units; every step of the conversion chain must be clear.
  3. Separate the hardware feedback polling frequency from the ROS publish frequency; do not do synchronous CAN reads in the real-time loop.
  4. ROS2 topics beat UDP in this scenario; the benefits of the ecosystem and debugging tools outweigh the microsecond-level latency difference.
  5. Safety design runs through the whole chain: hardware confirmation gate, process mutex lock, state machine arbitration, safe homing.
  6. Gravity-compensation teaching is a high-value Real-to-Sim scenario: low stiffness + gravity feedforward + target following the feedback

updates are the key design.

39.10 FAQ​


Loading Comments...