Skip to main content
Stage 3 · Chapter 12 · Practice

12. Camera Configuration and LeRobot Data Collection

Chapter 12 of the SO-ARM Physical AI Beginner's Course — connect and verify front and side cameras, understand image/action synchronization, then record your first LeRobot dataset with lerobot-record and manage episodes with the keyboard controls.

⚡ No-code · No environment setup

Skip the setup — run the reBot Arm and LeRobot from one app

SenseCraft Robotics is Seeed's no-code platform for the SO-ARM101, reBot Arm 102 + B601-RS and B601-DM. Connect the arms, calibrate, collect demonstrations, train and run inference from a guided interface — no Python environment, no terminal.

  • ✅ 6-step guided workflow
  • ✅ Cloud training — no local GPU
  • ✅ Windows / macOS client
  • ✅ SO-ARM101 · B601-RS · B601-DM
⚠️
Safety check before running

Clear valuable items and unrelated people within 1 meter of the robotic arm workspace. Make sure the arm is firmly mounted and that power and cables are connected properly before running this chapter.

12.1 Single-Camera vs. Dual-Camera Setup​

Layout

12.1 Single-Camera vs. Dual-Camera Setup

Two cameras and two views are required for data collection and model training in this course. Depending on the mounting position, the common layouts are:

LayoutInstallation and purposeSuitable scenarios
Gripper viewTop-view camera mounted above the front of the workbench to cover the work area; gripper camera mounted near the gripper to observe grasping detailsFine operations that require observing contact between the gripper and the object
Side-view assistanceTop-view camera mounted above the front of the workbench; side-view camera mounted at the front side of the workbench to observe arm height and gripper motionTasks such as grasping, handling, and placing
Side-view assistance camera layout

This course uses the side-view assistance layout (a front camera plus a side camera), which is also the layout used by the Chapter 22 no-code workflow.

12.2 Finding Camera Device Names​

Detect

12.2 Finding Camera Device Names

A camera's index can change if you reboot or re-plug — a behavior mostly dependent on your operating system. Before every recording session, detect the cameras plugged into your system:

lerobot-find-cameras opencv

The terminal prints something like:

--- Detected Cameras ---
Camera #0:
Name: OpenCV Camera @ 0
Type: OpenCV
Id: 0
Backend api: AVFOUNDATION
Default stream profile:
Width: 1920
Height: 1080
Fps: 15.0
--------------------
(more cameras ...)

You can find the pictures taken by each camera in the outputs/captured_images directory — open them to confirm which index is your front camera and which is the side camera.

tip

Avoid connecting USB cameras through a hub. Connect them directly, preferably to USB 3.0 ports, to ensure sufficient image transmission bandwidth.

12.3 Verify Cameras While Teleoperating​

Preview

12.3 Verify Cameras While Teleoperating

Before recording, confirm both views are live and framed correctly by teleoperating with camera display enabled:

lerobot-teleoperate \
--robot.type=so101_follower \
--robot.port=/dev/ttyACM0 \
--robot.id=my_awesome_follower_arm \
--robot.cameras="{ front: {type: opencv, index_or_path: 0, width: 640, height: 480, fps: 30, fourcc: "MJPG"}, side: {type: opencv, index_or_path: 2, width: 640, height: 480, fps: 30, fourcc: "MJPG"}}" \
--teleop.type=so101_leader \
--teleop.port=/dev/ttyACM1 \
--teleop.id=my_awesome_leader_arm \
--display_data=true

The index_or_path values come from the last digit of each camera ID reported by lerobot-find-cameras opencv.

tip

fourcc: "MJPG" requests compressed frames. Under MJPG this setup supports 3 cameras at 1920×1080 @ 30FPS. YUYV is uncompressed — it lowers usable resolution and FPS and can lag the arm. Do not connect two cameras through the same USB hub.

12.4 Optional: Depth Cameras (RealSense / Orbbec)​

Optional

12.4 Optional: Depth Cameras (RealSense / Orbbec)

RealSense depth cameras provide RGB-D perception for tasks such as object recognition and close-range manipulation. The recommended models are D405 (short-range stereo depth, 7-50 cm working range, ideal for tabletop manipulation) and D435i (depth + RGB + IMU).

1. Switch to the camera branch — depth camera support lives on DepthCameraSupport:

git checkout DepthCameraSupport
git pull origin DepthCameraSupport
git branch --show-current # expect: DepthCameraSupport

2. Install the RealSense extra in editable mode:

pip install -e ".[realsense]"

3. Grant camera permissions and detect:

chmod a+rw /dev/bus/usb/*/*
lerobot-find-cameras realsense

4. Example: teleoperate with a D435i color+depth pair (use the serial number from the detection output in serial_number_or_name):

lerobot-teleoperate \
--robot.type=so101_follower \
--robot.port=/dev/ttyACM0 \
--robot.id=my_awesome_follower_arm \
--robot.cameras='{
d435i_color: {
type: realsense_d435i_color,
serial_number_or_name: "419522072950",
width: 640, height: 480, fps: 30,
color_mode: rgb, color_stream_format: rgb8,
rotation: 0, warmup_s: 1
},
d435i_depth: {
type: realsense_d435i_depth,
serial_number_or_name: "419522072950",
width: 640, height: 480, fps: 30,
max_depth_m: 2.0, depth_alpha: 0.2,
rotation: 0, warmup_s: 5
}
}' \
--teleop.type=so101_leader \
--teleop.port=/dev/ttyACM1 \
--teleop.id=my_awesome_leader_arm \
--display_data=true

Parameter notes: depth_alpha scales the depth image (start at 0.2); with 3+ depth cameras reduce fps to 15; keep 640×480 for stability.

12.5 Image and Action Synchronization​

Sync

12.5 Image and Action Synchronization

During recording, LeRobot runs one control loop per frame:

  • read both cameras (front, side);
  • read leader joints → actions;
  • read follower joints → state;
  • timestamp everything and append one row.

Because cameras deliver frames on their own schedule, the loop aligns by timestamp, not by wish: each dataset row pairs the freshest camera images with the joint data from the same instant. This is why --dataset.fps should not exceed what your cameras can stably deliver (30 fps at 640×480 MJPG is the safe choice).

12.6 Recording Your First Dataset​

Record

12.6 Recording Your First Dataset

Record the Chapter 11 task (pick-and-place A to B) locally — the dataset stays on your machine:

lerobot-record \
--robot.type=so101_follower \
--robot.port=/dev/ttyACM0 \
--robot.id=my_awesome_follower_arm \
--robot.cameras="{ front: {type: opencv, index_or_path: 0, width: 640, height: 480, fps: 30, fourcc: "MJPG"}, side: {type: opencv, index_or_path: 2, width: 640, height: 480, fps: 30, fourcc: "MJPG"}}" \
--teleop.type=so101_leader \
--teleop.port=/dev/ttyACM1 \
--teleop.id=my_awesome_leader_arm \
--display_data=true \
--dataset.repo_id=seeedstudio123/test \
--dataset.num_episodes=5 \
--dataset.single_task="Grab the black cube" \
--dataset.push_to_hub=false \
--dataset.episode_time_s=30 \
--dataset.reset_time_s=30

repo_id can be customized; with push_to_hub=false the dataset lands in ~/.cache/huggingface/lerobot/seeedstudio123/test/.

Recording Parameters​

ParameterDescriptionDefault
--dataset.episode_time_sDuration per data episode (seconds)60
--dataset.reset_time_sEnvironment reset time after each episode (seconds)60
--dataset.num_episodesTotal episodes to record50

Keyboard Controls During Recording​

KeyAction
→ (Right Arrow)Early-stop current episode/reset; move to next
← (Left Arrow)Cancel current episode; re-record it
ESCStop session immediately, encode videos, and save the dataset
tip

If the keyboard shortcuts do not respond, first check that $DISPLAY is set, or downgrade pynput: pip install pynput==1.6.8

While recording you will see streaming stats like:

INFO ol_robot.py:219 dt:33.34 (30.0hz) dtRlead: 5.06 (197.5hz) dtWfoll: 0.25 (3963.7hz) dtRfoll: 6.22 (160.7hz) dtRlaptop: 32.57 (30.7hz) dtRphone: 33.84 (29.5hz)

dt near 33 ms means the loop holds 30 Hz — that's a healthy session.

Checkpointing and Resuming​

  • Checkpoints are created automatically during recording.
  • To resume after an interruption, re-run the same command with --resume=true.
  • --dataset.num_episodes then counts the episodes to record THIS session, not the grand total — 15 recorded of a 50 target → set 35.
  • To start over from scratch, delete the dataset directory manually.

Recording on the Hugging Face Hub (Optional)​

Log in once with a write-access token from HF settings:

huggingface-cli login --token ${HUGGINGFACE_TOKEN} --add-to-git-credential
HF_USER=$(huggingface-cli whoami | head -n 1)

Then set --dataset.repo_id=${HF_USER}/record-test and --dataset.push_to_hub=true to publish the dataset.

12.7 Tips for Gathering Good Data​

Quality

12.7 Tips for Gathering Good Data

  • Task: grasp objects at different marked points and place them at Point B (Chapter 11's cross pattern).
  • Scale: record ≥50 episodes (10 episodes per point).
  • Consistency:
    • Keep cameras fixed;
    • Maintain identical grasping behavior;
    • Ensure the manipulated object is visible in both camera feeds.
  • Progression: start with reliable grasping before adding variations (new positions, techniques, camera adjustments). Avoid rapid complexity increases.
  • Environment: keep camera positions, angles, and ambient lighting stable; avoid unstable backgrounds or people walking through the camera view — large differences between recording and deployment environments cause policies to fail.

💡 Rule of thumb: you should be able to do the task yourself by only looking at the camera images. If you can't, the model can't either.

Set --dataset.num_episodes high enough before starting, and don't stop midway unless necessary — dataset statistics (mean and variance) are computed after collection finishes and are required for training.

Loading Comments...