Skip to main content
Stage 4 · Chapter 20 · Practice

20. Preparing the SO-ARM VLA Dataset

Chapter 20 of the SO-ARM Physical AI Beginner's Course — turn a Stage-3 LeRobot dataset into a GR00T-ready VLA dataset: language annotations, meta/modality.json, the new_embodiment tag and so100_dualcam config, dimension checks, and multi-task organization.

⚡ No-code · No environment setup

Skip the setup — run the reBot Arm and LeRobot from one app

SenseCraft Robotics is Seeed's no-code platform for the SO-ARM101, reBot Arm 102 + B601-RS and B601-DM. Connect the arms, calibrate, collect demonstrations, train and run inference from a guided interface — no Python environment, no terminal.

  • ✅ 6-step guided workflow
  • ✅ Cloud training — no local GPU
  • ✅ Windows / macOS client
  • ✅ SO-ARM101 · B601-RS · B601-DM

20.1 Prerequisites​

Prerequisites

20.1 Prerequisites

You need:

  • A clean Stage-3 dataset recorded on the SO-ARM (Chapters 11-13): two camera views (front + side), 50+ episodes, one task per episode, quality-checked;
  • The Isaac-GR00T repository cloned on your training machine (Chapter 21 installs the full environment — this chapter only edits dataset files);
  • The official recipe for reference: Fine-tune GR00T N1.5 on SO101.
tip

Your existing ACT dataset is the raw material — GR00T reuses the same LeRobot episodes. This chapter only adds the language and modality metadata.

20.2 Checking the LeRobot Dataset​

Check

20.2 Checking the LeRobot Dataset

Dataset Directory Structure​

~/.cache/huggingface/lerobot/seeedstudio123/test/
├── meta/
│ ├── info.json ← fps, features, camera keys, robot info
│ ├── tasks.jsonl ← task descriptions (edit here!)
│ ├── episodes/... ← per-episode metadata
│ └── stats/... ← normalization statistics
├── data/ ← parquet frames
└── videos/ ← camera streams

Quick Check with Python​

from lerobot.common.datasets.lerobot_dataset import LeRobotDataset

ds = LeRobotDataset("seeedstudio123/test", root="~/.cache/huggingface/lerobot")
print(ds.meta.info) # fps, features
print(ds[0]["observation.state"].shape) # expect torch.Size([6])
print(ds[0]["action"].shape) # expect torch.Size([6])

Required Checklist​

  • observation.state and action are both 6-dim (5 joints + gripper);
  • Exactly two camera features, e.g. observation.images.front / observation.images.side;
  • Every episode belongs to one task with a meaningful description;
  • No known broken episodes left in the set (Chapter 13 cleanup).

20.3 Adding Language Task Descriptions​

Language

20.3 Adding Language Task Descriptions

If you record a new dataset for Stage 4, bind the instruction at record time with the same --dataset.single_task you already use:

--dataset.single_task="Pick up the block at point A and place it at point B"

One short, verb-first sentence per task — it flows into the dataset's task metadata automatically.

Method B: Backfill meta/tasks.jsonl​

For an existing dataset, edit meta/tasks.jsonl so every task index maps to a proper instruction sentence. Keep the mapping consistent: the model will learn these exact strings.

Language Annotation Guidelines​

  1. One task = one fixed sentence; the same task never appears with two phrasings;
  2. Verb-first and concrete: "Put the block into the box" beats "block handling";
  3. English or Chinese both work — GR00T's VLM handles both — but don't mix languages within one task.

20.4 Creating meta/modality.json​

Modality

20.4 Creating meta/modality.json

modality.json tells GR00T which dataset fields feed which model inputs. The SO-ARM's standard two-camera layout matches the official so100_dualcam data config; a minimal equivalent for a local dataset looks like this:

{
"state": {
"single_arm": [0, 5],
"gripper": [5, 6]
},
"action": {
"single_arm": [0, 5],
"gripper": [5, 6]
},
"video": {
"front": "observation.images.front",
"side": "observation.images.side"
},
"annotation": {
"human.task_description": "task_description"
}
}

Field Description​

FieldMeaning
state.single_armSlice [start, end) of observation.state for the 5 arm joints
state.gripperSlice for the gripper dim
action.*Same slicing on the action vector
videoCamera key → dataset feature name (must match recording keys exactly)
annotation.human.task_descriptionWhere the language instruction comes from (Chapter 18's recommended key)
note

The so100_dualcam config in the Isaac-GR00T repo is the canonical version of this file — if your layout matches the standard (two cameras, 6-dim state/action), prefer passing --data-config so100_dualcam at training time over hand-maintaining a copy.

20.5 Setting the Embodiment Tag​

Embodiment

20.5 Setting the Embodiment Tag

The SO-ARM fine-tunes as a new embodiment: tag new_embodiment. You rarely write it into the dataset itself — it is a training/inference argument (Chapter 21: --embodiment-tag new_embodiment on the inference service, and the SO101 fine-tuning recipe sets it during training).

What matters at dataset time is that the data config matches reality: two cameras and 6-dim state/action, as verified in 20.2.

20.6 Checking Joint Order and Data Dimensions​

Verify

20.6 Checking Joint Order and Data Dimensions

Step 1: Print dataset meta​

Confirm the feature list and dims (see 20.2's Python snippet): 6/6 for state/action, two image features.

Step 2: Verify modality slicing​

If you wrote a custom modality.json, the slices must cover [0,6) exactly, with no gaps or overlaps.

Step 3: Visualize the data​

lerobot-dataset-viz \
--repo-id seeedstudio123/test \
--mode local \
--episode-index 0

Check that: images are the right cameras, gripper dim actually opens/closes during grasp, joints move in a plausible order.

Step 4: Statistical checks​

Sanity-check meta/stats: state min/max should sit inside the calibrated joint ranges; images' mean brightness shouldn't be near 0 or 255 (black or blown-out recordings).

20.7 Multi-Task Dataset Organization​

Multi-task

20.7 Multi-Task Dataset Organization

Record several tasks into one dataset; each episode stores its task_index, and tasks.jsonl maps each index to its instruction sentence. This is the natural shape for language-conditioned fine-tuning.

Method B: Merging multiple datasets​

Merge per-task datasets with the Chapter 13 toolbox (--operation.type merge). Requirements for a valid merge: identical camera configuration, identical robot/feature layout, and distinct, consistent task sentences per source dataset.

Data Volume Recommendations​

SetupEpisodesNotes
Single task, fixed A-to-B~50Sanity fine-tune
Single task, varied positions50-100The Stage-3 default
Multi-task (3-5 tasks)50-100 per taskLanguage conditioning needs per-task coverage

20.8 Data Quality Checklist​

Checklist

20.8 Data Quality Checklist

  • Every episode has a correct, single instruction sentence;
  • Camera keys in modality.json match the dataset features character-for-character;
  • state / action are 6-dim and correctly sliced (single_arm / gripper);
  • Failed and outlier episodes deleted (Chapter 13);
  • Statistics present (meta/stats) — never train on a dataset whose recording session was killed midway;
  • A copy of the final dataset backed up before Chapter 21 starts editing anything.

Dataset ready — next chapter fine-tunes GR00T on it.

Loading Comments...