Skip to main content
Stage 4 · Chapter 22 · Practice

22. No-Code VLA with SenseCraft Robotics

Chapter 22 of the SO-ARM Physical AI Beginner's Course — the no-code VLA path: connect and calibrate the arms in SenseCraft Robotics, verify teleoperation, bind cameras, collect and clean datasets, train in the cloud or locally, and run inference — all without a terminal or a training GPU.

Who this chapter is forEveryone — but especially readers without a training GPU.Same task as Chapter 11 (pick at A, place at B), same theory — no Python required.A guided 6-step app workflow replaces the terminal.
⚡ No-code · No environment setup

Skip the setup — run the reBot Arm and LeRobot from one app

SenseCraft Robotics is Seeed's no-code platform for the SO-ARM101, reBot Arm 102 + B601-RS and B601-DM. Connect the arms, calibrate, collect demonstrations, train and run inference from a guided interface — no Python environment, no terminal.

  • ✅ 6-step guided workflow
  • ✅ Cloud training — no local GPU
  • ✅ Windows / macOS client
  • ✅ SO-ARM101 · B601-RS · B601-DM
tip

SenseCraft Robotics is Seeed's no-code platform for the SO-ARM101 (and the reBot arms). Connect the arms, calibrate, collect demonstrations, train and run inference from a guided interface — no Python environment, no terminal. This chapter is the GUI counterpart of everything you did in Stages 3-4.

22.1 Preparation​

Prepare

22.1 Preparation

Hardware​

SO-ARM101 Pro hardware list

ItemLeaderFollower
ArmBlack assembled Leader arm ×1White assembled Follower arm ×1
LeRobot servo control board×1×1
Power cable5V power cable ×1Pro: 12V ×1; Standard: 5V
Data cableUSB-C ×1USB-C ×1
Mounting clamp×2×2

Shared: flexible gripper parts, two 32 × 32 mm USB cameras (the kit includes one; prepare a second separately — training data must contain two views), screwdriver, mouse mat.

The arms must be assembled, mounted, powered, and connected by USB. If assembly is not complete, return to Chapter 6.

Computer and software​

  • Windows or macOS computer; local training requires a compatible GPU;
  • Stable network for downloads, login, cloud training, and inference;
  • SenseCraft Robotics installed, and a registered SenseCraft account signed in.

Scene and safety​

  • Mark two fixed positions on the table: Point A for the object's start, Point B for its destination;
  • Prepare an easy-to-grasp object (a red block or soft object);
  • Make sure Point A, Point B, both arms, and the object are visible in the camera views and unobstructed;
  • Clear the workspace of people, clutter, cables, and fragile objects. Keep the Leader away from the Follower and out of the Follower's camera view.
Task scene and safety example
note

Interface names, button locations, and training backends may change with SenseCraft Robotics versions. Serial ports and dataset names shown here are examples — always use the devices your computer detects.

22.2 Connect the Arms​

Connect

22.2 Connect the Arms

warning

Safety notice: disconnect power before installing, connecting, or removing the arms. Confirm the arms are secure, the cables are correct, and the workspace is clear before restoring power. Never connect or disconnect power while powered.

Install the arm bodies. Place the Leader and Follower on a stable table; secure each with two clamps; keep a safe distance between arms; with power off, move each joint by hand to confirm smooth motion without collisions.

Install the arm bodies

Install the control boards. One LeRobot servo control board per arm: align with the base slot, check connector orientation, seat it securely; verify every servo cable is fully home and not sharply bent or pinched.

Connect the data cables. Leader → USB-C → computer; Follower → USB-C → computer. For easier serial identification, connect the arm ends first and plug the computer ends one at a time during binding (22.3).

Install the control boards

Install the power interfaces and power on. With adapters unplugged from AC: insert each DC cable, tighten the locking collar; Pro = Leader 5V / Follower 12V, Standard = both 5V — do not mix; route cables clear of joint motion. Then connect power, watch the board indicators, and confirm both USB-C (data) and DC (power) are attached.

Install the power interfaces

22.3 Device Setup in the App​

Device setup

22.3 Device Setup in the App

After signing in, open Projects → New Project, enter a name and description, and create it. The project overview gives access to device setup, action replay, datasets, training, models, and operation; if it shows "To be configured" or "Not connected", click Go to Device Setup.

Create a project

Select the device model​

In Device Pairing, select SO-ARM101 + SO-ARM101, then click Next.

Select SO-ARM101 + SO-ARM101

Bind the USB serial ports​

  1. Initial scan: disconnect both USB cables, click Rescan, note the ports shown;
  2. Bind the Leader: connect the Leader, Rescan, bind the newly appearing port to the Leader;
  3. Bind the Follower: connect the Follower, Rescan, bind the new port to the Follower;
  4. Both arms show Connected → Next.

Bind the Leader and Follower serial ports

tip

Serial-port troubleshooting: after each scan, bind only the newly appearing port — never identify devices by COM number alone. If a port is missing, reconnect the USB cable and scan again; if only one port appears, check the other cable and the arm's power.

Arm calibration verification​

Move the Leader and Follower to the middle posture shown on screen and clear the workspace. Two modes:

  • Automatic Calibration — the system identifies each joint's travel range by driving the arm. Requires all joints to have reliable physical stops. Remove loads, align both arms roughly vertical, tick the confirmation checkbox, click Start Calibration, and wait.
  • Manual Calibration — for joints without reliable stops, or to verify step by step: keep the Leader powered, move its joints to mid-range, click Start Calibration, and follow the on-screen guidance for each joint of both arms.

Do not teleoperate or collect data during calibration. If the posture looks abnormal, a joint is obstructed, or calibration fails — stop, check the arm and workspace, and retry.

Teleoperation verification​

  1. Click Start Teleoperation;
  2. Move the Leader slightly — the Follower must follow synchronously, in the same direction, smoothly;
  3. Click End Teleoperation, then Confirm Teleoperation Normal (or Abnormal, Return to Recalibrate).

Teleoperation verification

tip

Gravity compensation (optional): the arms have some weight, so hand-adjusting the Follower takes effort. Gravity compensation offsets part of the weight to make adjustment easier — turn it off after adjustment and before teleoperation verification. It assists manual movement only; it does not make the Follower follow the Leader.

Bind the cameras​

Two cameras and two views are required. Common layouts (Chapter 12 discussed the same choice): gripper view (top camera + gripper camera, for fine contact-sensitive operations) or side-view assistance (top camera + side camera, for grasping/handling/placing — what this course uses).

  1. Connect both cameras, click Rescan;
  2. Assign the streams to Front Camera and Side Camera;
  3. Check both previews: arms, object, and target position clearly visible → Next.

Bind the front and side cameras

22.4 Action Replay (Optional Warm-Up)​

Replay

22.4 Action Replay (Optional Warm-Up)

Action Replay records arm motions through Leader teaching and saves them to an action list for replay — a handy way to verify the chain before committing to a dataset:

FunctionOperationPurpose
Record an actionClick + → teach with the Leader → Stop RecordingRecord grasp / move / place actions
Replay an actionClick ReplayCheck continuity, direction, gripper open/close

Action list and replay

22.5 Dataset: Configure, Record, Clean​

Dataset

22.5 Dataset: Configure, Record, Clean

A small-batch, multi-session approach is recommended, exactly as Chapter 11 planned: ~10 episodes per batch; after 2-3 batches keep ~20-30 valid episodes for the first training; add data for complex variants later.

Configure a data-collection task​

Open Dataset → Collect Data and enter the task information:

FieldExampleGuidance
Dataset nameSO-ARM101 pick-and-place A-to-B-01"device + task + batch" naming
Task descriptionMove the object from the left to the rightState the goal clearly; descriptions must match exactly when merging
Number of episodes10Each episode completes one full task
Duration per episode20-30 secondsCover the complete action
Rest duration5 secondsReset arms and scene

Configure a data-collection task

Record task episodes​

Each episode records the complete grasp at A → move → release at B flow. Keep the procedure consistent; add small position/angle variations only when more generalization is needed.

  1. Place the object at Point A, confirm the initial posture, click Start Recording;
  2. Teach the task with the Leader, then return the arm to the initial posture;
  3. Wait out the remaining time or click ➡ (or press Space) to end the episode early;
  4. During the rest period, return the object to Point A and prepare the next episode.

Record task episodes

note

Important:

  • Secure the cameras; arms, gripper, object, and Points A and B must stay visible in both views;
  • Don't let key actions be blocked or leave the camera views;
  • On failure, dropped object, video stutter, or a blocked camera — click Record Again or press Esc;
  • You can finish the batch first, then inspect and delete abnormal episodes;
  • Stop immediately on any loss-of-control or collision risk.

Inspect, delete, and merge​

OperationMethod
Inspect episodesSelect an episode, play the video / action replay; check task completion and gripper motion
Delete abnormal episodesBatch Delete Episodes → select → confirm → Generate Deleted Copy (originals are not overwritten)
Merge datasetsMerge → select datasets → new name (task descriptions, device combos, and camera configs must match)

Inspect dataset

22.6 Training​

Training

22.6 Training

Training turns the teaching data into an action model — the GUI equivalent of Chapter 15.

ParameterOption / valueDetails
Training hardwareCloud · automatically select GPUCloud server, consumes credits
Local · freeCurrent computer, requires a compatible local GPU
Training datasetSelect the target datasetYour cleaned dataset from 22.5
PolicyACTCurrent default action-control policy
Training steps10000Initial value; adjust by results

Recommended steps and episode counts (matches Chapter 11's guidance):

Task difficultyTask descriptionEpisodesSteps
BeginnerFixed Point A to Point B~2010,000-15,000
IntermediateGrasp and place at random positions~5030,000-40,000
AdvancedMultiple steps or long duration~10080,000-100,000

Training duration depends on the GPU and steps — 20,000 cloud steps may take minutes to tens of minutes; 100,000 about five times as long. Click Start Training and watch progress under Current Training Tasks.

Training configuration

22.7 Model and Operation (Inference)​

Operate

22.7 Model and Operation (Inference)

Open Model to see training results; confirm the task and device combination match your project. Then Operation loads the model onto the arms:

  1. Select a model marked as supporting the current arms;
  2. Select an inference method: Cloud Inference or Local Inference;
  3. Start inference and watch the task run.

Model list

Cloud vs. local inference:

ComparisonCloud inferenceLocal inference
ComputeHigh-performance cloud GPULocal CPU (GPU not supported currently)
Performance depends onNetwork qualityLocal CPU performance
ParametersAction count (default 120); chunk threshold (default 0.9 — higher is more cautious, lower smoother)Run count; time limit per run
Data outputInference verification onlyAuto-generates a dataset from the runs
CostSubject to platform creditsUsually free, CPU-limited

Model operation interface

note

Before operation, confirm the arms are connected and the workspace is safe. During operation, do not disconnect or disassemble the arms. If results disappoint, return to Dataset — delete abnormal episodes, add valid data, and train again. That is Chapter 16's iteration loop, one more time.

22.8 Course Conclusion​

Conclusion

22.8 Course Conclusion

You have now walked the SO-ARM from cardboard box to a trained, deployed policy — twice:

  • The code path (Stages 2-3): assemble, calibrate, teleoperate, record, train ACT, evaluate, iterate;
  • The VLA paths (Stage 4): fine-tune GR00T on your own GPU pipeline, or run the whole loop no-code on SenseCraft Robotics.

Where to go next:

  • Chapter 17's double-arm setup if you skipped it;
  • The Robotics Wiki for the wider SO-ARM ecosystem: GR00T on Jetson Thor, AmazingHand, Isaac Lab RL, LeIsaac simulation;
  • Your own tasks — the entire course was scaffolding for them.

If the course helped you, star SO-ARM100 and Seeed-Projects/lerobot on GitHub, and share what you build in the community groups from the course introduction.

Loading Comments...