Skip to main content
Stage 1 · Chapter 1 · Overview

1. Course Overview

Seeed Studio collaborates with NVIDIA on a hands-on curriculum for developers: from robot demonstrations and simulation to VLA post-training and real-world deployment — built here around the SO-ARM101.

The Course Workflow​

End to end

The Course Workflow

This course focuses on the complete development workflow of the SO-ARM101 robotic arm. It guides learners through hardware setup, data collection, model training, simulation validation, and finally deployment and inference — on the real arm and on Jetson edge devices. By combining LeRobot, NVIDIA Isaac Sim, Isaac GR00T N1.7, and Jetson, the course builds a complete experimental environment for robot learning and embodied AI.

Through this course, learners will understand how to:

  • collect robotic-arm data via leader-follower teleoperation;
  • train a Vision-Language-Action policy with Isaac GR00T N1.7 on that data;
  • scale up with simulated episodes and data augmentation;
  • evaluate the trained model in the real world;
  • deploy the model on a Jetson device and run the task at the edge.
SO-ARM101 kit

The Demonstration Task​

Vial to rack

The Demonstration Task

For demonstration purposes, this course uses a simple pick-and-place task: put the three vials into the vial rack. The same task is used by NVIDIA's SO-101 workshop, so your dataset stays compatible with NVIDIA's reference datasets and checkpoints.

You can adjust the target task according to your own environment and requirements — the pipeline (collect → train → deploy → evaluate) does not change.

What This Course Emphasizes​

Reproducible platform

What This Course Emphasizes

This course does not only focus on training and running a single model. More importantly, it emphasizes how to build a reproducible and extensible robotic experimental platform:

  • a fixed dataset schema (six joint dimensions, two cameras, one task sentence) that works unchanged across the real robot, Isaac Sim, and Jetson;
  • commands that were verified end to end on the SO-ARM101;
  • the same tools as the reBot DLI course, so you can move between the two arms without relearning the pipeline.

Next: Chapter 2 — LeRobot Background and the Community.

Loading Comments...