10. Train the GR00T N1.7 Policy
Understand Isaac GR00T N1.7, prepare the SO-101 dataset for it, and fine-tune a task-specific VLA model on the data collected in Chapter 9.
10.1 NVIDIA Isaac GR00T N1.7
10.1 NVIDIA Isaac GR00T N1.7
NVIDIA Isaac GR00T N1.7 is an open Vision-Language-Action (VLA) model for generalized robot skills. This cross-embodiment model takes multimodal input — language and images — to perform manipulation tasks in diverse environments.
The model is trained once and adapted per embodiment through modality configurations: a small file that tells GR00T which dataset columns are the arm, the gripper, the cameras, and the language instruction. This chapter builds exactly that configuration for the SO-ARM101.
References:
10.2 Prepare the Python Environment
10.2 Prepare the Python Environment
sudo apt install git-lfs && git lfs install
cd ~
git clone --recurse-submodules https://github.com/NVIDIA/Isaac-GR00T
cd Isaac-GR00T
sudo apt-get update && sudo apt-get install -y ffmpeg
uv sync --python 3.12
Fine-tuning the 3B model needs an RTX 5090 / RTX 6000 class GPU (NVIDIA's workshop baseline). An 8 GB laptop GPU is not enough for this chapter; the ACT sanity check at the end of this chapter still runs on small GPUs.
10.3 Handling the Dataset
10.3 Handling the Dataset
LeRobot writes dataset v3; GR00T N1.7 fine-tuning reads the older v2 layout. Convert the dataset recorded in Chapter 9:
cd ~/Isaac-GR00T
uv run --project scripts/lerobot_conversion \
python scripts/lerobot_conversion/convert_v3_to_v2.py \
--repo-id so101_vials_real \
--root $HOME/rebot-arm-dli-isaacsim/datasets
The converter moves the v3 copy aside as so101_vials_real_V30 and leaves
the v2 dataset at the original path. If you plan to merge simulated
episodes later (Chapter 13), do the merge before converting.
Then add meta/modality.json inside the converted dataset:
{
"state": {
"single_arm": { "start": 0, "end": 5 },
"gripper": { "start": 5, "end": 6 }
},
"action": {
"single_arm": { "start": 0, "end": 5 },
"gripper": { "start": 5, "end": 6 }
},
"video": {
"wrist": { "original_key": "observation.images.front" },
"front": { "original_key": "observation.images.external" }
},
"annotation": {
"human.task_description": { "original_key": "task_index" }
}
}
Why the split is at 5:
| Dimensions | Meaning |
|---|---|
| 0–4 | shoulder_pan, shoulder_lift, elbow_flex, wrist_flex, wrist_roll |
| 5 | gripper |
SO-ARM101 has five arm joints plus a gripper — six values in total. The
reBot course uses seven, so do not copy its end: 6 split.
The camera mapping is deliberate:
| Dataset feature | Physical camera | GR00T input |
|---|---|---|
observation.images.front | Gripper / wrist camera | wrist |
observation.images.external | Overhead camera | front |
10.4 Register the SO-101 Modality Config
10.4 Register the SO-101 Modality Config
cd ~/Isaac-GR00T
mkdir -p examples/so101
Create examples/so101/so101_config.py:
# SPDX-License-Identifier: Apache-2.0
from gr00t.configs.data.embodiment_configs import register_modality_config
from gr00t.data.embodiment_tags import EmbodimentTag
from gr00t.data.types import (
ActionConfig,
ActionFormat,
ActionRepresentation,
ActionType,
ModalityConfig,
)
so101_config = {
# Current frame from both cameras; keys match meta/modality.json
"video": ModalityConfig(
delta_indices=[0],
modality_keys=["wrist", "front"],
),
# Current joint reading
"state": ModalityConfig(
delta_indices=[0],
modality_keys=["single_arm", "gripper"],
),
# Predict 16 future steps
"action": ModalityConfig(
delta_indices=list(range(0, 16)),
modality_keys=["single_arm", "gripper"],
action_configs=[
# Arm: relative deltas generalize better across poses
ActionConfig(
rep=ActionRepresentation.RELATIVE,
type=ActionType.NON_EEF,
format=ActionFormat.DEFAULT,
),
# Gripper: absolute target works better for open/close
ActionConfig(
rep=ActionRepresentation.ABSOLUTE,
type=ActionType.NON_EEF,
format=ActionFormat.DEFAULT,
),
],
),
"language": ModalityConfig(
delta_indices=[0],
modality_keys=["annotation.human.task_description"],
),
}
register_modality_config(so101_config, embodiment_tag=EmbodimentTag.NEW_EMBODIMENT)
10.5 Fine-Tune the GR00T N1.7 Policy
10.5 Fine-Tune the GR00T N1.7 Policy
Route A — your real dataset (the default path of this course):
cd ~/Isaac-GR00T
export SAVE_STEPS=5000
bash examples/finetune.sh \
--base-model-path nvidia/GR00T-1.7-3B \
--dataset-path $HOME/rebot-arm-dli-isaacsim/datasets/so101_vials_real \
--modality-config-path examples/so101/so101_config.py \
--embodiment-tag NEW_EMBODIMENT \
--output-dir $HOME/groot_so101_real
Route B — co-training with simulated episodes. Merge the datasets
first (Chapter 13), then point --dataset-path at the merged set. NVIDIA's
workshop recipe: a few real episodes plus 70–100 simulated ones.
Route C — sequential fine-tuning. Fine-tune on simulation first, then continue from that checkpoint on real data:
bash examples/finetune.sh \
--base-model-path $HOME/groot_so101_sim/checkpoint-5000 \
--dataset-path $HOME/rebot-arm-dli-isaacsim/datasets/so101_vials_real \
--modality-config-path examples/so101/so101_config.py \
--embodiment-tag NEW_EMBODIMENT \
--output-dir $HOME/groot_so101_sim_then_real
Useful environment variables from examples/finetune.sh:
| Variable | Default | Effect |
|---|---|---|
SAVE_STEPS | 1000 | Checkpoint interval |
MAX_STEPS | 10000 | Total optimizer steps |
GLOBAL_BATCH_SIZE | 32 | Lower it on a smaller GPU |
EPISODE_SAMPLING_RATE | 0.1 | Fraction of steps that sample episodes |
DS_WEIGHTS_ALPHA | unset | Balances merged sources by size |
USE_WANDB | 1 | Set to 0 to disable experiment logging |
Before spending GPU hours, a small ACT policy trains on the same dataset in minutes and confirms the dataset, normalizers, and optimizer are wired correctly:
cd ~/rebot_lerobot && source .venv/bin/activate
lerobot-train \
--policy.type=act --policy.push_to_hub=false \
--dataset.repo_id=so101_vials_real \
--dataset.root=$HOME/rebot-arm-dli-isaacsim/datasets/so101_vials_real \
--output_dir=/tmp/act_check --steps=60 --batch_size=4
10.6 Training Outputs
10.6 Training Outputs
$HOME/groot_so101_real/
├── checkpoint-1000/
├── checkpoint-2000/
├── checkpoint-5000/
└── ...
Each checkpoint contains the model weights and the experiment configuration needed by the inference server. More steps are not always better: evaluate several checkpoints on the real robot (Chapter 11) and keep the one that completes the task most reliably.