Skip to main content
Stage 4 · Chapter 14 · Deploy on Jetson

14. Setup Your Jetson Edge Device

Prepare the Jetson platform for GR00T N1.7 TensorRT deployment: select the target, flash JetPack 7.2, and verify the board before connecting the robot.

14.1 Supported Targets​

Orin or Thor

14.1 Supported Targets

The validated deployment targets for the SO-ARM101 pipeline are:

TargetValidated software pathRuntime environment used later
Jetson AGX OrinJetPack 7.2 / L4T R39.2.venv-jp72 with scripts/deployment/orin_jp72/run_full_trt.sh
Jetson AGX ThorJetPack 7.2 / L4T R39.2.venv with scripts/activate_thor.sh
Engines are target-specific

TensorRT engines depend on the GPU architecture. Orin and Thor may share the same compatible checkpoint and dataset, but each target must build its own engine bundle (Chapter 17).

14.2 Prepare the Host Computer​

Ubuntu host

14.2 Prepare the Host Computer

Prepare an Ubuntu host with:

  • at least 25 GB of free space for SDK Manager and JetPack packages;
  • a reliable USB Type-C data cable;
  • a stable network connection;
  • administrator access.

Install NVIDIA SDK Manager from the official download page: https://developer.nvidia.com/sdk-manager.

14.3 Enter Force Recovery Mode​

Button dance

14.3 Enter Force Recovery Mode

Jetson AGX Thor Developer Kit​

  1. Power off the Jetson.
  2. Connect its recovery USB Type-C port to the host computer.
  3. Hold the Force Recovery button.
  4. Press and release Reset while continuing to hold Force Recovery.
  5. Release Force Recovery.
  6. Confirm that SDK Manager detects the target.
MarkButton
11Power
12Force Recovery
13Reset

Jetson AGX Orin Developer Kit​

The Orin developer kit must be powered on before this procedure; use button 2 (Force Recovery) and button 3 (Reset):

  1. Connect USB Type-C port 10 — next to the 40-pin header — to the Ubuntu host.
  2. Connect the power supply and make sure the kit is powered on.
  3. Press and hold button 2 (Force Recovery).
  4. While holding Force Recovery, press and hold button 3 (Reset).
  5. Release both buttons.
  6. Confirm that SDK Manager detects the Jetson AGX Orin target.
MarkButton or port
1Power button
2Force Recovery button
3Reset button
10USB Type-C port used for flashing

Alternative: Enter Recovery Mode While Powered Off​

  1. Make sure the developer kit is powered off.
  2. Press and hold button 2 (Force Recovery).
  3. Connect the power supply. If the power LED does not turn on, press and release button 1 (Power).
  4. Release Force Recovery.
  5. Confirm that SDK Manager detects the target.

Reference: NVIDIA Jetson AGX Orin Developer Kit User Guide — Force Recovery Mode.

14.4 Install JetPack​

SDK Manager

14.4 Install JetPack

In SDK Manager:

  1. Select Jetson AGX Thor / Jetson AGX Orin as the target hardware.
  2. Select JetPack 7.2.
  3. Use Direct Flash unless your deployment requires an ISO workflow.
  4. Complete the target installation and initial Ubuntu setup.

Follow the SDK Manager wizard through Installation completed successfully before disconnecting the recovery cable.

14.5 Verify the Jetson​

On the device

14.5 Verify the Jetson

Run these commands on the target:

tr -d '\0' < /proc/device-tree/model
cat /etc/nv_tegra_release
df -h /
free -h

Confirm that:

  • the detected model matches the intended Orin or Thor target;
  • the system reports the expected JetPack/L4T release;
  • the NVMe or root filesystem has enough space for the checkpoint, backbone, ONNX files, and TensorRT engines;
  • the system boots normally after a restart.

Reserve approximately 45–50 GB for a complete local TensorRT workflow.

Next: Chapter 15 — Connect the Robot Hardware.

Loading Comments...