Skip to main content
Stage 4 · Chapter 15 · Deploy on Jetson

15. Connect the Robot Hardware

Attach the SO-101 follower to the Jetson over USB serial, connect the two cameras, and carry over the calibration — the edge device then needs nothing else from the workstation at runtime.

15.1 Hardware Requirements​

What you need

15.1 Hardware Requirements

  • Jetson AGX Orin or AGX Thor with JetPack 7.2 (Chapter 14);
  • SO-ARM101 follower arm — USB serial, no CAN adapter needed;
  • two USB cameras (wrist + external, as in Chapter 8);
  • a powered USB 3.0 hub — Thor provides only two Type-A ports, which is not enough for the follower and two cameras at once;
  • the follower's 12 V power supply and USB data cable.
Leader arm not required at the edge

The leader arm is only used for data collection. A Jetson deployment needs the follower, the cameras, and the policy — nothing else.

15.2 Connect the Devices​

Order matters

15.2 Connect the Devices

  1. Keep the follower's 12 V power off.
  2. Connect the follower's USB serial port to the Jetson (directly, or through the powered hub).
  3. Connect the wrist and external cameras through the powered hub.
  4. Copy the calibration directory from the workstation (see below).
  5. Apply follower power last.
Copy the calibration, not just the code

The follower plays back the calibration written for its exact ID. Copy the workstation's calibration to the same path on the Jetson:

# on the workstation
rsync -av ~/.cache/huggingface/lerobot/calibration/ \
jetson:/home/<jetson-user>/.cache/huggingface/lerobot/calibration/

15.3 Identify the Serial Port​

USB serial

15.3 Identify the Serial Port

Apply follower power, then check the device node:

ls /dev/ttyACM*

Confirm the port works with LeRobot's finder (unplug and replug when prompted):

lerobot-find-port

Export the values used by every later command — the same names as the workstation:

export ROBOT_PORT=/dev/ttyACM0
export ROBOT_ID=so101_follower

If the port cannot be opened, fix the permissions on the Jetson:

sudo usermod -aG dialout $USER   # log out and back in once
sudo chmod 666 /dev/ttyACM*

15.4 Identify the Cameras​

Two video nodes

15.4 Identify the Cameras

ls /dev/video*
lerobot-find-cameras opencv

Map the preview images (file names contain the device index) and export — the same variables as Chapter 8:

export CAMERA_GRIPPER=4
export CAMERA_EXTERNAL=6

Camera indices can change after a reboot or replug; re-run this check before every deployment session.

15.5 Hardware Readiness Checklist​

Before Chapter 16

15.5 Hardware Readiness Checklist

  • Jetson at the validated JetPack/L4T release, boots reliably;
  • Follower enumerated at the expected /dev/ttyACM* node;
  • Calibration files present under ~/.cache/huggingface/lerobot/calibration/;
  • Both cameras enumerate and preview at 640×480 and 30 FPS;
  • ROBOT_PORT, ROBOT_ID, CAMERA_GRIPPER, CAMERA_EXTERNAL exported;
  • Powered hub in use; no device drops under load.

Next: Chapter 16 — Configure the GR00T Software Environment.

Loading Comments...