Skip to main content
Stage 2 · Chapter 7 · Build Your Robot Lab

7. Prepare the Robot Arm

Two arms: a leader you move by hand and a follower that repeats the motion. Install the environment, write servo IDs (skip on pre-built arms), calibrate both, and verify with a first teleoperation.

7.1 The Two Arms​

Leader and follower

7.1 The Two Arms

Leader arm — a low-cost open-source arm designed for education and research, available as a complete unit or a DIY kit. Six joints driven by 7.4 V-class STS3215 servos on a 5 V supply; it only reads joint angles.

Follower arm — the arm that executes. On the Pro kit it runs 12 V servos; it mirrors the leader during teleoperation and later executes the trained VLA policy.

Do not mix the power supplies

The leader runs on 5 V and the follower on 12 V. Swapping them can damage the servos. Power both arms down before changing any cable.

The full assembly walkthrough lives in the beginner course: Beginner Chapter 6 — Configure Motors and Assemble the Arms covers 3D printing, motor planning, ID writing, and step-by-step assembly; Beginner Chapter 7 — Servo Debugging covers the Feetech debugging tool for a misbehaving servo.

7.2 Install the LeRobot Environment​

Install once

7.2 Install the LeRobot Environment

Before calibration, install the exact environment every later chapter uses. Install uv first, then create the workspace:

curl -LsSf https://astral.sh/uv/install.sh | sh
echo 'export PATH="$HOME/.local/bin:$PATH"' >> ~/.bashrc
source ~/.bashrc
uv --version

mkdir ~/rebot_lerobot
cd ~/rebot_lerobot
sudo apt update
sudo apt install -y ffmpeg

# Download the Seeed LeRobot fork (includes SO101 leader/follower support)
git clone https://github.com/Seeed-Projects/lerobot.git

# Create virtual environment (Python 3.12)
uv venv --python 3.12 .venv
source .venv/bin/activate

uv pip install --upgrade pip
uv pip install -e ./lerobot

# Feetech servo SDK — required by the SO-101 buses
uv pip install feetech-servo-sdk
Re-entering the environment

The runtime environment only needs to be configured once. Later chapters assume you can re-enter it with: cd ~/rebot_lerobot && source .venv/bin/activate

7.3 Kit or Pre-Built?​

Skip IDs if pre-built

7.3 Kit or Pre-Built?

Your situationAssembleWrite servo IDsCalibrate
3D-printed or kit versionYesYesYes
Pre-built arm (整机)Already doneSkip — IDs are written at the factoryYes

If you bought pre-built arms, jump straight to 7.5 Calibrate the Arms.

Label every servo before it goes into a joint — F1–F6 on follower servos, L1–L6 on leader servos. Joint 1 = shoulder pan, 2 = shoulder lift, 3 = elbow, 4 = wrist pitch, 5 = wrist roll, 6 = gripper. SO-ARM101 leader joints 1–3 use different gear ratios than SO-ARM100 — check the ratio table in Beginner Chapter 6.2 before mounting anything.

One servo at a time

All six servos share one serial bus. Configure IDs with exactly one servo wired to the controller board, or a duplicate ID gets written to every servo that has it.

7.4 Write Servo IDs (Kit Version Only)​

lerobot-setup-motors

7.4 Write Servo IDs (Kit Version Only)

Find the controller-board port first:

lerobot-find-port

Unplug the board when prompted and replug it; the printed port is yours (usually /dev/ttyACM0).

Flash IDs joint by joint:

lerobot-setup-motors \
--robot.type=so101_follower \
--robot.port=/dev/ttyACM0

The tool names the joint to connect — wire up that single servo, press Enter, and it writes the ID and baud rate:

Connect the controller board to the 'gripper' motor only and press enter.

Repeat for all six follower joints, then run the same tool for the leader:

lerobot-setup-motors \
--teleop.type=so101_leader \
--teleop.port=/dev/ttyACM1

Configure serial port permissions (and remember them after reboots):

sudo usermod -aG dialout $USER   # log out and back in once
sudo chmod 666 /dev/ttyACM*

On Ubuntu, the brltty service can claim the USB serial adapter. If the port disappears after a few seconds, remove it: sudo apt remove brltty.

7.5 Calibrate the Arms​

Reference pose

7.5 Calibrate the Arms

Calibration is required for both kit and pre-built arms. It teaches LeRobot each joint's middle position and its two mechanical end stops. Calibration files live under ~/.cache/huggingface/lerobot/calibration/, keyed by arm ID — reuse an ID only for the same physical arm.

Find both ports, then export the values used by every later chapter:

export TELEOP_PORT=/dev/ttyACM0
export TELEOP_ID=so101_leader
export ROBOT_PORT=/dev/ttyACM1
export ROBOT_ID=so101_follower

Calibrate the leader:

lerobot-calibrate \
--teleop.type=so101_leader \
--teleop.port=$TELEOP_PORT \
--teleop.id=$TELEOP_ID
  1. Move every joint to the middle of its travel. Center the wrist roll carefully — if it starts at an end stop, the encoder can overflow during the sweep.
  2. Press Enter, then sweep each joint slowly to both end stops, one joint at a time. Repeats are fine; the extremes are overwritten.
  3. Press Enter to save.

Calibrate the follower the same way:

lerobot-calibrate \
--robot.type=so101_follower \
--robot.port=$ROBOT_PORT \
--robot.id=$ROBOT_ID

For the follower, stop at the arm's true mechanical end stop — not at a cable, not at the table. A pinched cable records a false limit and compresses the usable range.

Signature of a bad calibration

If the follower mirrors only half of the leader's motion, or a joint snaps to an end stop, the range sweep was too short. Recalibrate that arm and move every joint through its complete travel.

If you run the NVIDIA workshop tooling, verify the follower's quality:

export ROBOT_PORT ROBOT_ID
python ~/Sim-to-Real-SO-101-Workshop/docker/real/scripts/so101_check_calibration.py

A good calibration ends with:

Overall: ✓ PASS — calibration looks good.

7.6 Verify the Robotic Arm​

First teleoperation

7.6 Verify the Robotic Arm

Bring both arms to a similar pose, then run:

lerobot-teleoperate \
--robot.type=so101_follower \
--robot.port=$ROBOT_PORT \
--robot.id=$ROBOT_ID \
--teleop.type=so101_leader \
--teleop.port=$TELEOP_PORT \
--teleop.id=$TELEOP_ID

Move the leader slowly. The follower must track each joint in the same direction and reach the same end stops. Stop with Ctrl+C.

This also confirms the joint ordering used everywhere else in the course: shoulder_pan, shoulder_lift, elbow_flex, wrist_flex, wrist_roll, gripper. If one joint moves backwards, recalibrate — do not compensate in software.

Keep one hand near the follower's power switch during the first runs.

Next: Chapter 8 — Building the Workspace.

Loading Comments...