Skip to main content

Seeed Studio Round Display for XIAO Christmas Ball

On this tutorial I'm going to show you how you can create a Christmas ball with falling snow and changing background images.

The program performs the following:

  • Displays a background image stored as a C array.
  • Simulates snow particles falling over the image, with a wind effect.
  • Detects touch input and cycles through a set of background images.
  • Uses double-buffering for smooth animations.

Environment Preparation

Hardware

For the project, we're going to need:

I'm using the XIAO ESP32S3 because of the memory. The PNGDEC requires a bit of memory to run ~40kbytes.

Software Preparation

To use the Round Display, head to Getting Started with Round Display for XIAO to install the necessary libraries.

Try some of the examples to see if everything is working well.

Libraries

For this project, we're going to use the libraries that come bundled with the Seeed Studio Round Display For XIAO

Install all the libraries like specified in the tutorial Getting Started with Round Display for XIAO. After that, you need the following:

  • PNGdec library .
  • Update LVGL library (or not install the one from Seeed Studio github)

Images

Our images are PNG images stored in Flash Arrays. They are displayed using PNGdec library.

All images must be PNG

Here are the images that I've used - all are AI generated

Our background images need to be prepared for that TFT_eSPI can display them and they fit well on the Round Display for XIAO.

Prepare images

Resize Images

Our Round Display for XIAO has a 240x240 resolution. We need to resize the images. I'm going to show how to do it using GIMP

  1. Open the image
  2. Go to Image > Scale Image
  1. Set Width and Height to 240. Because the Keep Ratio is selected (the chain), once you change the width, the height should also change.
  1. Press the Scale button.
  1. Save the image (I'm going to override the old one)

Create the Flash Arrays

NOTE: This instructions are inside the TFT_eSPI Flash_PNG example.

To create the flash array, go to File to C style array converter

The steps now are:

  1. Upload the image using Browse . After uploading the image
  1. We need to set some options
  • Treat as binary

All the other options gray out.

  1. Let's change the Data type to char
  1. Press convert. This will convert the image to an array.
  1. You can now press the button Save as file to save your image and add it to your Arduino Sketch or press the button Copy to clipboard If you Copy to clipboard, you'll have to press the 3 dots on the right side of the Arduino editor and choose New Tab

Give it a name (generally your image name with .h extension)

You'll end up with all your images as .h files.

Code

Here's the code for the Christmas ball. A little explanation of the principal functions of the code. The code also includes some comments.

Headers and libraries

We start by including some libraries.

#include <PNGdec.h>
#include <TFT_eSPI.h>
#include <Wire.h>

#include "background1.h"
#include "background2.h"
#include "background3.h"

#define USE_TFT_ESPI_LIBRARY
#include "lv_xiao_round_screen.h"

Remember that you need to have the Seeed Studio libraries installed.

Background images

Here are the functions to manage the background images

struct Background {
const uint8_t *data;
size_t size;
};

const Background backgrounds[] = {
{(const uint8_t *)background1, sizeof(background1)},
{(const uint8_t *)background2, sizeof(background2)},
{(const uint8_t *)background3, sizeof(background3)},
};

  • Struct: Each background image is stored as a Background struct containing:

    • data: Pointer to the PNG data.
    • size: Size of the PNG file.
  • Array: The backgrounds array stores all the background images. The currentBackground variable tracks the currently displayed background.

Snow particles Simulation

  1. Initialization of particles
void initParticles() {
for (int i = 0; i < numParticles; i++) {
particles[i].x = random(0, sprite.width());
particles[i].y = random(0, sprite.height());
particles[i].speed = random(3, 8);
}
}
  • It initializes numParticles with random positions and speeds.
  1. Particle updates
void updateParticles() {
for (int i = 0; i < numParticles; i++) {
particles[i].speed += random(-1, 2); // Speed variation
particles[i].speed = constrain(particles[i].speed, 3, 8);
particles[i].y += particles[i].speed; // Move down
particles[i].x += random(-1, 2); // Wind effect
// Wrap-around logic
if (particles[i].y > sprite.height()) {
particles[i].y = 0;
particles[i].x = random(0, sprite.width());
particles[i].speed = random(3, 8);
}
if (particles[i].x < 0) particles[i].x = sprite.width();
if (particles[i].x > sprite.width()) particles[i].x = 0;
}
}
  • Updates particle positions with:
    • Falling Effect: Each particle moves down.
    • Wind Effect: Adds a slight horizontal drift.
    • Wrap Around: Particles reset to the top when they exit the bottom.
  1. Rendering particles:
void renderParticlesToSprite() {
for (int i = 0; i < numParticles; i++) {
sprite.fillCircle(particles[i].x, particles[i].y, 2, TFT_WHITE);
}
}
  • It renders each particle as a small white circle

PNG Decoding

int16_t rc = png.openFLASH((uint8_t *)backgrounds[currentBackground].data,
backgrounds[currentBackground].size,
pngDrawToSprite);
if (rc != PNG_SUCCESS) {
Serial.println("Failed to open PNG file!");
return;
}
png.decode(NULL, 0);
  • Loads and decodes the current background PNG using the png.openFLASH() function

Touch interaction

if (chsc6x_is_pressed()) {
currentBackground = (currentBackground + 1) % numBackgrounds; // Cycle backgrounds
delay(300); // Debounce
}
  • Detects a touch event using the chsc6x_is_pressed() and changes the background image by incrementing currentBackground

Setup and loop

  • Setup:
void setup() {
Serial.begin(115200);
tft.begin();
tft.fillScreen(TFT_BLACK);
sprite.createSprite(240, 240); // Match display size
pinMode(TOUCH_INT, INPUT_PULLUP);
Wire.begin();
initParticles();
}
  • Initializes the display, touch input and snow particles

  • Main loop:

void loop() {
sprite.fillScreen(TFT_BLACK);
// Render background and snow
int16_t rc = png.openFLASH((uint8_t *)backgrounds[currentBackground].data,
backgrounds[currentBackground].size,
pngDrawToSprite);
if (rc == PNG_SUCCESS) {
png.decode(NULL, 0);
updateParticles();
renderParticlesToSprite();
sprite.pushSprite(0, 0);
}
// Handle touch input
if (chsc6x_is_pressed()) {
currentBackground = (currentBackground + 1) % numBackgrounds;
delay(300);
}
delay(10); // ~100 FPS
}
  • Clears the sprite, renders the current frame (background + particles), and checks for user input.

Double buffering

To reduce the flickering and improving animation smoothness of the snow flakes, we use double buffering.

This allows us to draw in an off-screen buffer before displaying it on the screen.

Double buffering here

In this project, the TFT_eSPI library's TFT_eSprite class implements double buffering.

  1. Sprite creation
  • The sprite (off-screen buffer) is created in the setup() function:
sprite.createSprite(240, 240); // Match display size
  1. Drawing the buffer
  • All drawing operations (background rendering and snow particle animation) are done on the sprite:
sprite.fillScreen(TFT_BLACK); // Clear the sprite
renderParticlesToSprite(); // Draw snow particles
  1. Updating the display
  • After the frame is fully drawn in the sprite, it is pushed to the display in one operation:
sprite.pushSprite(0, 0);
  • This transfers the buffer's contents to the screen instantly.
  1. Reuse
  • The sprite is reused for every frame by clearing it at the start of the loop():
sprite.fillScreen(TFT_BLACK);

Advantages of Using Double Buffering

  • Smooth Snow Animation: The falling snow particles are updated seamlessly without flickering.
  • Dynamic Background Switching: The touch-triggered background changes happen without visible delays or artifacts.
  • Efficient Rendering: Drawing in memory (RAM) is faster than directly updating the display line by line.

Here's the complete code for the project:

/**
*
* To create the images as C arrays, visit:
* https://notisrac.github.io/FileToCArray/
*
*/
#include <PNGdec.h>
#include <TFT_eSPI.h>

#include "background1.h"
#include "background2.h"
#include "background3.h"

#define USE_TFT_ESPI_LIBRARY
#include "lv_xiao_round_screen.h"

// PNG decoder and TFT display instances
PNG png;
//TFT_eSPI tft = TFT_eSPI();
TFT_eSprite sprite = TFT_eSprite(&tft); // Off-screen buffer

#define MAX_IMAGE_WIDTH 240

// Backgrounds for the snow globe
struct Background {
const uint8_t *data;
size_t size;
};

// Define the backgrounds with explicit casting
const Background backgrounds[] = {
{(const uint8_t *)background1, sizeof(background1)},
{(const uint8_t *)background2, sizeof(background2)},
{(const uint8_t *)background3, sizeof(background3)},
};
const size_t numBackgrounds = sizeof(backgrounds) / sizeof(backgrounds[0]);

int currentBackground = 0; // Index of the current background

// Snow particle properties
const int numParticles = 100; // Number of snow particles
struct Particle {
int16_t x, y; // Position
int16_t speed; // Vertical speed
};
Particle particles[numParticles];

// Function to draw PNG to the sprite (callback for PNG decoder)
void pngDrawToSprite(PNGDRAW *pDraw) {
uint16_t lineBuffer[MAX_IMAGE_WIDTH];
png.getLineAsRGB565(pDraw, lineBuffer, PNG_RGB565_BIG_ENDIAN, 0xffffffff);
sprite.pushImage(0, pDraw->y, pDraw->iWidth, 1, lineBuffer);
}

// Initialize snow particles
void initParticles() {
for (int i = 0; i < numParticles; i++) {
particles[i].x = random(0, sprite.width());
particles[i].y = random(0, sprite.height());
particles[i].speed = random(3, 8); // Random speed for each snowflake
}
}

// Update snow particle positions
void updateParticles() {
for (int i = 0; i < numParticles; i++) {
particles[i].speed += random(-1, 2); // Random variation in speed
particles[i].speed = constrain(particles[i].speed, 3, 8);
particles[i].y += particles[i].speed;
particles[i].x += random(-1, 2); // Wind effect

// Wrap around screen
if (particles[i].y > sprite.height()) {
particles[i].y = 0;
particles[i].x = random(0, sprite.width());
particles[i].speed = random(3, 8);
}
if (particles[i].x < 0) particles[i].x = sprite.width();
if (particles[i].x > sprite.width()) particles[i].x = 0;
}
}

// Render snow particles to the sprite
void renderParticlesToSprite() {
for (int i = 0; i < numParticles; i++) {
sprite.fillCircle(particles[i].x, particles[i].y, 2, TFT_WHITE);
}
}

void setup() {
Serial.begin(115200);
Serial.println("\n\nUsing the PNGdec library with touch interaction");

// Initialize TFT
tft.begin();
tft.fillScreen(TFT_BLACK);
sprite.createSprite(240, 240); // Match display size

// Initialize touch interrupt pin
pinMode(TOUCH_INT, INPUT_PULLUP);
Wire.begin();

// Initialize particles
initParticles();

Serial.println("Setup complete.");
}

void loop() {
// Clear the sprite for the new frame
sprite.fillScreen(TFT_BLACK);

// Render the current background to the sprite
int16_t rc = png.openFLASH((uint8_t *)backgrounds[currentBackground].data,
backgrounds[currentBackground].size,
pngDrawToSprite);


if (rc != PNG_SUCCESS) {
Serial.println("Failed to open PNG file!");
return;
}
png.decode(NULL, 0); // Decode and render background

// Update and render snow particles
updateParticles();
renderParticlesToSprite();

// Push the sprite to the display
sprite.pushSprite(0, 0);

// Check for touch input using chsc6x_is_pressed
if (chsc6x_is_pressed()) {
currentBackground = (currentBackground + 1) % numBackgrounds; // Cycle through backgrounds
delay(300); // Debounce delay
}

delay(10); // ~100 FPS
}

Now you can use your own pictures to create a magical Christmas Ball.

✨ Contributor Project

Tech Support & Product Discussion

Thank you for choosing our products! We are here to provide you with different support to ensure that your experience with our products is as smooth as possible. We offer several communication channels to cater to different preferences and needs.

Loading Comments...