Skip to main content

Get Started with Indicator for Meshtastic

SenseCAP Indicator is a 4-inch touchscreen device designed for Meshtastic®, powered by dual MCUs, the ESP32 and RP2040, and supports Wi-Fi, BLE, and LoRa®. It is an open-source, powerful IoT development platform.

Introduction

Feature

  • Supports Meshtastic: Pre-flashed with Meshtastic firmware, it is ready to work once powered on. You can also upgrade the firmware using Meshtastic Flasher.
  • Dual MCUs and Rich GPIOs: Equipped with powerful ESP32S3 and RP2040 dual MCUs and over 400 Grove-compatible GPIOs for flexible expansion options.
  • Local LoRa® Hub for IoT Connectivity: Integrated with the Semtech SX1262 LoRa® chip, the device can be converted to a LoRaWAN® Single-Channel Gatewa via tutorial. Alternatively, connect LoRa® devices to popular IoT platforms like Matter via Wi-Fi.
  • Fully Open Source Platform: Leverage the extensive ESP32 and Raspberry Pi open-source ecosystem for infinite application possibilities.
  • Suitable for Multiple Application Scenarios: Can be used as a Meshtastic desktop node or a car node, as well as a LoRaWAN® Single-Channel Gateway.

Specification

Screen3.95 Inch, Capacitive RGB Touch Screen
Screen Resolution480 x 480 pixels
Power Supply5V-DC, 1A
BatteryN/A
Processor

ESP32-S3: Xtensa® dual-core 32-bit up to 240 MHz

RP2040: Dual ARM Cortex-M0+ up to 133MHz

Flash

ESP32-S3: 8MB

RP2040: 2MB

External StorageSupport up to 32GB Micro SD Card (not included)
Wi-Fi802.11b/g/n, 2.4GHz
BluetoothBluetooth 5.0 LE
LoRa(SX1262)Support 862-930MHz
Buzzer(Not developed yet)MLT-8530, Resonant Frequency:2700Hz
CertificationCE/FCC

Hardware Overview

pir

Get Started

note

When the device is in the states below, please don't manually reboot or turn off it. Or else the device can be dead.

  1. Not finishing the message transmission process
  2. Being configured

Flash Application Firmware

note

Before flashing the firmware, please make sure that the indicator you purchased is the version for Meshtastic. Do not flash the Meshtastic firmware onto an indicator that is not compatible with Meshtastic. This may cause hardware damage. Please don't use NRF-OTA to update the firmware, it may cause the device to be completely dead.

Video Instruction

Visit Meshtastic Web Flasher.

Select the target device to Seeed SenseCAP Indicator and choose the latest firmware, then click Flash.

pir

Press and hold the button while plugging in the USB cable.

pir

Enable the Full Erase and Install, and click Erase Flash and Install.

There will show 2 ports, select the USB serial port and click Connect.

note

Please select the USB Serial one, not the INDICATOR RP2040.

pir

Flash GPS Firmware(optional)

The SenseCAP Indicator doesn't have a GPS built-in, to get the GPS location, a Grove GPS Module is required.
Connect the GPS Module to the Grove port and then flash the GPS firmware.

pir

Long press this internal button using a needle, then connect the device to your PC by the provided USB type-C cable, release the button once connected.

pir

Download the UF2 file and copy it to the RPI-RP2 drive. Firmware should be flashed after the file is downloaded and the device reboots.

pir

Download Meshtastic App:

Connect via App

  • Power on the device, the device page will display the mac address of the current device.

pir

  • Select the target device on the Bluetooth panel.

pir

  • Enter the code and then click Pair to connect the device.

pir

Configure the Parameters

In order to start communicating over the mesh, you must set your region. This setting controls which frequency range your device uses and should be set according to your regional location.

pir

Region List

Region CodeDescriptionFrequency Range (MHz)Duty Cycle (%)Power Limit (dBm)
UNSETUnsetN/AN/AN/A
USUnited States902.0 - 928.010030
EU_868European Union 868MHz869.4 - 869.651027

Refer to LoRa Region by Country for a more comprehensive list.

info

EU_868 has to adhere to an hourly duty cycle limitation of 10%, calculated every minute on a rolling 1-hour basis. Your device will stop transmitting if you reach it, until it is allowed again.

Now that you have set the LoRa region on your device, you can continue with configuring any LoRa Configs to suit your needs.

Keyboard

note

The keyboard usage of version 2.5.xx(The factory firmware is v2.5.11.) and version newer than 2.6.xx is different. Please check the following according to your current firmware version.

pir

For version2.5.xx

For version2.6 +

FAQ

RP2040 part

RP2040 has not been developed yet, so the buzzer/SD card/map functions are not available yet. We are working with Meshtastic to optimize it.

Role Selection

caution

DO NOT select the Repeater role, which will cause the device to repeatedly reboot.

GPS Module

If you didn't connect the GPS module, please disable the GPS function in the Meshtastic App, otherwise the device will keep trying to find the GPS module, which will cause the device to take a long time to boot up the screen.

pir

Tech Support & Product Discussion

Loading Comments...