Skip to main content

Complete Training Guide for SO-ARM with AmazingHand

This document explains how to combine the SO-ARM101 follower arm with the AmazingHand dexterous hand and perform teleoperation using LeRobot.

1. Hardware Connection​

  1. The STL file for the SOARM-to-AmazingHand adapter is available here:

lerobot/soarm_amazinghand_link_step_stl/step at soarm_amazinghand · xiehuangbao888/lerobot

  1. Remove the original SOARM gripper.
  1. Mount the SOARM-to-AmazingHand adapter onto the arm.
  1. Install the AmazingHand dexterous hand.
  1. Wire the devices as follows:
DeviceSerial PortDescription
SO-101 follower arm (gripper servo #6 removed)/dev/ttyACM0Only joint servos 1~5 are retained
SO-101 leader arm (gripper servo #6 retained)/dev/ttyACM1Gripper opening/closing used as input signal
AmazingHand dexterous hand/dev/ttyACM28 servos with IDs 1~8

If your serial ports differ, replace them with the actual port names in the following commands.


The robot will:

  • Control the 5 joints of the follower arm (servos 1~5) via /dev/ttyACM0.
  • Control the AmazingHand dexterous hand via /dev/ttyACM2.
  • Map the leader arm's gripper.pos proportionally to the dexterous hand's opening angle (0 = fully open, 100 = fully closed).

Calibration files are automatically saved to:

~/.cache/huggingface/lerobot/calibration/robots/so101_amazing_hand/<robot.id>.json
~/.cache/huggingface/lerobot/calibration/teleoperators/so101_leader/<teleop.id>.json

2. Environment and Connection​

git clone https://github.com/xiehuangbao888/lerobot.git

Switch to the existing lerobot virtual environment.

First, grant device permissions:

sudo chmod 666 /dev/ttyACM*

Step 1: Calibrate the Leader Arm​

cd ~/lerobot
conda activate lerobot
python -m lerobot.scripts.lerobot_calibrate \
--teleop.type=so101_leader \
--teleop.port=/dev/ttyACM1 \
--teleop.id=amazing_hand_leader

Follow the prompts:

  1. Place all joints of the leader arm at their mid positions and press Enter.
  2. Move each joint to its maximum and minimum ranges in turn, then press Enter to finish.

Step 2: Calibrate the Follower Arm​

python -m lerobot.scripts.lerobot_calibrate \
--robot.type=so101_amazing_hand \
--robot.port=/dev/ttyACM0 \
--robot.id=amazing_hand_follower \
--robot.hand_port=/dev/ttyACM2

Follow the prompts:

  1. Place the 5 joints of the follower arm at their mid positions and press Enter.
  2. Move the 5 joints to their maximum and minimum ranges in turn, then press Enter to finish.

Note: The follower arm has only 5 joints; gripper servo #6 has been removed.

Step 3: Run Teleoperation​

python -m lerobot.scripts.lerobot_teleoperate \
--robot.type=so101_amazing_hand \
--robot.port=/dev/ttyACM0 \
--robot.id=amazing_hand_follower \
--robot.hand_port=/dev/ttyACM2 \
--teleop.type=so101_leader \
--teleop.port=/dev/ttyACM1 \
--teleop.id=amazing_hand_leader \
--display_data=true

You can customize the grasping motion. The relevant file is located at:

src/lerobot/robots/so_amazing_hand/config_so_amazing_hand.py

3. Collect Dataset with the Dexterous Hand​

python -m lerobot.scripts.lerobot_record \
--robot.type=so101_amazing_hand \
--robot.port=/dev/ttyACM0 \
--robot.id=amazing_hand_follower \
--robot.hand_port=/dev/ttyACM2 \
--robot.cameras='{
wrist: {type: opencv, index_or_path: 2, width: 640, height: 480, fps: 30},
top: {type: opencv, index_or_path: 4, width: 640, height: 480, fps: 30}
}' \
--teleop.type=so101_leader \
--teleop.port=/dev/ttyACM1 \
--teleop.id=amazing_hand_leader \
--display_data=true \
--dataset.repo_id=seeed/amazing_soarm \
--dataset.num_episodes=20 \
--dataset.single_task="Pick up the cube with the dexterous hand"

Parameter descriptions:

ParameterDescription
--robot.camerasCamera configuration; supports opencv, realsense, etc. index_or_path is the camera index or video stream path.
--dataset.repo_idDataset ID on Hugging Face, in the format {username}/{dataset_name}.
--dataset.num_episodesNumber of episodes to record.
--dataset.single_taskTask description written into the dataset metadata.
--robot.hand_use_proportional_controlDefaults to true; no need to set it explicitly. Set to false for binary open/close behavior.

4. Training Policy​

lerobot-train \
--dataset.repo_id=seeed/amazing_soarm \
--policy.type=act \
--output_dir=outputs/train/amazing_soarm \
--job_name=amazing_soarm \
--policy.device=cuda \
--wandb.enable=false \
--policy.push_to_hub=false \
--steps=60000 \

5. Evaluation and Deployment​

Evaluate the Trained Policy on the Real Robot​

python -m lerobot.scripts.lerobot_record \
--robot.type=so101_amazing_hand \
--robot.port=/dev/ttyACM0 \
--robot.id=amazing_hand_follower \
--robot.hand_port=/dev/ttyACM2 \
--robot.cameras='{
wrist: {type: opencv, index_or_path: 0, width: 640, height: 480, fps: 30},
top: {type: opencv, index_or_path: 4, width: 640, height: 480, fps: 30}
}' \
--policy.path=outputs/train/amazing_soarm/checkpoints/last/pretrained_model \
--dataset.repo_id=seeed_val/amazinghand_pick_cube_eval \
--dataset.num_episodes=10 \
--dataset.single_task="Pick up the cube with the dexterous hand" \
--display_data=true
Loading Comments...