Skip to main content

Edge License Plate Recognition — Selection, Deployment and Measured Data

Before you use it

Supports mainland China single-row blue plates (7 characters) and green new-energy plates (8 characters); two-row, special-purpose and overseas plates are not supported. The licence of the detection and recognition weights is not yet confirmed; confirm it before commercial distribution.

What this solution does​

Keep the network cameras already mounted at the gate and add one recognition host on site to read plates. When a whitelisted vehicle arrives, the gate controller sends the barrier one opening signal; every vehicle leaves a record with its plate number, confidence and a snapshot. It fits residential, campus and staff car-park gates, and can also run without a barrier as an entry/exit log.

  • Plates and video stay on site

    Recognition runs on the host on site. Snapshots stay there for 7 days by default and leave only when fetched by link.

  • 30 fps at 1080p

    reComputer J30 Series and RK3576 Series both process 1080p at 29–30 fps; see "Performance and measured data".

  • Keep your cameras

    Existing 1080p network cameras connect over RTSP; the host pulls the stream across the LAN.

  • One record per vehicle

    Each vehicle is reported once with plate number, plate type, confidence and a snapshot link; a parking system subscribes to one MQTT topic.

On a real device​

The recognition host's own browser preview page: the plate is boxed and labelled with its number and confidence, and the last five reads are listed on the right.

Plate preview on a reComputer J30 Series: blue plate 皖A62599 read at 0.98, with the last five reads on the right

The input frames are stills from the CCPD public test set (MIT licence) looped over RTSP, not site footage.

reComputer J30 Series reading the green new-energy plate 皖AF10528 at 0.87

Hardware you need​

Three things on site: the gate camera, one recognition host, and, for automatic opening, a gate controller plus an interposing relay.

① Gate camera: your existing network camera, 1080p or better, with an RTSP stream.

② Recognition host: pick one; one host per gate camera.

Recognition hostMeasured (1080p input)Choose it when
reComputer Super J3011reComputer Super J3011
Jetson Orin Nano, JetPack 6.2
30 fpsDefault choice
reComputer Super J4012reComputer Super J4012
Jetson Orin NX, JetPack 6.2
Same package as J30The host also runs other models
reComputer RK3588reComputer RK3588 Series
On-board NPU
Deployment and output measuredThe site standardises on Rockchip
reComputer RK3576reComputer RK3576 Series
On-board NPU
29–30 fpsCost comes first

③ Gate controller (optional): reComputer R1100 Series (R1124-10). It runs the MQTT broker, holds the whitelist, and signals the barrier from a digital output through a DIN-rail interposing relay. Closing stays with the barrier's own loop or radar.

Camera, recognition host and gate controller sit on the same LAN; wired connections are recommended.

Deploying on site​

1. Mount the camera​

The plate must be legible in the picture

Mount the camera 3–8 m from the lane at a fixed position, aimed where plates pass. Recognition only runs inside a configured region of the picture (the lower middle by default); check that region again whenever the camera moves.

2. Install the software: three steps​

Device-by-device steps are on the reference design page; this is the outline.


  1. Gate controller (optional): install the MQTT broker and the gate service on the R1124-10, upload the whitelist CSV, and confirm the barrier moves with the test-open endpoint.
  2. Recognition host: enter the camera's RTSP address and the MQTT broker address, then deploy. The first deployment downloads the runtime and models; after that it runs offline.
  3. Check: open the preview page on port 8080 of the host; passing vehicles show a boxed plate, and the plate topic carries one record per vehicle.

Before going live, check the reads against real plates using daytime and night footage from your own gate.

Interfaces​

Results go over MQTT to the broker you entered at deployment (usually the R1124-10); snapshots and status use HTTP.

  • Parking or billing system: subscribe to the plate topic, one record per vehicle; reconcile on plate_normalized.
  • Barrier: the R1124-10 checks each plate record against the whitelist and publishes the result on the gate topic. The same plate arriving again within the cooldown is logged as suppressed and does not reopen.
  • Your own system: fetch the snapshot by the link in the record, or monitor the service through the health endpoint.
Topic / portContent
MQTT <site>/parking/<camera>/platePlate number, plate type (cn_blue / cn_green), confidence, voting frames, position in the picture, snapshot link
MQTT <site>/parking/<camera>/gateGate record: open_pulse (opened) or suppressed, with the matching plate record and whitelist label
MQTT <root>/statusService status, published periodically; the last one stays on the broker if the host goes offline
HTTP 8080 /snapshots/{seq}.jpgSnapshot linked from the plate record, kept 7 days by default
HTTP 8081 /whitelist (R1124-10)GET returns the whitelist CSV, PUT replaces it (a 400 names the failing line); POST /gate/test fires one test opening
HTTP 8099 /healthzService status including processing speed

Snapshots are not embedded in records; a record carries only the link and the snapshot's sha256.

Performance and measured data​

Processing speed​

DeviceProcessing speedPlate detection per frameConditions
reComputer J30 Series (Orin Nano)29.9 fps (measured)p50 5.6 ms (measured)1080p RTSP at 30 fps
reComputer RK3576 Series29–30 fps (measured)p50 23.1 ms, recognition 1.8 ms (measured)Same

Reproduce: sensecraft-solutions/solutions/edge_plate_recognition (deployment package) with input clip plate-labeled40-1080p-120s.mp4

Plate reads​

Input is CCPD test-set plate stills, each held for several seconds, streamed at 1080p over RTSP. Ground truth comes from the CCPD file names.

DeviceInputResult
reComputer J30 Series40 stills56 plate records published, 50 match the ground truth (measured)
reComputer RK3576 Series40 stills57 plate records published, 51 match the ground truth (measured)
reComputer J30 Series8 stills5 read correctly, 3 produced no record, 0 wrong plates (measured)
reComputer RK3588 Series8 stills5 read correctly, 3 produced no record, 0 wrong plates (measured)

One still can produce more than one record while it stays on screen, so record counts exceed still counts. When a plate cannot be read the host publishes nothing: neither device published a wrong plate on the 8 stills.

Reproduce: sensecraft-solutions/solutions/edge_plate_recognition/gallery/ATTRIBUTION.md (file names and ground truth of the 8 stills)

Models and runtimes​

DeviceDetectionRecognitionRuntime
reComputer J30 / J40 SeriesYOLOX-Tiny, 640×640, FP16PlateRecNet (in-house), 96×32, FP16TensorRT, hardware decode
reComputer RK3588 / RK3576 SeriesYOLOX-Tiny, 640×640, INT8PlateRecNet, 96×32, INT8 (FP16 output layer)RKNN runtime 2.3.2, MPP hardware decode

Parameters that affect results (deployment package config/plate.json):

  • plate.roi: recognition region, lower middle of the picture by default. Redraw it after the camera moves.
  • plate.vote: up to 7 frames vote per vehicle; a record is published when at least 3 agree with confidence 0.6 or higher.
  • plate.dedup_s: the same plate is published at most once in 30 s.

Known degradation​

  • Unsupported plate types: Supports single-row blue (7-character) and new-energy green (8-character) plates only. Double-row yellow, trailers, police and overseas plates are not supported.
  • Camera angle and speed: Vehicles must enter at an angle ≤ 30° with plate width > 96 pixels in the frame. Acute entry angles (> 45°) or speeds over 30 km/h degrade detection.
  • Glare and headlight overexposure: Direct glare or high-beam headlights at night can wash out characters. Even supplemental lighting (~5000K) is recommended in unlit gates.

Data and asset sources​

  • CCPD (Xu, Z. et al., ECCV 2018): github.com/detectRecog/CCPD, MIT License, Copyright (c) 2017 CCPD. The screenshots on this page use its test-set images; the plates are real plates from the public dataset.
  • Detection model code YOLOX: Apache-2.0. The recognition model structure is in-house code. The licence of both sets of trained weights is not yet confirmed; confirm it before commercial distribution.
Loading Comments...