Skip to main content

HVAC Setpoint Control on an Edge Gateway: Hardware, Deployment, and Measured Results

Usage notice

This is a supervisory setpoint recommender, not a safety-certified control system: the plant's own interlocks and safety controls take precedence, and no energy-saving figure is given.

What this solution does​

A central HVAC plant in an office, a mall or a factory usually runs to a fixed schedule: the same setpoint whether the floor is full or empty. This solution puts a gateway beside the plant that reads the HVAC controller and an energy meter into one point model, learns a setpoint recommendation from that building's own historical data, and writes it back to the controller; a write counts as applied only after the value has been read back from the field and matches what was sent.

It is used on central plant: chillers, air handlers, and the controllers in front of them. It is not for split-unit air conditioners, and it is not on the safety loop.

  • Selection and deployment: reference design page
  • Source repository: not published. github.com/Seeed-Solution/Solution_HVAC_SmartControl is not publicly accessible.
  • Existing controllers and meters connect as they are

    Controllers that speak OPC UA, Modbus TCP, Modbus RTU over RS-485 or BACnet/IP are not replaced, and the SDM630 meter has a built-in template. Up to 2,000 points, of which up to 50 may be writable.

  • Every write is read back and verified

    Last-known-good value, quality, timestamp and priority are frozen before the write; the point is re-read after a settle delay and compared within a tolerance. A readback whose quality is not good does not pass.

  • Automatic rollback and alarms on faults

    Readback mismatch, source offline, prediction disabled, operator abort and a partially applied batch all trigger a rollback. Alarms are keyed by cause, so a repeating fault re-uses the open alarm.

  • Measured capacity: 2,000 points at 349.99 events/s

    Against a 350.0 target, measured in one 180 s loopback run on a reComputer R2000 series. Conditions are in the appendix.

What the console shows​

The running console renders the point table with per-point quality, the access page with each source and its registered point count, and a command-receipt ledger. The ledger is where the write path is visible: each row carries the requested value, the effective value, the actor, the protocol acknowledgement and — after the settle delay — the readback result. A write whose register was changed out of band reads mismatched, compensated with the value that was found, and the compensation command issued by plugin:prediction:rollback appears as the next row.

The access page lists every source with its registered point count; this is the first place wiring shows up as working:

Access page: protocol, address, online state and registered point count for each source

The point table carries per-point quality, so a point that is not reading good is visible here:

Point table: name, current value, unit, quality and last update

The prediction runtime page shows this round's recommended setpoints, the history window behind them and the current control mode:

Prediction runtime page: this round's recommended setpoints, history window and control mode

The write path is visible in the command receipt ledger — requested value, effective value, actor, protocol acknowledgement and readback each get a column:

Command dispatch step two: confirm the value to write, the target point and the safety limits

The captures above are connected to the package's own protocol simulators, not to a physical meter or controller; the gateway side runs the shipped software.

What hardware you need​

Three things: a controller you already have, a meter, and one Docker host.

① The HVAC controller — whatever is already in front of the plant, as long as it speaks OPC UA, Modbus TCP/RTU or BACnet/IP. For a dry run with no plant attached, the package ships an OPC UA simulator on port 4841.

② The energy meter — an Eastron SDM630 on the Modbus V2 register map, over Modbus TCP, a Modbus TCP gateway, or RS-485. Ten read-only points: three-phase voltage and current, total active power (kW), total power factor, frequency, imported active energy (kWh).

③ The gateway host — the only device you need to choose. The service is a Docker workload on x86-64 or arm64, so a Linux machine already on the plant network is a supported target.

GatewayStorageWhen to choose it
reComputer R1124-10reComputer R1124-10
4 GB RAM, RS-485 / RS-232 / DI / DO on board
16 GB eMMCThe history lives on a server; the gateway keeps a short local window
reComputer R1125-10reComputer R1125-10
same board, larger eMMC
32 GB eMMCMonths of operating history stay on the gateway; the training set can be re-imported locally

The R1100 series carries RS-485 on board, so a meter on RS-485 needs no USB adapter. The service itself needs about 1 GB of disk; storage decides how much history you can look back on locally without a server.

Other prerequisites: Docker Engine 20.10 or newer, host ports 8280 and 4841 free, and at least one week of historical operation as CSV or Excel with timestamp, setpoint, measured temperature and power consumption columns.

Negative Selection Boundaries​

  • Local Storage Horizon: R1124-10 (16GB eMMC) stores a short local window; if you require months of high-frequency telemetry stored on-premise for offline model retraining, choose R1125-10 (32GB).
  • Safety Interlocks: This gateway provides advisory setpoints; never wire it into emergency boiler or chiller safety cut-off circuits requiring certified safety controllers.

How to deploy on site​

1. Install the hardware: wiring​

Check the meter's byte and word order first

The built-in SDM630 template defaults to big-endian bytes and words, taken from the vendor's published default. Read a register with a known physical value and compare against the meter's own display. Voltage and frequency that are close but wrong, or imported energy that jumps backwards, usually mean a word-order setting error; check word order before wiring.

Put the gateway on the same network as the controller and the meter (or its Modbus TCP gateway). For Modbus RTU, match the baud rate, parity and unit id to what the meter is configured for ; a mismatch shows only as a timeout, with no error message. Use the serial-device deployment profile: the standard Docker profile attaches no host serial device, so there is no /dev/ttyUSB0 inside the container.

2. Software: three steps​

The per-step form fields and application packages are on the reference design page; pick a configuration for your site and download.


Outline:

  1. Deploy the service — Docker deployment, either on the machine running the deployment tool or over SSH to a device on the plant network. The form carries the meter transport, the OPC UA endpoint, the safety limits, the control mode and the alarm thresholds.
  2. Open the console — create the first administrator and confirm both sources are online with their expected point counts. The access wizard asks for address and poll interval per protocol:
Access wizard step one: choose the protocol, fill in the address and poll interval
  1. Commission — register the meter, run predictions in observe mode, inject faults on purpose, and only then enable writes. Before a batch goes out, confirm on the selection page exactly which points it covers:
Batch dispatch selection: the points covered by this batch and their current values

Leave Control Mode at observe and leave Safety Baseline Approved By blank. While the approver is blank the baseline shows as unapproved; entering a name means that engineer signs off the safety limits.

The estimate to a running console with points reading is about 60 minutes. Commissioning takes longer, because it includes a full occupancy cycle of observe-mode predictions reviewed by whoever operates the plant.

What the published image covers

The published missionpack-knn:v1.6.5 does not carry the SDM630 template, the rollback coordinator or the alarm envelope. On v1.6.5 the observe-mode substeps still apply; the meter, rollback and alarm substeps cannot be completed.

Available interfaces​

Everything the deployment exposes sits behind one HTTP port on the gateway host. Nothing leaves the plant network unless northbound publishing is turned on.

  • Operators — the browser console on 8280: point table with per-point quality, meter registration, prediction runs, command receipts, alarm banner.
  • Monitoring — GET /system/runtime-metrics. With northbound publishing enabled it carries northbound.spool.queued and northbound.spool.dropped; queued back to 0 with dropped unchanged is the check the commissioning step asks for.
  • Your own system — the same console API surface behind 8280, plus the health endpoint the deployment waits on at startup.

Full endpoint list​

Port / endpointWhat it servesNeeds internet
8280 /Browser consoleNo
8280 /system/runtime-metricsRuntime counters, northbound spool countersNo
8280 /api/v1/healthHealth check; startup allows 30 sNo
4841Built-in OPC UA simulator, for a dry runNo

On a command receipt, read the readback column: protocol_acknowledged only means the controller accepted the frame. The readback column (matched, or mismatched, compensated with the value found) is what the field actually holds. A compensation issued by the rollback coordinator appears as its own receipt immediately after the write it undid, so the audit trail reads in order without joining two tables.

Container logs rotate at 10 MB with four backups (docker logs missionpack_knn). Export the command audit trail, the rollback journal and the alarm history before they age away.

Southbound protocol scope​

All points sit in one registry, capped at 2,000 points, of which at most 50 may be writable. The 10 SDM630 meter points are read-only; they count toward the 2,000 and not toward the 50.

TransportRoleConstraints
OPC UARead and write on the HVAC controllerEndpoint set per deployment; built-in simulator on 4841
Modbus TCPMeter and controllersUnit id and port per source; direct or through a TCP gateway
Modbus RTU (RS-485)MeterNeeds the serial-device deployment profile; the standard profile does not attach host serial devices
BACnet/IPRead and write on air handlersWrites use a priority and release with Null. COV subscription, BBMD registration and MS-TP are not implemented

Performance and measured data​

Everything here was measured against the protocol simulator over loopback; there is no building site data, and each figure comes from a single run unless stated otherwise.

Capacity​

MetricValueConditions
Sampling throughput349.99 events/s (99.99% of the 350.0 target)2,000 points, 4 protocol sources
Prediction rate0.939 cycle/sSame run
Peak process-group RSS217.3 MiBSame run

Conditions for all three rows: 2,000 points across 4 protocol sources, OPC UA and Modbus sampled every 5 s, BACnet every 10 s, loopback only, 180 s run, on a reComputer R2000 series (arm64).

Reproduce: upstream b5fe4cc, capture capacity-smoke r14

Latency​

MetricValueConditions
Prediction cycle latency46.27 ms maxn = 4 cycles, no load
Control admission latency1.41 ms maxn = 2 cycles, no load

Both reflect only the cost of the code path itself.

Reproduce: upstream f831bae, runtime baseline of northbound-smoke

Runtime and key parameters​

The prediction model is KNN, trained on the building's own operating history (CSV or Excel with timestamp, setpoint, measured temperature and power columns); the service is a Docker workload on x86-64 or arm64. Each prediction can be reviewed in the console before it goes to the controller.

  • Control mode and safety limits: control mode ships as observe, so no point is written until an operator changes it. The setpoint minimum / maximum of 18 / 30 °C, the maximum change of 1.0 °C per 300 s and the mode whitelist off / fan / cool / heat / auto are all placeholders; fill them in for the plant.
  • Write-back verification is off by default: the prediction-run config (created in the console) must state "rollback": { "enabled": true, "settle_seconds": 2.5 } explicitly; a config without a rollback section is treated as enabled: false.
  • settle_seconds (0–30, default 1.0) must be longer than the source's sampling interval, or the readback sees the pre-write value and reports a mismatch that does not exist.

Known degradation​

  • The prediction rate has a structural ceiling (not fixed): the prediction loop sleeps a fixed interval after each cycle, so its rate is 1/(1.0 + t_cycle). At 2,000 points t_cycle is about 0.119 s, which puts the ceiling near 0.894 cycle/s, below the 0.90 gate the soak test requires.
  • Only Modbus writes are verified by readback: a BACnet output has no write priority available and is skipped.
  • Byte order: until checked against the meter's own display, meter points are decoded with the vendor-default (big-endian) word order and may be wrong.

Next steps​

  • Read/write with independent readback against real OPC UA, Modbus TCP, Modbus RTU (USB-to-RS-485) and BACnet/IP devices on a reComputer R10 series or reTerminal DM.
  • A 72-hour unattended run on the same target hosts, with network, broker, process and device recovery drills during the run.

Data and asset sources​

  • SDM630 register map — Eastron's published Modbus protocol document (Modbus V2 register map, IEEE-754 float32 input registers). Addresses follow that document; the big-endian byte and word order is the vendor default.
  • Historical operation data — supplied by the deploying site. Nothing is distributed with the package, and no public dataset is used or required.
  • Console captures — original screen captures of the packaged software running against the package's own protocol simulators. The simulator configuration, capture host and checksums are recorded in the package's gallery/ATTRIBUTION.md. No third-party asset, brand mark or stock image is included.
  • Architecture diagram — drawn from a structured architecture IR; original work, no third-party art.
Loading Comments...