Skip to main content

Getting Started with Sound Event Detection Module

Introduction

A compact edge audio board delivers real-time sound detection with strong local data privacy protection. It detects five abnormal sound events — Baby Cry, Glass Break, Gunshot, T3/T4 Alarms, and Snore, enabling immediate response and reliable early warning. Designed for native ESPHome integration with seamless compatibility for Home Assistant with XIAO series, ideal for home security monitoring or responsive automation triggers.

pir

Specification

FeatureDescription
Core ChipXMOS XU316-1024-QF60BC24
Supported EventsBaby Cry / Glass Break / Gunshot / Smoke Alarm & CO Alarm (T3/T4) / Snoring
Digital MicrophonesHigh-performance digital microphones × 1
Sensitivity-26 dBFS
Acoustic Overload Point120 dBL
SNR64 dBA
Power SupplyUSB 5V, External 5V
Dimensions40 × 20 mm
Operating Temperature0℃ – 65℃

Hardware Overview and Dimensions

Front View

pir

Back View

pir

USB Usage

This device can operate in standalone mode and supports plug-and-play communication through the USB interface using AT commands.

First, connect the device to your computer using a USB Type-C to USB Type-A cable.

  • Step 1 :Next, open PuTTY or any other serial terminal software. If you have not installed one yet, you can download PuTTY from the following link:

  • Step 2 :After opening the serial terminal, select the correct COM port and set the baud rate to 115200. Once connected, you will be able to interact with the device through the USB interface.

pir

Since the device continuously listens for sound events, you can test it by generating supported sound events near the device.

pir

Furthermore, you can adjust device parameters using AT commands. Below are some commands you can use to interact with the device.

CommandDescriptionExample
AT+GETDETECTGet currently enabled detection types (1–5 types).AT+GETDETECT+GETDETECT:baby_cry,glass_break
AT+SETDETECT=<types>Set event types to detect (comma-separated, maximum of 5).AT+SETDETECT=baby_cry,snore
AT+GETEVENTTHRESHOLD=<type>Get the confidence threshold for a specific event.AT+GETEVENTTHRESHOLD=baby_cry+GETEVENTTHRESHOLD:baby_cry,70
AT+SETEVENTTHRESHOLD=<type>,<val>Set the confidence threshold for a specific event.AT+SETEVENTTHRESHOLD=baby_cry,75
AT+GETSUPPORTEDLISTList all event types supported by the device.AT+GETSUPPORTEDLIST+GETSUPPORTEDLIST:doorbell,glass_break,baby_cry,...
AT+SETOUTPUTTYPE=<type>Set what gets output when an event is detected.AT+SETOUTPUTTYPE=highest_confidence
AT+GETINTMODEGet the current interrupt mode.AT+GETINTMODE+GETINTMODE:single
AT+SETINTMODE=<mode>Set the interrupt operation mode.AT+SETINTMODE=continuous
AT+RESETINTReset interrupt status and pull the INT_N pin HIGH.AT+RESETINT
AT+SAVECONFIGSave the current configuration so it persists after reboot.AT+SAVECONFIG
AT+GETFWVERSIONGet the firmware version string.AT+GETFWVERSION+GETFWVERSION:1.0.2
AT+RESETRestore default settings and restart the device (clears all custom configuration).AT+RESET

When an event is detected the device automatically sends:

+EVENT: <event_id>,<confidence>

Example: +EVENT: 1,87 → event ID 1 (baby_cry), 87% confidence


AT+SETOUTPUTTYPE values

ValueBehaviour
highest_confidenceOnly the single top-confidence event is reported
all_eventsAll detected events are reported each detection cycle

AT+SETINTMODE values

ValueBehaviour
singleINT_N fires once, then must be reset with AT+RESETINT
continuousINT_N fires continuously while event is detected

Arduino Usage

Plug XIAO

This device supports XIAO modules and can be connected to any available UART pins on the board. It is compatible with ESP32S3, ESP32C6, and ESP32C3 modules, so you only need to modify the RX and TX pin definitions in the code accordingly. Plug the device in the same orientation as shown in the images.

pir

Download the Library

  • Go to the GitHub repository Link
  • Click the green "Code" button
  • Select "Download ZIP"
  • Save the file (e.g., AudioEventSensor-main.zip) to your computer

pir

Install the Library in Arduino IDE

  • Open Arduino IDE
  • Go to Sketch → Include Library → Add .ZIP Library...
  • Navigate to your downloaded ZIP file
  • Click "Open" to install

pir

Verify Installation

Go to File → Examples → AudioEventSensor to see example sketches

pir

Change the UART Pins

According to your XIAO board, you should change the UART pin definitions in the code. In this example, we use the XIAO ESP32S3.

#define UART1_TX 43
#define UART1_RX 44

Basic Usage

After you flash to ESP32,this code initializes an Audio Event Sensor over UART and configures it to detect specific sound events such as gunshot and glass break. During setup, it resets the device, reads the firmware version, retrieves the list of supported sound events, and sets detection thresholds for each selected event. The configuration is then saved so the settings persist after reboot. In the main loop, the program continuously listens for detected sound events and prints them to the serial monitor in real time. This allows the system to act as an early warning and monitoring solution for abnormal acoustic events.

pir

Bonus : Email Notifications

  • First, you need to create an App Password. Please refer to this guide
  • Next, download and install the required supporting libraries.Install the ESP Mail Client library from the Arduino Library Manager.

pir

Code

Email Ino
#include <WiFi.h>
#include <ESP_Mail_Client.h>
#include <AudioEventSensor.h>

// WiFi credentials
#define WIFI_SSID "WIFI-SSID"
#define WIFI_PASSWORD "PASSWORD"

// Email credentials
#define SENDER_EMAIL "[email protected]"
#define SENDER_PASSWORD "abcd efgh ijkh xvyz"
#define RECIPIENT_EMAIL "[email protected]"

#define SMTP_HOST "smtp.gmail.com"
#define SMTP_PORT 587

// UART pins for audio sensor
#define UART1_TX 43
#define UART1_RX 44

// Cooldown period in milliseconds (30 seconds)
#define EVENT_COOLDOWN_MS 30000

// Event tracking structure
struct EventTracker {
String eventType;
unsigned long lastTriggerTime;
int detectionCount;
};

// Track multiple event types
EventTracker events[] = {
{"baby_cry", 0, 0},
{"glass_break", 0, 0},
{"gunshot", 0, 0},
{"snore", 0, 0},
{"T3", 0, 0},
{"T4", 0, 0}
};
const int EVENT_COUNT = 6;

SMTPSession smtp;
AudioEventSensor audio(Serial1);

void setup() {
Serial.begin(115200);
delay(1000);

Serial1.begin(115200, SERIAL_8N1, UART1_RX, UART1_TX);
audio.begin(115200);

Serial.println("=================================");
Serial.println("Audio Event Email Alert System");
Serial.println("=================================\n");

// Connect to WiFi
WiFi.begin(WIFI_SSID, WIFI_PASSWORD);
Serial.print("Connecting to Wi-Fi");

while (WiFi.status() != WL_CONNECTED) {
Serial.print(".");
delay(300);
}

Serial.println();
Serial.print("Connected with IP: ");
Serial.println(WiFi.localIP());
Serial.println();

// Initialize audio sensor
Serial.println("Initializing audio sensor...");
delay(2000);

audio.resetDevice();
delay(500);

// Get firmware version
String firmwareVersion;
if (audio.getFirmwareVersion(firmwareVersion)) {
Serial.print("Firmware version: ");
Serial.println(firmwareVersion);
}

// Configure detection
Serial.println("Setting detection types...");
if (audio.setDetectTypes("gunshot,glass_break,baby_cry,snore,T3")) {
Serial.println("✓ Detection types set: gunshot, glass_break");
} else {
Serial.println("✗ Failed to set detection types");
}
delay(500);

// Set thresholds
audio.setEventThreshold("glass_break", 60);
audio.setEventThreshold("gunshot", 65);
delay(500);

// Save configuration
audio.saveConfig();
delay(500);

Serial.println("\n=================================");
Serial.println("System ready. Monitoring events...");
Serial.println("=================================\n");
}

void loop() {
// Check for audio events
if (audio.available()) {
String eventData = audio.readEvent();

if (eventData.length() > 0) {
Serial.print("[" + getTimestamp() + "] ");
Serial.println(eventData);

// Extract event type from the event string
String eventType = extractEventType(eventData);
int confidence = extractConfidence(eventData);

// Check if we should send an email for this event
if (shouldSendEmail(eventType)) {
Serial.println("\n>>> ALERT: New " + eventType + " detected!");
Serial.println(">>> Sending email notification...");

sendEventEmail(eventType, confidence);

Serial.println(">>> Email sent. Cooldown active for " +
String(EVENT_COOLDOWN_MS/1000) + " seconds.\n");
}
}
}

delay(100);
}

// Extract event type from event string (e.g., "glass_break 95% confidence")
String extractEventType(String eventData) {
int spaceIndex = eventData.indexOf(' ');
if (spaceIndex > 0) {
return eventData.substring(0, spaceIndex);
}
return eventData;
}

// Extract confidence from event string
int extractConfidence(String eventData) {
int percentIndex = eventData.indexOf('%');
if (percentIndex > 0) {
// Find the last space before %
int lastSpace = eventData.lastIndexOf(' ', percentIndex);
if (lastSpace > 0) {
String confStr = eventData.substring(lastSpace + 1, percentIndex);
return confStr.toInt();
}
}
return 0;
}

// Check if enough time has passed since last email for this event type
bool shouldSendEmail(String eventType) {
unsigned long currentTime = millis();

for (int i = 0; i < EVENT_COUNT; i++) {
if (events[i].eventType == eventType) {
// Check if cooldown period has passed
if (currentTime - events[i].lastTriggerTime >= EVENT_COOLDOWN_MS) {
// Update last trigger time
events[i].lastTriggerTime = currentTime;
events[i].detectionCount++;
return true;
} else {
// Still in cooldown period
unsigned long timeRemaining = EVENT_COOLDOWN_MS - (currentTime - events[i].lastTriggerTime);
Serial.println(" ⏳ Cooldown active. " + String(timeRemaining/1000) + "s remaining.");
return false;
}
}
}

return false; // Unknown event type
}

// Send email notification
void sendEventEmail(String eventType, int confidence) {
// Prepare email subject and body
String subject = "🚨 ALERT: " + formatEventName(eventType) + " Detected!";

String body = "SECURITY ALERT\n";
body += "═══════════════════════════════\n\n";
body += "Event Type: " + formatEventName(eventType) + "\n";
body += "Confidence: " + String(confidence) + "%\n";
body += "Time: " + getTimestamp() + "\n";
body += "Device: ESP32 Audio Sensor\n";
body += "Location: [Your Location]\n\n";
body += "═══════════════════════════════\n";
body += "This is an automated alert from your audio monitoring system.\n";

// Send the email
gmail_send(subject, body);
}

// Format event name for display
String formatEventName(String eventType) {
if (eventType == "glass_break") return "Glass Breaking";
if (eventType == "gunshot") return "Gunshot";
if (eventType == "baby_cry") return "Baby Crying";
if (eventType == "snore") return "Snoring";
return eventType;
}

// Get formatted timestamp
String getTimestamp() {
unsigned long seconds = millis() / 1000;
unsigned long minutes = seconds / 60;
unsigned long hours = minutes / 60;

seconds = seconds % 60;
minutes = minutes % 60;
hours = hours % 24;

char timestamp[12];
sprintf(timestamp, "%02lu:%02lu:%02lu", hours, minutes, seconds);
return String(timestamp);
}

// Gmail send function
void gmail_send(String subject, String textMsg) {
MailClient.networkReconnect(true);

smtp.debug(0); // Set to 1 for debug output
smtp.callback(smtpCallback);

Session_Config config;
config.server.host_name = SMTP_HOST;
config.server.port = SMTP_PORT;
config.login.email = SENDER_EMAIL;
config.login.password = SENDER_PASSWORD;
config.login.user_domain = F("127.0.0.1");
config.time.ntp_server = F("pool.ntp.org,time.nist.gov");
config.time.gmt_offset = 3;
config.time.day_light_offset = 0;

SMTP_Message message;
message.sender.name = F("ESP32 Security System");
message.sender.email = SENDER_EMAIL;
message.subject = subject;
message.addRecipient(F("Security Admin"), RECIPIENT_EMAIL);
message.text.content = textMsg;
message.text.transfer_encoding = "base64";
message.text.charSet = F("utf-8");
message.priority = esp_mail_smtp_priority::esp_mail_smtp_priority_high;
message.addHeader(F("Message-ID: <[email protected]>"));

if (!smtp.connect(&config)) {
Serial.printf("✗ Connection error, Status Code: %d, Error Code: %d, Reason: %s\n",
smtp.statusCode(), smtp.errorCode(), smtp.errorReason().c_str());
return;
}

if (!MailClient.sendMail(&smtp, &message)) {
Serial.printf("✗ Send error, Status Code: %d, Error Code: %d, Reason: %s\n",
smtp.statusCode(), smtp.errorCode(), smtp.errorReason().c_str());
} else {
Serial.println("✓ Email sent successfully!");
}
}

void smtpCallback(SMTP_Status status) {
Serial.println(status.info());

if (status.success()) {
Serial.println("────────────────────");
Serial.printf("✓ Message sent: %d\n", status.completedCount());
Serial.printf("✗ Message failed: %d\n", status.failedCount());
Serial.println("────────────────────\n");
smtp.sendingResult.clear();
}
}



Then, replace the following parameters in the code with your own values: the sender email address, the UART pins, App Password, the receiver email address, and your Wi-Fi SSID and password.

pir

Tech Support & Product Discussion

Thank you for choosing our products! We are here to provide you with different support to ensure that your experience with our products is as smooth as possible. We offer several communication channels to cater to different preferences and needs.

Loading Comments...