Skip to main content

Home Assistant and Sound Event Detection Module

Introduction

A compact edge audio board provides real-time sound detection with strong local data privacy protection. It can detect five abnormal sound events—Baby Cry, Glass Break, Gunshot, T3/T4 alarms, and Snore—enabling immediate response and reliable early warning. In this tutorial, we will learn how to compile and upload the firmware to a XIAO ESP32 board.

Hardware Required

ReSpeaker XVF3800 Home Assistant Yellow KitXiao ESP32S3

Install ESPHome Builder

Settings → Add-ons → Click on Add-on Store → Install ESPHome Device Builder add-on.

Go to Home Assistant > Settings > Add-ons.

pir

Click Add-on Store (usually at the bottom right)

pir

Under Official add-ons, search for and install ESPHome Device Builder.

pir

After installation, click Start to run the ESPHome add-on.

pir

Enable Start on Boot, Watchdog, and Show in Sidebar for easier access.

From the Home Assistant sidebar, go to ESPHome Builder.

Add Sound event device

Click + NEW DEVICE.

pir

Click Continue → New Device Setup, then provide an appropriate name for the device.

pir

pir

In this demo, we are using the XIAO ESP32-S3, so we will select ESP32-S3 as the target board. This may differ depending on the board you are using.

pir

Select your new device entry and click Edit. Delete the entire YAML template, then copy and paste the provided YAML file into the editor.

Sound Event YAML
##############################################################
# Sound Event Sensor - ESPHome Configuration
# Sensor: XU316 / AudioEventSensor (Seeed)
# Communication: UART via AT Commands
# No external .h file needed - pure YAML + inline lambdas
##############################################################

esphome:
name: sound-event-sensor
friendly_name: Sound Event Sensor

on_boot:
priority: -100 # Run after everything else is initialized
then:
- logger.log: "=== Sound Event Sensor Booting ==="

# Step 1: Wait for sensor to be ready
- delay: 2s

# Step 2: Reset device for clean state
- logger.log: "Resetting device..."
- uart.write:
id: uart_bus
data: "AT+RESET\r\n"
- delay: 3s # Wait for device to come back up after reset
- logger.log: "Device reset complete."

# Step 3: Get and log firmware version
- logger.log: "Requesting firmware version..."
- uart.write:
id: uart_bus
data: "AT+GETFWVERSION\r\n"
- delay: 500ms

# Step 4: Apply all settings from the configurable values below
- script.execute: apply_all_settings

- logger.log: "=== Setup complete. Monitoring for events... ==="


##############################################################
# Hardware Settings - Change these to match YOUR wiring
##############################################################
esp32:
board: esp32-s3-devkitc-1
variant: esp32s3
framework:
type: arduino
version: recommended


##############################################################
# Network
##############################################################
wifi:
ssid: !secret wifi_ssid
password: !secret wifi_password
ap:
ssid: "SoundSensor Fallback"
password: "soundsensor123"

captive_portal:

ota:
- platform: esphome
password: !secret ota_password

api:
id: api_id

logger:
level: DEBUG # Set to INFO to reduce log noise after testing


##############################################################
# UART - The serial link to your sensor
# Adjust tx_pin / rx_pin to match your wiring
##############################################################
uart:
id: uart_bus
tx_pin: GPIO43 # ← CHANGE to your TX pin
rx_pin: GPIO44 # ← CHANGE to your RX pin
baud_rate: 115200
debug: # Remove this block after testing
direction: BOTH
dummy_receiver: false


##############################################################
# Global Variables (internal state)
##############################################################
globals:
# UART line receive buffer
- id: uart_rx_buffer
type: std::string
restore_value: no
initial_value: '""'


##############################################################
# SCRIPTS
##############################################################
script:
- id: apply_all_settings
then:
# ── Build detect types from whichever switches are ON ──
- lambda: |-
std::string types = "";
auto add = [&](bool on, const char* name) {
if (on) { types += (types.empty() ? "" : ","); types += name; }
};
add(id(sw_detect_baby_cry).state, "baby_cry");
add(id(sw_detect_glass_break).state, "glass_break");
add(id(sw_detect_gunshot).state, "gunshot");
add(id(sw_detect_snore).state, "snore");
add(id(sw_detect_t3).state, "T3");
add(id(sw_detect_t4).state, "T4");
if (types.empty()) types = "gunshot"; // safety fallback
std::string cmd = "AT+SETDETECT=" + types + "\r\n";
ESP_LOGI("sound", "Setting detect types: %s", types.c_str());
id(uart_bus).write_array((const uint8_t*)cmd.c_str(), cmd.length());

- delay: 400ms

# ── Set thresholds for all 6 event types ──────────────
- lambda: |-
int val = (int) id(num_thr_baby_cry).state;
std::string cmd = "AT+SETEVENTTHRESHOLD=baby_cry," + std::to_string(val) + "\r\n";
ESP_LOGI("sound", "baby_cry threshold -> %d", val);
id(uart_bus).write_array((const uint8_t*)cmd.c_str(), cmd.length());
- delay: 400ms

- lambda: |-
int val = (int) id(num_thr_glass_break).state;
std::string cmd = "AT+SETEVENTTHRESHOLD=glass_break," + std::to_string(val) + "\r\n";
ESP_LOGI("sound", "glass_break threshold -> %d", val);
id(uart_bus).write_array((const uint8_t*)cmd.c_str(), cmd.length());
- delay: 400ms

- lambda: |-
int val = (int) id(num_thr_gunshot).state;
std::string cmd = "AT+SETEVENTTHRESHOLD=gunshot," + std::to_string(val) + "\r\n";
ESP_LOGI("sound", "gunshot threshold -> %d", val);
id(uart_bus).write_array((const uint8_t*)cmd.c_str(), cmd.length());
- delay: 400ms

- lambda: |-
int val = (int) id(num_thr_snore).state;
std::string cmd = "AT+SETEVENTTHRESHOLD=snore," + std::to_string(val) + "\r\n";
ESP_LOGI("sound", "snore threshold -> %d", val);
id(uart_bus).write_array((const uint8_t*)cmd.c_str(), cmd.length());
- delay: 400ms

- lambda: |-
int val = (int) id(num_thr_t3).state;
std::string cmd = "AT+SETEVENTTHRESHOLD=T3," + std::to_string(val) + "\r\n";
ESP_LOGI("sound", "T3 threshold -> %d", val);
id(uart_bus).write_array((const uint8_t*)cmd.c_str(), cmd.length());
- delay: 400ms

- lambda: |-
int val = (int) id(num_thr_t4).state;
std::string cmd = "AT+SETEVENTTHRESHOLD=T4," + std::to_string(val) + "\r\n";
ESP_LOGI("sound", "T4 threshold -> %d", val);
id(uart_bus).write_array((const uint8_t*)cmd.c_str(), cmd.length());
- delay: 400ms

# ── Save to sensor flash ───────────────────────────────
- logger.log: "Saving config to sensor..."
- uart.write:
id: uart_bus
data: "AT+SAVECONFIG\r\n"
- delay: 500ms
- logger.log: "Settings applied and saved!"


##############################################################
# INTERVAL - Parse incoming UART lines every 50ms
##############################################################
interval:
- interval: 50ms
then:
- lambda: |-
while (id(uart_bus).available()) {
uint8_t b;
id(uart_bus).read_byte(&b);
char c = (char)b;

if (c == '\n') {
std::string line = id(uart_rx_buffer);
id(uart_rx_buffer) = "";
if (!line.empty() && line.back() == '\r') line.pop_back();
if (line.empty()) continue;

ESP_LOGD("uart_rx", "<- %s", line.c_str());

// ── +EVENT: id,confidence ─────────────────────
if (line.size() > 7 && line.substr(0, 7) == "+EVENT:") {
std::string payload = line.substr(7);
while (!payload.empty() && payload[0] == ' ') payload.erase(0,1);

size_t comma = payload.find(',');
if (comma != std::string::npos) {
int event_id = std::stoi(payload.substr(0, comma));
int pct = (int) std::stof(payload.substr(comma + 1));

// ID map matches AudioEventSensor.cpp
const char* label_map[] = {"", "baby_cry", "glass_break", "gunshot", "snore", "T3", "T4"};
std::string name = (event_id >= 1 && event_id <= 6) ? label_map[event_id] : "unknown";
std::string full = name + " " + std::to_string(pct) + "% confidence";

id(txt_last_event_full).publish_state(full);
id(txt_last_event_name).publish_state(name);
id(sen_confidence).publish_state((float)pct);
ESP_LOGI("sound", "EVENT: %s", full.c_str());
}
}

// ── +GETFWVERSION:1.0.0 ───────────────────────
else if (line.size() > 14 && line.substr(0, 14) == "+GETFWVERSION:") {
std::string ver = line.substr(14);
while (!ver.empty() && ver[0] == ' ') ver.erase(0,1);
id(txt_firmware_version).publish_state(ver);
ESP_LOGI("sound", "Firmware: %s", ver.c_str());
}

else if (line == "OK") {
ESP_LOGD("sound", "<- OK");
} else if (line.size() >= 5 && line.substr(0, 5) == "ERROR") {
ESP_LOGW("sound", "<- ERROR: %s", line.c_str());
}

} else if (c != '\r') {
id(uart_rx_buffer) += c;
}
}


##############################################################
# SWITCHES
# All 6 events ON by default — user can disable any in HA
# After changing: press the "Apply Settings" button
##############################################################
switch:
- platform: template
name: "Detect Baby Cry" # Class ID 1
id: sw_detect_baby_cry
icon: mdi:baby-face-outline
optimistic: true
restore_mode: RESTORE_DEFAULT_ON # ← ON by default

- platform: template
name: "Detect Glass Break" # Class ID 2
id: sw_detect_glass_break
icon: mdi:glass-fragile
optimistic: true
restore_mode: RESTORE_DEFAULT_ON # ← ON by default

- platform: template
name: "Detect Gunshot" # Class ID 3
id: sw_detect_gunshot
icon: mdi:target
optimistic: true
restore_mode: RESTORE_DEFAULT_ON # ← ON by default

- platform: template
name: "Detect Snore" # Class ID 4
id: sw_detect_snore
icon: mdi:sleep
optimistic: true
restore_mode: RESTORE_DEFAULT_ON # ← ON by default

- platform: template
name: "Detect T3" # Class ID 5 (custom event)
id: sw_detect_t3
icon: mdi:waveform
optimistic: true
restore_mode: RESTORE_DEFAULT_ON # ← ON by default

- platform: template
name: "Detect T4" # Class ID 6 (custom event)
id: sw_detect_t4
icon: mdi:waveform
optimistic: true
restore_mode: RESTORE_DEFAULT_ON # ← ON by default


##############################################################
# NUMBER SLIDERS - Confidence thresholds
# All default to 80% — adjust per event in HA
# After changing: press the "Apply Settings" button
##############################################################
number:
- platform: template
name: "Baby Cry Threshold"
id: num_thr_baby_cry
icon: mdi:tune
unit_of_measurement: "%"
min_value: 0
max_value: 100
step: 5
initial_value: 80 # ← Default 80%
restore_value: true
optimistic: true

- platform: template
name: "Glass Break Threshold"
id: num_thr_glass_break
icon: mdi:tune
unit_of_measurement: "%"
min_value: 0
max_value: 100
step: 5
initial_value: 80 # ← Default 80%
restore_value: true
optimistic: true

- platform: template
name: "Gunshot Threshold"
id: num_thr_gunshot
icon: mdi:tune
unit_of_measurement: "%"
min_value: 0
max_value: 100
step: 5
initial_value: 80 # ← Default 80%
restore_value: true
optimistic: true

- platform: template
name: "Snore Threshold"
id: num_thr_snore
icon: mdi:tune
unit_of_measurement: "%"
min_value: 0
max_value: 100
step: 5
initial_value: 80 # ← Default 80%
restore_value: true
optimistic: true

- platform: template
name: "T3 Threshold"
id: num_thr_t3
icon: mdi:tune
unit_of_measurement: "%"
min_value: 0
max_value: 100
step: 5
initial_value: 80 # ← Default 80%
restore_value: true
optimistic: true

- platform: template
name: "T4 Threshold"
id: num_thr_t4
icon: mdi:tune
unit_of_measurement: "%"
min_value: 0
max_value: 100
step: 5
initial_value: 80 # ← Default 80%
restore_value: true
optimistic: true


##############################################################
# BUTTONS
##############################################################
button:
- platform: template
name: "Apply Settings"
id: btn_apply_settings
icon: mdi:content-save-cog
on_press:
- script.execute: apply_all_settings

- platform: template
name: "Reset Sensor"
id: btn_reset
icon: mdi:restart
on_press:
- logger.log: "Manual reset triggered"
- uart.write:
id: uart_bus
data: "AT+RESET\r\n"
- delay: 3s
- script.execute: apply_all_settings

- platform: template
name: "Save Sensor Config"
id: btn_save_config
icon: mdi:content-save
on_press:
- uart.write:
id: uart_bus
data: "AT+SAVECONFIG\r\n"

- platform: template
name: "Get Firmware Version"
id: btn_get_fw
icon: mdi:information
on_press:
- uart.write:
id: uart_bus
data: "AT+GETFWVERSION\r\n"

- platform: restart
name: "Restart ESP32"
icon: mdi:restart-alert
entity_category: config


##############################################################
# TEXT SENSORS
##############################################################
text_sensor:
- platform: template
name: "Last Sound Event"
id: txt_last_event_full
icon: mdi:ear-hearing
# Example: "glass_break 87% confidence"

- platform: template
name: "Event Type"
id: txt_last_event_name
icon: mdi:waveform
# Example: "gunshot"
# Use this in HA automations → trigger when state = "gunshot"

- platform: template
name: "Firmware Version"
id: txt_firmware_version
icon: mdi:chip
entity_category: diagnostic

- platform: wifi_info
ip_address:
name: "IP Address"
icon: mdi:ip-network
entity_category: diagnostic
ssid:
name: "Connected SSID"
icon: mdi:wifi
entity_category: diagnostic


##############################################################
# SENSORS
##############################################################
sensor:
- platform: template
name: "Event Confidence"
id: sen_confidence
icon: mdi:percent
unit_of_measurement: "%"
accuracy_decimals: 0

- platform: wifi_signal
name: "WiFi Signal"
update_interval: 60s
entity_category: diagnostic
icon: mdi:wifi-strength-2

note

In this example, we are using the XIAO ESP32S3, so you may need to update the following parameters in the YAML file according to your board and wiring configuration

board: esp32-s3-devkitc-1   # your board name
tx_pin: GPIO43 # your TX pin connection
rx_pin: GPIO44 # your RX pin connection

Once your YAML is saved, click INSTALL.

pir

Choose Manual Download

pir

Wait for the firmware to compile.

Download the generated .bin firmware file to your computer from Factory Format.

pir

Connect the embedded sound sensor ESP32-S3 board to your PC using a USB Type-C cable.

Open Web ESPHome in Google Chrome.

Click Connect and choose the correct serial port from the list.

pir

Once connected, click INSTALL

Select the .bin file you just downloaded.

pir

Wait for the installation to complete (may take a few minutes).

After success, you’ll see a confirmation message.

pir

Return to Home Assistant > Settings > Devices & Services.

pir

You should see ESPHome listed as a discovered integration.

Click Add, then Submit to finish setup.

pir

pir

Then, you will be able to interact with the device through the Home Assistant interface and create your own automations with other peripherals. For example, you can trigger a buzzer when glass break is detected, or automatically play calm lullaby music on a smart speaker when a baby’s cry is detected.

Demo

Tech Support & Product Discussion

Thank you for choosing our products! We are here to provide you with different support to ensure that your experience with our products is as smooth as possible. We offer several communication channels to cater to different preferences and needs.

Loading Comments...