Starai Arm Manipulator - ROS2 MoveIt Guide
| Follower Viola | Leader Violin | Follower Cello |
|---|---|---|
![]() | ![]() | ![]() |
Product Introduction
-
Open-Source & Easy for Secondary Development This series of servo motors, provided by Fashion Star Robotics, offers an open-source, easily customizable 6+1 degrees of freedom robotic arm solution.
-
Dual-Arm Systems with Various Payloads The Violin serves as the leader robotic arm. When at 70% of its arm span, the follower arm Viola has an operating payload of 300g, while the follower arm Cello has an operating payload of 750g.
-
Supported ROS2, Moveit2 and Isaac Sim It supports ROS2 for publishing and subscribing to robotic arm data topics and controlling the robotic arm, and also supports MoveIt2 for inverse kinematics calculation, as well as simulation in Isaac Sim.
-
LeRobot Platform Integration Support It's specifically designed for integration with the LeRobot platform. This platform provides PyTorch models, datasets, and tools for imitation learning in real-world robotics tasks, including data collection, simulation, training, and deployment.
-
Open-Source SDK Supports Python and C++ SDK Development
-
Button Hover Simulates gravity compensation, allowing the robotic arm to hover at any position via a button.
-
Modular End Effector Enables quick DIY replacement.
-
Abundant Learning Resources We offer comprehensive open-source learning resources, including environment setup, installation and debugging guides, and custom grasping task examples to help users quickly get started and develop robotic applications.
-
Nvidia Platform Compatibility Deployment is supported via the Nvidia Jetson platform.
Specifications
| Item | Follower Arm | Viola | Leder Arm |Violin | Follower Arm |Cello |
|---|---|---|---|
| Degrees of Freedom | 6+1 | 6+1 | 6+1 |
| Reach | 470mm | 470mm | 670mm |
| Span | 940mm | 940mm | 1340mm |
| Repeatability | 2mm | - | 1mm |
| Working Payload | 300g (with 70% Reach) | - | 750g (with 70% Reach) |
| Servos | RX8-U50H-M x2 RA8-U25H-M x4 RA8-U26H-M x1 | RX8-U50H-M x2 RA8-U25H-M x4 RA8-U26H-M x1 | RX18-U100H-M x3 RX8-U50H-M x3 RX8-U51H-M x1 |
| Parallel Gripper Ki | ✅ | - | ✅ |
| Wrist Rotate | Yes | Yes | Yes |
| Hold at any Position | Yes | Yes (with handle button) | Yes |
| Wrist Camera Mount | Provides reference 3D printing files | Provides reference 3D printing files | |
| Works with LeRobot | ✅ | ✅ | ✅ |
| Works with ROS 2 | ✅ | ✅ | ✅ |
| Works with MoveIt2 | ✅ | ✅ | ✅ |
| Works with Gazebo | ✅ | ✅ | ✅ |
| Communication Hub | UC-01 | UC-01 | UC-01 |
| Power Supply | 12V10A/120w XT30 | 12V10A/120w XT30 | 12V25A/300w XT60 |
For more information about servo motors, please visit the following link.
Dependent Environment
No LSB modules are available.
Distributor ID: Ubuntu
Description: Ubuntu 22.04.5 LTS
Release: 22.04
Codename: Jammy
ROS2: Humble
Install ROS2 Humble
Install Moveit2
sudo apt install ros-humble-moveit*
Install Servo Motor's SDK
sudo pip install pyserial
sudo pip install fashionstar-uart-sdk
Create a workspace and Initialization
mkdir -p ~/starai_ws/src
cd ~/starai_ws
colcon build
Clone starai-arm-moveit2 Ros2's Package
cd ~/starai_ws/src
git clone https://github.com/Seeed-Projects/fashionstar-starai-arm-ros2.git
cd ~/starai_ws
colcon build
echo "source ~/starai_ws/install/setup.bash" >> ~/.bashrc
source ~/.bashrc
Viola
Starai Arm MoveIt2 Simulation Script (Optional)
ros2 launch viola_moveit_config demo.launch.py
Using a Real Robotic Arm
Step 1: Start the Arm Control Node
Start the arm hardware driver, the Arm Will Move to The Zero Position.
ros2 launch viola_moveit_config driver.launch.py
Step2: Starthe Moveit2
ros2 launch viola_moveit_config moveit_write_read.launch.py
End-effector pose read/write demo
ros2 run arm_moveit_write topic_publisher
Cello
Starai Arm MoveIt2 Simulation Script (Optional)
ros2 launch cello_moveit_config demo.launch.py
Using a Real Robotic Arm
Step 1: Start the Arm Control Node
Start the arm hardware driver, the Arm Will Move to The Zero Position.
ros2 launch cello_moveit_config driver.launch.py
Step2: Starthe Moveit2
ros2 launch cello_moveit_config actual_robot_demo.launch.py
End-effector pose read/write demo
ros2 launch cello_moveit_config moveit_write_read.launch.py
Position and orientation topic sending node demo
update here src/arm_moveit_write/src/topic_publisher.cpp
// // viola
// dataset1_ = {
// {0.003, -0.204, 0.274}, // position
// {0.014, 0.717, 0.017, 0.696}, // orientation
// "open" // gripper_state
// };
// dataset2_ = {
// {-0.00, -0.34, 0.177}, // position
// {0.0, 0.7071, 0.0, 0.7071}, // orientation
// "close" // gripper_state
// };
// cello
dataset1_ = {
{-0.278, 0.000, 0.438}, // position
{0.707, 0.000, -0.707, 0.000}, // orientation
"open" // gripper_state
};
dataset2_ = {
{-0.479, -0.000, 0.369}, // position
{0.707, -0.000, -0.707, 0.000}, // orientation
"close" // gripper_state
}
colcon build
source install/setup.sh
ros2 run arm_moveit_write topic_publisher
FAQ
-
If you experience flickering in the RViz2 interface, try the following commands:
export QT_AUTO_SCREEN_SCALE_FACTOR=0