Skip to main content

One doc tagged with "J601-Robotics carrier board"

View all tags

reComputer Robotics J601 Hardware & I/O

This wiki provides a comprehensive introduction to the hardware features and interface usage of the reComputer Jetson Robotics J601 carrier board. It covers detailed specifications, supported modules, setup instructions, and practical guides for using various interfaces such as M.2, Ethernet, USB, CAN, RS485/RS232, UART, I2C, I2S, GPIO, GMSL2 camera expansion, 5G, and GPS, helping users quickly get started with robotics development on the J601 platform.