4G LTE HAT on Raspberry Pi- TCP/IP Networking Explained
Introduction
TCP (Transmission Control Protocol) is vital for applications involving the Raspberry Pi 4G HAT because it ensures reliable, ordered, and error-checked data transmission over the internet. This is crucial for real-time applications like IoT devices, where consistent communication with cloud servers or remote systems is needed. TCP’s reliability makes it ideal for sending critical data (e.g., sensor readings, telemetry) and receiving commands, ensuring no data is lost or corrupted. It supports diverse applications such as remote monitoring, messaging systems, and file transfers with the Raspberry Pi acting as a gateway or client.
Prerequisites
Hardware Requirements
| Raspberry Pi 5 | Raspberry Pi 4G LTE CAT4 HAT |
|---|---|
![]() | ![]() |
Software Requirements
Communication drivers and tools
If you have not installed relevant drivers and communication tools, please check the guide first
Additional Requirements
You will need a pre-configured TCP server with the following details:
- Host: For example, your own server or for testing purposes tcpbin.com
- Port Number: A dedicated port number, or in this case, we will use port
4242oftcpbin.com.
tcpbin.com is a public TCP server used for testing and debugging TCP/IP communication. It echoes back the messages sent to it, making it ideal for verifying connectivity and data transmission.
Send AT Commands to tcpbin.com
Open Minicom on Raspberry Pi or Qcom Tool on Windows via USB.
sudo minicom -D /dev/ttyUSB2
| Step | Action | AT Command | Expected Response |
|---|---|---|---|
| 1 | Configure the APN for your mobile network provider. | AT+QICSGP=1,1,"dialogbb","","",1 | OK |
| 2 | Activate the PDP context. | AT+QIACT=1 | OK |
| 3 | Verify the PDP context is activated. | AT+QIACT? | +QIACT: 1,1,1,"<Your_IP_Address>" OK |
| 4 | Open a TCP connection to the server. | AT+QIOPEN=1,0,"TCP","tcpbin.com",4242,0,0 | +QIOPEN: 0,0 (Indicates a successful connection) |
| 5 | Send a message to the server. | AT+QISEND=0 | > (Prompt to enter the message) After typing message: Hello TCPBin<Ctrl+Z> SEND OK |
| 6 | Read the response from the server. | AT+QIRD=0,1500 | +QIRD: <length> Hello TCPBin OK |
| 7 | Close the TCP connection. | AT+QICLOSE=0 | OK |
Automated Python Script
Below is an automated Python script to interact with the Quectel 4G LTE module on a Raspberry Pi. The script uses the serial library to send AT commands to the module. You can customize the variables for APN, port, baud rate, TCP port, and address.
Python Code Implementation
Step 1. Prepare the Directory and Virtual Environment
- Open a terminal on your Raspberry Pi.
- Create a new project folder and navigate into it:
mkdir TCP_EX
cd TCP_EX
- Set up a Python virtual environment:
python3 -m venv --system-site-packages env
- Activate the virtual environment:
source env/bin/activate
- Install the required libraries:
pip install pyserial
Step 2. Prepare the Python Script
-
Open the Thonny Python IDE (pre-installed on Raspberry Pi).
-
Create a new file in Thonny and paste the provided code into the editor.
-
Update the usb_port parameter to match your Raspberry Pi's serial port for the 4G HAT. Typically, it might be
/dev/ttyUSB2or/dev/ttyUSB3. Example:
usb_port = "/dev/ttyUSB2"
- Save the file as test_mqtt.py in the TCP_EX folder.
import serial
import time
# Configuration Variables
APN = "dialogbb" # Replace with your network APN
PORT = "/dev/ttyUSB2" # Serial port connected to the Quectel module
BAUDRATE = 9600 # Communication baud rate
TCP_ADDRESS = "tcpbin.com" # TCP server address
TCP_PORT = 4242 # TCP server port
MESSAGE = "Hello TCPBin" # Message to send
def send_command(ser, command, wait_for="OK", timeout=5):
"""
Send an AT command to the module and wait for a response.
"""
ser.write((command + "\r\n").encode())
time.sleep(0.5)
end_time = time.time() + timeout
response = b""
while time.time() < end_time:
if ser.in_waiting > 0:
response += ser.read(ser.in_waiting)
if wait_for.encode() in response:
break
print(f">> {command}")
print(response.decode().strip())
return response.decode().strip()
def main():
try:
# Open serial connection
ser = serial.Serial(PORT, BAUDRATE, timeout=1)
time.sleep(2) # Allow the module to initialize
# 1. Configure APN
send_command(ser, f'AT+QICSGP=1,1,"{APN}","","",1')
# 2. Activate PDP Context
send_command(ser, "AT+QIACT=1")
# 3. Check PDP Context State
send_command(ser, "AT+QIACT?")
# 4. Open TCP Connection
send_command(ser, f'AT+QIOPEN=1,0,"TCP","{TCP_ADDRESS}",{TCP_PORT},0,0')
time.sleep(5) # Allow connection to establish
# 5. Send Data
send_command(ser, f"AT+QISEND=0")
ser.write((MESSAGE + "\x1A").encode()) # Send message and end with Ctrl+Z
time.sleep(1) # Allow time for sending
print("Message sent.")
# 6. Read Response
response = send_command(ser, "AT+QIRD=0,1500")
print(f"Server Response: {response}")
# 7. Close Connection
send_command(ser, "AT+QICLOSE=0")
print("Connection closed.")
# Close serial port
ser.close()
except Exception as e:
print(f"Error: {e}")
if __name__ == "__main__":
main()
Step 3. Run the Script
- Open a terminal, ensure you're in the project directory:
cd TCP_EX
- Activate the virtual environment:
source env/bin/activate
- Run the script using Python:
python test_tcp.py
- The output
Resources
- [PDF Book] TCP Application Guide
Tech Support & Product Discussion
Thank you for choosing our products! We are here to provide you with different support to ensure that your experience with our products is as smooth as possible. We offer several communication channels to cater to different preferences and needs.