ThingsBoard Integrated(via TTS)
ThingsBoard is an open-source IoT platform that enables rapid development, management, and scaling of IoT projects. Our goal is to provide the out-of-the-box IoT cloud or on-premises solution that will enable server-side infrastructure for your IoT applications.
The content of this chapter will guide users how to connect the SenseCAP T1000 Tracker to ThingsBoard through TTN.
Get Started
Before starting the setup, please check Connect SenseCAP T1000 to TTS to connect your SenseCAP T1000 Tracker to TTS first.
Configura the ThingsBoard
To get started, create an account with ThingsBoard.
Create Converter
First, we need to create an Uplink Data Converter which will be used for receiving messages from the TTS.
Navigate to Data converters, click Create new converter.
![]()
Name the converter, enable Debug mode, copy the following code and click Add.
var data = decodeToJson(payload);
var deviceName = data.end_device_ids.device_id;
var deviceType = data.end_device_ids.application_ids.application_id;
var telemetry = {};
var messages = data.uplink_message.decoded_payload.messages[0];
for (var i = 0; i < messages.length; i++) {
var measurement = messages[i];
var type = measurement.type.toLowerCase();
var typeKey = '';
for (var j = 0; j < type.length; j++) {
if (type[j] === ' ') {
typeKey += '_';
} else {
typeKey += type[j];
}
}
telemetry[typeKey] = measurement.measurementValue;
}
var result = {
deviceName: deviceName,
deviceType: deviceType,
telemetry: telemetry
};
function decodeToString(payload) {
return String.fromCharCode.apply(String, payload);
}
function decodeToJson(payload) {
var str = decodeToString(payload);
var data = JSON.parse(str);
return data;
}
return result;
![]()
Add integration
Navigate to Integration, click Add Integration.
![]()
Type: The Things Stack Community
Enable: Enable integration Debug mode Allow create devices or assets
![]()
Choose Select existing, and select the one we create before.
![]()
Skip the Downlink data converter.
![]()
Region: Region where your application was registered inside TTS
Username: Username from TTS
Password: Password from TTS
Use API v3: Set Enable
Info can be found in TTS MQTT integration.
![]()
![]()
Data view
Navigate to Entities -> Devices, here you can see that:
- a new device was registered in Thingsboard
- in the
Latest Telemetrysection you will the update data from the device.
![]()
Add Dashboard
Navigate to Dashboards, Click Create new dashboard.
Enter the dashboard title, and then click Next.
![]()
Add widget, select widget to add.
Location map
Select a map widget.
![]()
Type: Device
Device: The device we created.
Data key: latitude, longitude
![]()
Other parameters
Refer to the above steps to add other widgets.
Temperature
Device: The device we created.
Data key: air_temperature
![]()
Battery
Device: The device we created.
Data key: battery
![]()
Here is an basic example, you can customize your own dashboard.
![]()