Low Data Consumption Mode Config(for 4G version)
This tutorial will guide users to configure the low data consumption mode for the M2 Multi-Platform Gateway 4G version. In this mode, the traffic per month is expected to be around 60M. The specific traffic depends on the nodes packets, etc.
- The status display of the APP may be delayed
- The network switch and RGB indicator light will change after 5 minutes
Check Firmware Version
Before configuring the low data consumption mode, check the OS and firmware version first.
The OS version needs to be newer than 0.9.5
The firmware version needs to be newer than 1.1.6
Check the Quick Start to log in the Luci page.
Navigate to Status -> Overview, check the current OS and firmware version.

Upgrade OS
The firmware will be upgraded automatically, but user needs to upgrade the OS version manually.
Navigate to System -> Backup/Flash Firmware, click Update.
Keep the power connection during the upgrade period.

White List Config
This tab is used to filter out nodes you don't need to save traffic.
-
For
SenseCAPMode, Nodes other than SenseCAP will be automatically filtered, don’t need additional configuration. -
For
Packet ForwarderandBasic StationMode, need to enable the White List Mode.
If you are using AWS platform, you can skip this step, just config the white list on AWS console.

OUI List: The first three bytes of the node EUI. Used to filter join-request packets.
eg. for SenseCAP node, the OUI is '2CF7F1'
Network ID List/DevAddr: Used to filter uplink packets.
eg. for SenseCAP node,the NetID is '000013', DevAddr is '27000000 - 27FFFFFF'
More details refer to NetID and DevAddr Prefix Assignments

Set PING Params
Used to check if the link is up, leave it blank to assume interface is always online.

Enable Low Data Consumption Mode
Enable the Low Data Consumption Mode, and set the alive time, default in SesneCAP Platform: 86400.
After settings, please restart the gateway to apply the changes.