Skip to main content

Tutorial of AI Kit with Raspberry Pi 5 about YOLOv8n object detection

Introduction

YOLOv8 (You Only Look Once version 8) is the popular most YOLO series of real-time pose estimation and object detection models. It builds upon the strengths of its predecessors by introducing several advancements in speed, accuracy, and flexibility. The Raspberry-pi-AI-kit is used to accelerate inference speed, featuring a 13 TOPS neural network inference accelerator built around the Hailo-8L chip.

This wiki will guide you on how to use YOLOv8n for object detection with AI Kit on Raspberry Pi 5, from training to deployment.

Prepare Hardware

For Hailo8L 13 TOPS

Raspberry Pi5 8GBRaspberry Pi AI Kit

For Hailo8 26 TOPS

reComputer R1125reComputer AI R2130reComputer AI Industrial R2145
reComputer Industrial R20xxreComputer Industrial R21xx

Install Hardware

Please refer to this

On Host Computer

note

We will install hailo software, make sure you have a hailo account.

Install Ultralytics and train model

Install python3.11

sudo apt install python3.11

Create yolo_env as your virtual environment

python3.11 -m venv yolo_env

Activate the environment

source yolo_env/bin/activate

Install ultralytics

pip install ultralytics

Train YOLOv8n using the COCO dataset. If you want to train your own dataset, you can refer to this for instructions on how to do so.

mkdir yolomodel && cd yolomodel
yolo detect train data=coco128.yaml model=yolov8n.pt name=retrain_yolov8n epochs=100 batch=16

pir

You will get the best.pt model after your training, as shown below:

cd ./runs/detect/retrain_yolov8n/weights/
ls

pir

Convert the .pt model to .onnx.

yolo export model=./best.pt imgsz=640 format=onnx opset=11 

Result like below:

pir

Install hailo software

Install python 3.8

cd ~
sudo apt install python3.8

Create hailo_env as your virtual environment

python3.8 -m venv hailo_env

Activate the environment

source hailo_env/bin/activate

Install Hailo Dataflow Compiler 3.27, here you need to register Hailo and login, and download the software.

pir

pip install hailo_dataflow_compiler-3.27.0-py3-none-linux_x86_64.whl 

Install Model zoo, here you need to register Hailo and login, and download the software.

pir

pip install hailo_model_zoo-2.11.0-py3-none-any.whl 

Test whether hailo_model_zoo is functioning correctly.

hailomz -h

pir

Install hailo_model_zoo github file

cd yolomodel/runs/detect/retrain_yolov8n/weights

git clone https://github.com/hailo-ai/hailo_model_zoo.git

Install coco dataset for evaluate/optimize/compile the yolov8n model

python hailo_model_zoo/datasets/create_coco_tfrecord.py val2017
python hailo_model_zoo/datasets/create_coco_tfrecord.py calib2017

Use hailo_model_zoo to parse the model

hailomz parse --hw-arch hailo8l --ckpt ./best.onnx yolov8n

pir

Use hailo_model_zoo to optimize the model

note

If you execute the following command, you may encounter some errors. However, you can copy ./hailo_model_zoo/hailo_model_zoo to your local library. If the error indicates that the dataset cannot be found, you can navigate to ~/.hailomz, locate the dataset, and copy it to your local dataset directory.

hailomz optimize --hw-arch hailo8l --har ./yolov8n.har yolov8n

pir

Use hailo_model_zoo to compile the model

hailomz compile  yolov8n --hw-arch hailo8l --har ./yolov8n.har 

pir

After all you will get a hef model, you can use it to deploy on raspberry pi5 with AI kit

ls

pir

On Raspberry Pi5

update the system

sudo apt update
sudo apt full-upgrade

Set pcie to gen2/gen3(gen3 is faster than gen2)

Add following text to /boot/firmware/config.txt

#Enable the PCIe external connector

dtparam=pciex1

#Force Gen 3.0 speeds

dtparam=pciex1_gen=3

note

If you want to use gen2, please comment dtparam=pciex1_gen=3

Install hailo-all and reboot

Open the terminal on the Raspberry Pi 5 and enter the following command to install the Hailo software

sudo apt install hailo-all
sudo reboot

Check Software and Hardware

Open terminal on the Raspberry Pi5, and input command as follows to check if hailo-all have been installed.

hailortcli fw-control identify

The right result show as bellow:

pir

Open terminal on the Raspberry Pi5, and input command as follows to check if hailo-8L have been connected.

lspci | grep Hailo

The right result show as bellow:

pir

Clone the project

git clone https://github.com/Seeed-Projects/Benchmarking-YOLOv8-on-Raspberry-PI-reComputer-r1000-and-AIkit-Hailo-8L.git
cd Benchmarking-YOLOv8-on-Raspberry-PI-reComputer-r1000-and-AIkit-Hailo-8L

Copy your model to the raspberry pi5

Make a directory named hailomodel

mkdir hailomodel
note

The command below should be run on your host computer, not your Raspberry Pi 5. Ensure that both your host computer and Raspberry Pi 5 are connected to the same network.

scp -r ./yolomodel/runs/detect/retrain_yolov8n/weights/yolov8n.hef username@ip /home/pi/Benchmarking-YOLOv8-on-Raspberry-PI-reComputer-r1000-and-AIkit-Hailo-8L/hailomodel/

Change code

Find line 105 and 106 in object-detection-hailo.py, and change the code like below:

        elif args.network == "yolov8n":
self.hef_path = os.path.join(self.current_path, './hailomodel/yolov8n.hef')

Find line 172 in object-detection-hailo.py, and change the code like below:

    parser.add_argument("--network", default="yolov8n", choices=['yolov6n', 'yolov8s', 'yolox_s_leaky'], help="Which Network to use, defult is yolov6n")

Run the code

bash run.sh object-detection-hailo

Result

Here is the video in which we demonstrate the process of training the YOLOv8n model and deploying it on the Raspberry Pi 5. We set the batch size to 8, the input size to 640x640, and the input video frame rate to 240 fps. The inference speed achieved is 136.7 fps, which is exceptionally fast for most application scenarios.

Tech Support & Product Discussion

Thank you for choosing our products! We are here to provide you with different support to ensure that your experience with our products is as smooth as possible. We offer several communication channels to cater to different preferences and needs.

Loading Comments...