How to Update Jetson Orin Nano Developer Kit to Super Kit
What is Jetson Orin Nano Super Developer Kit
The NVIDIA Jetson Orin Nano™ Super Developer Kit is a compact, yet powerful computer that redefines generative AI for small edge devices. It delivers up to 67 TOPS of AI performance—a 1.7X improvement over its predecessor—to seamlessly run the most popular generative AI models, like vision transformers, large language models, vision-language models, and more. At just $249, it provides developers, students, and makers with the most affordable and accessible platform with the support of the NVIDIA AI software and a broad AI software ecosystem. Existing Jetson Orin Nano Developer Kit users can experience this performance boost with just a software upgrade, so everyone can now unlock new possibilities with generative AI.
What is surprising is Jetson Orin Nano Developer Kit can be upgraded to Jetson Orin Nano Super Developer Kit with just a software update.
How to Update to the Super Developer Kit
As long as you have an Nvidia Jetson Orin Nano 8GB in hand, you can upgrade it by following these steps:
- Step 1: Connect the hardware devices.
- Step 2: Open the SDKManager.
- Step 3: Configure and flash the system. Watch the video to immerse yourself in experiencing each step.
Actual performance of Orin Nano Super Developer Kit
Full performance release
Use the burn-in program to fully load the CPU and GPU, under which the module's maximum power reaches 21W, close to the power level of the Jetson Orin NX.
Jetson Orin cpu and gpu burn program download link.
Improved inference speed
Here, we use Ollama to load the Llama3.2-3B model and compare the inference speed of the model under different power modes. It is evident that with maximum power enabled, the model's inference speed is significantly faster, showing a 1.28x improvement compared to its predecessor.
Refer to this tutorial to learn how to quickly deploy Ollama on Nvidia Jetson.
Conclusion
The Jetson Orin Nano Super Developer Kit is your ultimate platform for leading the way in generative AI development for edge computing. Now is the perfect time to get started and join the vibrant and diverse community of advanced developers and researchers working together with NVIDIA to address real-world challenges with physical AI. For existing Jetson Orin Nano Developer Kit users, upgrade your JetPack SDK to unlock boosted performance today.
Tech Support & Product Discussion
Thank you for choosing our products! We are here to provide you with different support to ensure that your experience with our products is as smooth as possible. We offer several communication channels to cater to different preferences and needs.