Use SQLite on reComputer
Introduction

This wiki explains how to use the SQlite on reComputer box. SQLite is a lightweight, embedded relational database management system widely used in mobile devices, desktop applications, and embedded systems. It does not require a separate server process; the database is stored directly in a single ordinary disk file. SQLite is simple to use and offers excellent performance. It supports standard SQL syntax and is suitable for small to medium-sized data storage needs. Due to its zero-configuration and easy deployment features, SQLite has become the preferred database engine for many projects.
Prepare Hardware
| reComputer R1125 | reComputer AI R2130 | reComputer AI Industrial R2145 |
|---|---|---|
![]() | ![]() | ![]() |
| reComputer Industrial R20xx | reComputer Industrial R21xx |
|---|---|
![]() | ![]() |
Prepare software
update the system
sudo date -s "$(wget -qSO- --max-redirect=0 google.com 2>&1 | grep Date: | cut -d' ' -f5-8)Z"
sudo apt update
sudo apt full-upgrade
Install SQlite
sudo apt-get install sqlite3

Creat database
sqlite3 sensordata.db
With the .help command you can be quickly reminded of all the supported commands and their respective usage.
sqlite> .help

Then use .quit to quit SQlite shell.
sqlite> .quit
Using SQL
SQL creat table
sqlite3 sensordata.db
Then use command like below to creat a new table.
ain@raspberrypi:~ $ sqlite3 sensordata.db
SQLite version 3.40.1 2022-12-28 14:03:47
Enter ".help" for usage hints.
sqlite> BEGIN;
sqlite> CREATE TABLE dhtreadings (
...> id INTEGER PRIMARY KEY AUTOINCREMENT,
...> temperature NUMERIC,
...> humidity NUMERIC,
...> currentdate DATE,
...> currenttime TIME,
...> device TEXT
...> );
sqlite> COMMIT;
Check the table
You can use the following command to view the created table.
sqlite> .tables
dhtreadings
sqlite> .fullschema
CREATE TABLE dhtreadings (
id INTEGER PRIMARY KEY AUTOINCREMENT,
temperature NUMERIC,
humidity NUMERIC,
currentdate DATE,
currenttime TIME,
device TEXT
);
/* No STAT tables available */
SQL insert
To insert new temperature and humidity readings in the database, you could do something like this:
sqlite> BEGIN;
sqlite> INSERT INTO dhtreadings(temperature, humidity, currentdate, currenttime, device) values(22.4, 48, date('now'), time('now'), "manual");
sqlite> COMMIT;
SQL select
To access the data stored in the database, you use the SELECT SQL statement:
sqlite> SELECT * FROM dhtreadings;
1|22.4|48|2025-09-26|01:23:37|manual
So far, you only have 1 reading inserted in the database. You can insert a new reading as follows:
sqlite> BEGIN;
sqlite> INSERT INTO dhtreadings(temperature, humidity, currentdate, currenttime, device) values(22.5, 48.7, date('now'), time('now'), "manual");
sqlite> COMMIT;
And when you SELECT the data stored in the table, it returns 2 readings:
sqlite> SELECT * FROM dhtreadings;
1|22.4|48|2025-09-26|01:23:37|manual
2|22.5|48.7|2025-09-26|02:06:35|manual
SQL drop
If you want to completely delete the table from your database, you can use the DROP TABLE command.
NOTE: the next command will completely delete the dhtreadings table:
sqlite> DROP TABLE dhtreadings;
Now, if you type the ‘.tables‘ command:
sqlite> .tables
It doesn’t return anything, because your table was completely deleted.
Use Python with SQLite
Using Python to interact with SQLite like below:
test_sqlite.py
import sqlite3
from datetime import datetime
import os
def create_connection(db_file="dht_readings.db"):
"""Create a database connection to the SQLite database"""
conn = None
try:
conn = sqlite3.connect(db_file)
print(f"Connected to SQLite database: {db_file}")
except sqlite3.Error as e:
print(f"Error connecting to database: {e}")
return conn
def create_table(conn):
"""Create the dhtreadings table if it doesn't exist"""
try:
sql_create_dhtreadings_table = """
CREATE TABLE IF NOT EXISTS dhtreadings (
id INTEGER PRIMARY KEY AUTOINCREMENT,
temperature REAL NOT NULL,
humidity REAL NOT NULL,
currentdate TEXT NOT NULL,
currenttime TEXT NOT NULL,
device TEXT NOT NULL
);
"""
conn.cursor().execute(sql_create_dhtreadings_table)
conn.commit()
print("DHT readings table created successfully")
except sqlite3.Error as e:
print(f"Error creating table: {e}")
def insert_dht_reading(conn, temperature, humidity, device):
"""Insert a new DHT reading into the dhtreadings table"""
sql_insert = """INSERT INTO dhtreadings(temperature, humidity, currentdate, currenttime, device)
VALUES(?, ?, date('now'), time('now'), ?);"""
try:
cursor = conn.cursor()
cursor.execute(sql_insert, (temperature, humidity, device))
conn.commit()
print(f"New record created successfully with ID: {cursor.lastrowid}")
return cursor.lastrowid
except sqlite3.Error as e:
print(f"Error inserting data: {e}")
return None
def select_all_readings(conn):
"""Query all DHT readings in the dhtreadings table"""
try:
cursor = conn.cursor()
cursor.execute("SELECT * FROM dhtreadings ORDER BY currentdate DESC, currenttime DESC")
rows = cursor.fetchall()
print("\nAll DHT readings:")
print("ID | Temperature | Humidity | Date | Time | Device")
print("-" * 60)
for row in rows:
print(f"{row[0]} | {row[1]} | {row[2]} | {row[3]} | {row[4]} | {row[5]}")
except sqlite3.Error as e:
print(f"Error fetching data: {e}")
def main():
# Create a database connection
database = "dht_readings.db"
conn = create_connection(database)
# Create table
if conn is not None:
create_table(conn)
# Insert a sample reading as specified in your requirement
insert_dht_reading(conn, 22.5, 48.7, "manual")
# Insert some additional sample data for testing
insert_dht_reading(conn, 23.1, 45.2, "sensor1")
insert_dht_reading(conn, 21.8, 50.3, "sensor2")
# Display all readings
select_all_readings(conn)
# Close the connection
conn.close()
print("\nDatabase connection closed.")
else:
print("Error! Cannot create database connection.")
if __name__ == '__main__':
main()

Tech Support & Product Discussion
Thank you for choosing our products! We are here to provide you with different support to ensure that your experience with our products is as smooth as possible. We offer several communication channels to cater to different preferences and needs.