Skip to main content

Use uv on reComputer

Introduction

This wiki explains how to use the uv on reComputer box. uv is a fast, modern, and lightweight package manager and resolver for Python. It is designed to be a drop-in replacement for traditional Python package management tools like pip and pip-tools, offering significant improvements in speed, efficiency, and usability.

Prepare Hardware

reComputer R1125reComputer AI R2130reComputer AI Industrial R2145
reComputer Industrial R20xxreComputer Industrial R21xx

Prepare software

update the system

sudo date -s "$(wget -qSO- --max-redirect=0 google.com 2>&1 | grep Date: | cut -d' ' -f5-8)Z"
sudo apt update
sudo apt full-upgrade

Install uv

curl -LsSf https://astral.sh/uv/install.sh | sh

Use uv

Init the project

Here, we use uv_test as an example to demonstrate the usage of uv.

Note: Please make different project name make sure it is different from any package on PyPI.

uv init uv_test --package
cd uv_test

Check the structure of the project

ls -la
tree

Creat a python environment

Here you can creat a python environmet

uv venv 
source .venv/bin/activate

Add dependencies

Use numpy to build funcation:

uv add numpy

Creat funcation

Use NumPy to write an add function on add.py as an example:

add.py
import numpy as np

def add(arr1: np.ndarray, arr2: np.ndarray) -> np.ndarray:
"""
Adds two NumPy arrays element-wise.

Parameters:
arr1 (np.ndarray): The first input array.
arr2 (np.ndarray): The second input array.

Returns:
np.ndarray: The element-wise sum of arr1 and arr2.

Raises:
ValueError: If the input arrays have different shapes and cannot be broadcasted.
"""
# Ensure that both arrays have compatible shapes for element-wise addition
try:
result = np.add(arr1, arr2)
except ValueError:
raise ValueError("Input arrays have incompatible shapes for element-wise addition.")

return result

if __name__ == "__main__":
# Example usage
arr1 = [1, 2, 3]
arr2 = [4, 5, 6]
print("Result of addition:", add(arr1, arr2))

The results are as follows:

Build the package

To build the project into a usable .whl file, modify the toml file as follow:

Build the package:

uv build
ls -a

The results are as follows:

Test the package

Install the package as below:

uv pip install dist/uv_test-0.1.0-py3-none-any.whl 

Use python script to test the packag:

add.py
from uv_test.add import add

if __name__ == "__main__":
arr1 = [1, 2, 3]
arr2 = [4, 5, 6]
print("Result of addition:", add(arr1, arr2))

Push the package to PyPi

If you don't have a PyPI account, please register an account and get creat token.

uv publish

The result is like as below, and input your token:

Result

Finally, you can see your uploaded project on PyPI.

Tech Support & Product Discussion

Thank you for choosing our products! We are here to provide you with different support to ensure that your experience with our products is as smooth as possible. We offer several communication channels to cater to different preferences and needs.

Loading Comments...