Skip to main content

Wio-S3 Wireless Module Command List

Serial Debugging Command List​

System Command​

1. help [<string>] [-v <0|1>]

Print the summary of all registered commands if no arguments are given, otherwise print summary of given command.

ItemDescriptionData
<string>Name of commandOptional. If provided, display description for the specified command
-v, --verbose=<0|1>If specified, list console commands with given verbose level0 or 1

Examples:

  • help : Show all available commands.
  • help lora_tx : Show detailed information for the lora_tx command.
  • help -v 1 : Show full command list with verbose mode enabled.

LoRa Command​

1. lora_tx [-f <f>] [-s <6-12>] [-b <0|1|2>] [-c <1|2|3|4>] [-p] [--crc=<0|1>] [--iq=<0|1>] [--net=<0|1>] [-i <t>] [-d <d>] [-n <n>]

Send LoRa data packets with configurable radio parameters.

ItemDescriptionData
-f, --freq=<f>Set radio frequency in Hz415000000 ~ 940000000 Hz,
default: 868000000
-s, --sf=<6-12>Set LoRa SF6 ~ 12, default: 7
-b, --bw=<0|1|2>Set LoRa Bandwidth0:125KHz, 1:250KHz, 2:500KHz,
default: 0
-c, --cr=<1|2|3|4>Set LoRa Coding Rate1:CR_4_5, 2:CR_4_6, 3:CR_4_7, 4:CR_4_8, default: 1
-p, --power=Set radio powerLPA: -17 ~ +14 dB, HPA: -9 ~ +22 dB, default: 10
--crc=<0|1>Set LoRa CRC0:DISABLE, 1:ENABLE, default: 1
--iq=<0|1>Set LoRa IQ mode0:STANDARD, 1:INVERTED, default: 0
--net=<0|1>Set Public Network0:Private Network, 1:Public Network, default: 0
-i, --interval=<t>Set TX interval (ms)default: 0
-d, --txt=<d>Set text data to senddefault: hello
-n, --num=<n>Number of packets sent0: Keep sending, default: 1

Example: lora_tx -f 868000000 -s 7 -b 0 -c 1 -p 10 -d hello
Send a LoRa packet with frequency 868000000 Hz, SF7, 125 kHz bandwidth, coding rate 4/5, and send "hello" at TX power 10 dB.

2. lora_rx [-f <f>] [-s <6~12>] [-b <0|1|2>] [-c <1|2|3|4>] [--crc=<0|1>] [--iq=<0|1>] [--net=<0|1>] [--boosted=<0|1>]

Receive LoRa packets with configurable radio parameters.

ItemDescriptionData
-f, --freq=<f>Set radio frequency in Hz415000000 ~ 940000000 Hz, default: 868000000
-s, --sf=<6~12>Set LoRa SF6 ~ 12, default: 7
-b, --bw=<0|1|2>Set LoRa Bandwidth0:125KHz, 1:250KHz, 2:500KHz, default: 0
-c, --cr=<1|2|3|4>Set LoRa Coding Rate1:CR_4/5, 2:CR_4/6, 3:CR_4/7, 4:CR_4/8, default: 1
--crc=<0|1>Set LoRa CRC0:DISABLE, 1:ENABLE, default: 1
--iq=<0|1>Set LoRa IQ mode0:STANDARD, 1:INVERTED, default: 0
--net=<0|1>Set Public Network0:Private Network, 1:Public Network, default: 0

Example: lora_rx -f 868000000 -s 7 -b 0
Receive LoRa packets at frequency 868000000 Hz, SF7, 125 kHz bandwidth in normal RX mode.

3. lora_cw [-f <f>] [-p] [-o]

Transmit a continuous wave signal for RF testing and spectrum measurement.

ItemDescriptionData
-f, --freq=<f>Set radio frequency in Hz415000000 ~ 940000000 Hz, default: 868000000
-p, --power=<f>Set radio powerLPA: -17 ~ +14 dB, HPA: -9 ~ +22 dB, default: 10
-o, --ocp=<f>Set current limit step0 ~ 63, step 2.5mA, default: 24

Example: lora_cw -f 868000000 -p 10 -o 24
Transmit continuous wave signal at 868 MHz with 10 dB TX power and 60 mA OCP current limit for RF testing.

4. lora_fcc_fhss [-m <0|1>] [-s <6~12>] [-c <1|2|3|4>] [-p] [--crc=<0|1>] [--iq=<0|1>] [--net=<0|1>] [-i <t>] [-d <d>]

Transmit LoRa packets using frequency hopping mode for FCC compliance and RF certification testing.

ItemDescriptionData
-m, --mode=<0|1>Set FHSS mode0: FHSS_125K_MODE, 1: FHSS_500K_MODE, default: 0
-s, --sf=<6~12>Set LoRa SF6 ~ 12, default: 10
-c, --cr=<1|2|3|4>Set LoRa Coding Rate1:CR_4/5, 2:CR_4/6, 3:CR_4/7, 4:CR_4/8, default: 1
-p, --power=<f>Set radio powerLPA: -17 ~ +14 dB, HPA: -9 ~ +22 dB, default: 10
--crc=<0|1>Set LoRa CRC0:DISABLE, 1:ENABLE, default: 1
--iq=<0|1>Set LoRa IQ mode0:STANDARD, 1:INVERTED, default: 0
--net=<0|1>Set Public Network0:Private Network, 1:Public Network, default: 0
-i, --interval=<t>Set TX interval (ms)default: 0
-d, --txt=<d>Set text data to senddefault: hello seeed! 1234567

Example: lora_fcc_fhss -m 1 -s 10 -c 1 -p 14 --crc=1 --iq=0 --net=0 -i 1000 -d test
Transmit FHSS LoRa packets using FHSS_500K_mode, SF10, coding rate 4/5, 14 dB TX power, CRC enabled, standard IQ mode, private network mode, and send payload "test" every 1000 ms.

GPIO Command​

1. gpio [-p <0~48>] [-d <0|1>] [-v <0|1>]

Control GPIO pins for input/output testing and hardware validation.

ItemDescriptionData
-p, --pin=<0~48>GPIO pin number0 ~ 48, default: 0
-d, --direction=<0|1>Set GPIO direction0: INPUT, 1: OUTPUT, default: 1
-v, --value=<0|1>Set GPIO output value0: LOW, 1: HIGH, default: 0

Example: gpio -p 10 -d 1 -v 1
Set GPIO 10 as output mode and drive the pin output to high level.

Flash Command​

1. flash [-b <100~1000>]

Test flash memory read and write performance using block operations.

ItemDescriptionData
-b, --block=<100~1000>Block number to run read/write test100 ~ 1000, default: 100

Example: flash -b 500
Perform flash memory read/write test using 500 data blocks.

WiFi Command​

1. ap_set <ssid> [<pass>] [-a <authmode>] [-n <channel>] [-m <max_conn>]

Configure the device to operate in WiFi AP mode with custom SSID, password, authentication type, and channel settings.

ItemDescriptionData
<ssid>SSID of APRequired
<pass>Password of APOptional
-a, --authmode=<authmode>WiFi authentication typeopen / wep / wpa2 / wpa2_enterprise
-n, --channel=<channel>WiFi channelOptional
-m, --max_conn=<max_conn>Max station numberdefault: 2

Example: ap_set MyAP 12345678 -a wpa2 -n 6 -m 4
Create a WPA2 WiFi AP named "MyAP" on channel 6 with maximum 4 client connections.

2. ap_query

Display current AP configuration and disconnect station mode connection.

Example: ap_query

3. wifi <action> [--espnow_enc=<int>] [--storage=<str>]

WiFi operation actions.

ItemDescriptionData
<action>WiFi operation actioninit / deinit / start / stop / restart / status
--espnow_enc=<int>ESP-NOW encryptiononly for init / restart
--storage=<str>WiFi storage typeflash / ram

Example: wifi init --storage=flash
Initialize WiFi subsystem and store configuration in flash memory.

4. wifi_count [<action>]

WiFi count statistics.

ItemDescriptionData
<action>Counter operationquery(default) / clear

Example: wifi_count clear : Clear current WiFi count statistics.

5. wifi_mode <mode>

Set WiFi mode.

ItemDescriptionData
<mode>WiFi modeap / sta / apsta

Example: wifi_mode apsta : Enable simultaneous AP and Station mode.

6. wifi_protocol [<protocol>] [--2g=<2g_proto>] [--5g=<5g_proto>] [-i <interface>]

Configure the WiFi protocol supported by the selected interface (AP or STA).

Two configuration methods are available:

  • <protocol>: Configure WiFi protocol using esp_wifi_set_protocol()
  • --2g / --5g: Configure protocols separately for the 2.4 GHz and 5 GHz bands using esp_wifi_set_protocols()

Note:

  • esp_wifi_set_protocol() and esp_wifi_set_protocols() cannot be used simultaneously.
  • If no parameters are provided, the current WiFi protocol configuration will be displayed.
ItemDescriptionData
<protocol>Configure WiFi protocol using esp_wifi_set_protocol()Example: b, b/g, b/g/n
g/n is invalid.
--2g=<2g_proto>Configure 2.4 GHz protocol using esp_wifi_set_protocols()API: esp_wifi_set_protocols.
Protocol string: 'lr', 'b', 'g', 'n', 'ax'
Combine with lr mode: 'lr/b', 'lr/g', etc.
Protocol bitmap value: raw bitmap value with hex, eg: 0x40
--5g=<5g_proto>Configure 5 GHz protocolSame format as --2g
-i, --interface=<interface>Select WiFi interfaceap, sta, default: sta

Example: wifi_protocol --2g=lr/b/g/n -i sta
Configure the STA interface to support LR, 802.11b, 802.11g, and 802.11n protocols on the 2.4 GHz band.

7. wifi_bandwidth [<cbw>] [--2g=<2g_cbw>] [--5g=<5g_cbw>] [-i <interface>]

Configure WiFi bandwidth.

Two configuration methods are available:

  • <cbw>: Configure bandwidth using esp_wifi_set_bandwidth()
  • --2g / --5g: Configure bandwidth separately for 2.4 GHz and 5 GHz bands using esp_wifi_set_bandwidths()

Note:

  • esp_wifi_set_bandwidth() and esp_wifi_set_bandwidths() cannot be used simultaneously.
  • If no parameters are provided, the current WiFi bandwidth configuration will be displayed.
ItemDescriptionData
<cbw>Bandwidth using esp_wifi_set_bandwidth()20, 40
--2g=<2g_cbw>2.4 GHz bandwidth using esp_wifi_set_bandwidths()20, 40
--5g=<5g_cbw>5 GHz bandwidth using esp_wifi_set_bandwidths()20, 40
-i, --interface=<interface>Select WiFi interfaceap, sta, default: sta

Example: wifi_bandwidth --2g=20 -i sta
Configure the 2.4 GHz band to use a 20 MHz channel bandwidth.

8. wifi_ps <type>

Set WiFi power mode. This command configures the WiFi Power Save mode of the device. Different modes balance power consumption and network performance differently.

TypeModeLatencyDescription
0WIFI_PS_NONELowestNo power saving, full performance
1WIFI_PS_MIN_MODEMMediumBalanced power saving and performance
2WIFI_PS_MAX_MODEMHighestMaximum power saving, higher delay

Example: wifi_ps 1 : Set WiFi power save mode to minimum modem power saving.

9. wifi_country [<code>] [-s <int>] [-n <int>] [-p <str>]

Set or get WiFi country configuration. This command configures the WiFi regulatory domain, including allowed channels and transmit rules based on country regulations.

ItemDescriptionData
<code>Country code setting (or query current country if not provided)CN / US / JP / etc.
-s, --schan=<int>Start WiFi channel numberInteger (e.g. 1)
-n, --nchan=<int>Total number of supported channelsInteger (e.g. 13)
-p, --policy=<str>Country policy modeauto (default) / manual

Example: wifi_country CN -s 1 -n 13 -p auto
Set WiFi country to CN, enable channels 1-13, and use automatic regulatory policy.

10. sta_connect <ssid> [<pass>] [-b <bssid>] [-n <channel>] [-no-disconnect] [-no-reconnect] [-full-scan] [-failure_retry=<int>] [-5g-offset=<rssi_5g_offset>]

Connect the device in STA mode to a specified WiFi access point.

ItemDescriptionData
<ssid>SSID of WiFi APString (WiFi name)
<pass>Password of APString (WiFi password)
-b, --bssid=<bssid>Specific AP MAC addressMAC address (xx:xx:xx:xx:xx:xx)
-n, --channel=<channel>AP WiFi channelInteger
--no-disconnectFor test: do not run esp_wifi_disconnect before connect/
--no-reconnectDisable auto-reconnect in wifi disconnect handler/
--full-scanEnable full channel scan during sta connection/
--failure_retry=<int>Number of retry attempts after connection failureInteger
--5g-offset=<rssi_5g_offset>Offset value for 5g ssid when do full scan connectInteger

Example: sta_connect MyWiFi 12345678 -n 6 --failure_retry=3 --full-scan : Connect STA mode to specified WiFi AP with optional scan, retry, and connection behavior control.

11. sta_disconnect

Disconnect the device from the current WiFi AP or stop reconnect.

Example: sta_disconnect

12. sta_scan [-h] [<ssid>] [-b <bssid>] [-n <int>] [--max=<int>] [--min=<int>] [--passive] [--passive-time=<int>] [--dwell=<int>] [-2 <int/hex>] [-5 <int/hex>] [--count-only]

Scan available WiFi access points in station mode.

ItemDescriptionData
<ssid>SSID of WiFi APString (WiFi name)
-b, --bssid=<bssid>BSSID of APMAC address (xx:xx:xx:xx:xx:xx)
-n, --channel=<int>Channel of APInteger
-h, --show-hiddenShow hidden APs/
--max=<int>Maximum active scan timeInteger (ms)
--min=<int>Minimum active scan timeInteger (ms)
--passiveSet scan type to passive/
--passive-timePassive scan timeInteger (ms)
--dwell=<int>Home channel dwell timeInteger (ms)
-2, --bitmap-2g=<int/hex>2.4GHz channel scan bitmapHex/int (e.g. 0x842 for ch1/6/11)
-5, --bitmap-5g=<int/hex>5GHz channel scan bitmapHex/int (e.g. 0x6 for ch36/40)
--count-onlyFor test: do scan ap count only./

Example: sta_scan -h --passive --passive-time=120 --dwell=30 -2 0x842 -5 0x6
Perform a full passive WiFi scan showing hidden APs, scanning selected 2.4GHz and 5GHz channels.

13. wifi_txpower [-u <unit>] [--reset]

Set WiFi transmit power or reset to default.

ItemDescription
-u, --unitTX power value, each unit = 0.25 dBm (e.g. 8 = 2 dBm)
--resetReset TX power to default value from SDK configuration

Example: wifi_txpower -u 8 : Set WiFi transmit power to 2 dBm.

Network Command​

1. ping [-W <timeout>] [-i <interval>] [-s <size>] [-c <count>] [-Q <n>] [host] [--abort]

Send ICMP ECHO_REQUEST packets to a network host.

ItemDescriptionData
-W, --timeout=<timeout>Time to wait for responseInteger (seconds)
-i, --interval=<interval>Interval between sending packetsFloat/Integer (seconds)
-s, --packetsize=<size>Use <size> as number of data bytes to be sentInteger (bytes)
-c, --count=<count>Number of packets to send, stop after <count> repliesInteger, default: 5
-Q, --tos=<n>IP Type of Service field valueInteger
hostTarget IP address or domain nameString
--abortStop running ping processping abort -> esp_ping_stop

Example: ping -c 4 8.8.8.8 : Send 4 ICMP echo requests to 8.8.8.8.

2. iperf [-suV] [-c <host>] [-p <port>] [-l <length>] [-i <interval>] [-t <time>] [-b <bandwidth>] [-f <format>] [--abort]

Measure network performance (throughput, bandwidth, and latency) using TCP or UDP.

ItemDescriptionData
-c, --clientRun in client mode and connect to serverIP/domain
-s, --serverRun in server mode/
-u, --udpUse UDP instead of TCP/
-V, --ipv6_domainUse IPv6 protocol/
-p, --port=<port>Server port numberInteger
-l, --len=<length>Buffer length for transmissionInteger (bytes), Defaults: TCP=16384, IPv4 UDP=1470, IPv6 UDP=1450
-i, --interval=<interval>Seconds between periodic bandwidth reportsFloat/Integer (seconds)
-t, --time=<time>Test durationInteger (seconds), default 10s
-b, --bandwidth=<bandwidth>Target bandwidthMbits/sec
-f, --format=<format>Output formatString, k = Kbits/sec, m = Mbits/sec
--abortStop running iperf test/

Example: iperf -c 192.168.1.10 -t 10 -i 1: Run a TCP bandwidth test for 10 seconds against server 192.168.1.10, reporting results every 1 second.

BLE Command​

1. ble [-a <0|1>]

Control BLE advertising state for Bluetooth testing and discovery.

ItemDescriptionData
-a, --adv=<0|1>BLE advertising control0: Advertising Stop, 1: Advertising Begin, default: 0

Example: ble -a 1 : Start BLE advertising mode for device discovery.

Power Mode Command​

1. sleep [-m <0|1|2>]

Configure device sleep mode for low power testing.

ItemDescriptionData
-m, --mode=<0|1|2>Configure device sleep mode for low power testing.0: standby, 1: light sleep, 2: deep sleep, default: 0

Example: sleep -m 2 : Switch device into deep sleep mode.

Tech Support & Product Discussion​

Please submit any technical issue into our forum.

Thank you for choosing our products! We are here to provide you with different support to ensure that your experience with our products is as smooth as possible. We offer several communication channels to cater to different preferences and needs.

Loading Comments...