Wio-SX1262 with XIAO ESP32S3 Kit Connect to Chirpstack

Overview
LoRaWAN is a low-power, wide-area networking protocol built on top of the LoRa technique. It wirelessly connects devices to the internet and manages communication between end-node devices and network gateways.
Followed the Get Started for Lora, we configured Wio-SX1262 with XIAO ESP32S3 as one channel hub lora gateway.
This wiki page explains how set up LoraWAN based on Wio-SX1262 with XIAO ESP32S3 kit as single channel gateway exchange data. And also connect the Sensecap S210x lora sensor node to Wio-SX1262 with XIAO ESP32S3 kit and transmit the sensor data to Chirpstack.
Install Chirpstack locally
Please refer to instruction for installing Chirpstack locally.
- open a browser and visit http://localhost:8080 .
You should see the ChirpStack login page.
- Sign in with the default username
adminand passwordadmin.
Add Device Profile
Add device profiles under Tenant:

Add LaRaWAN Gateway
Register gateway and fill in the gateway EUI:

Added successfully!

Add SenseCAP LoRa Sensor
Configure LoRa Sensor via Sensecraft APP
We are going to add a sensecap sensor node to TTN.
Step 1. Download and Open the Sensecraft App.
Step 2. Press the sensor button and hold for 3 seconds, the LED will flash at 1s frequency.

Step 3. Please click “Scan” to add new device and start scanning the QR code on device.
Step 4. Click the "Advanced Configuration" and select the platform of "Other Platform"
Step 5. Select the Frequenct Plan consistent to gateway. We set gateway to EU868 already, so also sensor as EU868.
Step 6. The device uses OTAA to join the LoRaWAN network by default. Take down the device EUI, App EUI and APP key.
Add to Chirpstack
Step 1. Create an Application

Step 2. Add device in the application and copy the Device EUI and AppKEY to corresponding blank.

Step 3. Check sensor status

Tech Support & Product Discussion
Thank you for choosing our products! We are here to provide you with different support to ensure that your experience with our products is as smooth as possible. We offer several communication channels to cater to different preferences and needs.