Get Started with Meshtastic
When the device is in the states below, please don't manually reboot or turn it off. Or else the device can be dead.
- Not finishing the message transmission process
- Being configured
Get Started
Power on the device
Press once to power on the device. There will be a rising melody, and the green 🟢 LED light will stay on for about 1 s.
If the device doesn't respond when you press the button, please charge it first. Do not use the fast-charging charger.
Power off the device
Hold the button for more than 5s. The device will shut down after three beeps from the buzzer.
Connect via App
Download the Meshtastic App:
- IOS App
- Android App
- Select the target device on the Bluetooth panel.

- Enter the code (default code is
123456) and then clickPairto connect the device.

- Select the target device on the Bluetooth panel.
![]()
- Enter the code (the default code is
123456) and then clickOKto connect the device.
![]()
Configure the LoRa
In order to start communicating over the mesh, you must set your region. This setting controls which frequency range your device uses and should be set according to your regional location.
- IOS App
- Android App

![]()
Region List
| Region Code | Description | Frequency Range (MHz) | Duty Cycle (%) | Power Limit (dBm) |
|---|---|---|---|---|
| UNSET | Unset | N/A | N/A | N/A |
| US | United States | 902.0 - 928.0 | 100 | 30 |
| EU_868 | European Union 868MHz | 869.4 - 869.65 | 10 | 27 |
Refer to LoRa Region by Country for a more comprehensive list.
EU_868 has to adhere to an hourly duty cycle limitation of 10%, calculated every minute on a rolling 1-hour basis. Your device will stop transmitting if you reach it, until it is allowed again.
Now that you have set the LoRa region on your device, you can continue by configuring any LoRa Configs to suit your needs.
Device Status
| Light Status | Device Status | |
|---|---|---|
| 🟢green | Constant | Device Turning on |
| Fast Blinking | Normally Running | |
| Slow Blinking | Charging | |
| Constant | Fully Charged | |
| 🔴Red | Blinking | Low Power |
| ⚪️white | Constant | DFU Mode/Bootloader Mode |
Button Control
| Button Control | Device Respond |
|---|---|
| Click once (Turning off) | Device Turning on |
| Long press for 5s | Device Turning off |
| Double Click | Broadcast node ID and Position |
| Triple Click | Turning on/off GPS |
| four clicks | Temporarily turning on/off buzzer |
Flash Firmware
Please don't use OTA to update the firmware, it may cause the device to be completely dead. For detailed information, please click here
Step 1: Enter DFU mode
Enter DFU via the web flasher. If this fails many times, enter DFU manually.
- Via Web Flasher
- Manually Enter
Visit Meshtastic Web Flasher.
Connect the device to your PC, select the device as SenseCAP Mesh Tracker X1 and choose the latest firmware, then click Flash.
![]()
Click Enter DFU Mode, there will be a serial port named X1 xxx displayed. Click and connect it.
![]()
Try to enter DFU mode manually: press and hold the device button, then quickly connect the device with the computer via USB cable, keep holding the button until a white ⚪️ LED turned on.
To successfully enter the DFU mode, you need to perform this operation quickly. You may need to try multiple times.
![]()
The white ⚪️ LED will be solid if X1 is in DFU mode. And there should be a driver named X1 displayed on your computer.
![]()
Step 2: Flash Erase
Before flashing the firmware, please first erase it!
Click the trash symbol.
![]()
Download the erase firmware and copy it to the driver.
![]()
This process may take some time; wait for the drive to disappear.
Step 3: Flash Firmware
Select the latest firmware, and download the UF2 file.
![]()
Copy the UF2 file to the DFU drive. Firmware should be flashed after the file is downloaded and the device reboots.
Advanced Tutorial
Configure GPS
Please set GPS enabled. You can adjust the update interval and broadcast interval to obtain more up-to-date location information.

For IOS, please turn on the Accurate Location. Otherwise, the positioning may deviate.

Connect via Website
If you want to send text messages and communicate with other nodes in the website, you can connect the device to the Meshtastic Website now.
Step 1: Open the Website
Click here to go to the Website.
Step 2: Add the new device
Click "+ New Connection".
![]()
There are two ways to connect. You can choose your preferred method.
- Bluetooth
- Serial
Choose Bluetooth. Choose the device ID in the pop-up window.
![]()
Choose serial method. Open the device manager to see which port the device is connected to. Choose that port in the pop-up window.
![]()
Your device will be shown in the list. Click to connect. If the connection succeeds, you can see the device status directly on the website.
![]()
Configure Sensor
| Sensor | Description |
|---|---|
| Pressure | ✅ |
| 6-Axis Sensor (future version) | ✅ |
| 3-Axis Sensor (future version) | ✅ |
Buzzer and LED Config
| Type | Output PIN | |
|---|---|---|
| Buzzer | PWM buzzer | 25 |
| LED | RGB | R:03 G:24 B:28 |
| Vibra | - | 05 |
- IOS App
- Android App
Navigate to Settings -> External Notification -> Enable GPIO -> Set Output Pin GPIO.

Navigate to Settings -> External Notification -> Enable GPIO -> Set Output Pin GPIO.

Check External Notification Config for more details.
After you update the device configuration, the device will restart, which may take some time.
Configure Ringtone
Navigate to Settings -> Ringtone Config, then enter the RTTTL ringtone string you want to use for external notifications.
- IOS App
- Android App

![]()
- The Legend of Zelda: Item Get
- Super Mario Theme (Short)
- Mario Coin
- Nokia Ringtone
- Mario Power-Up
- Morse Code CQ
24:d=16,o=5,b=120:g,c6,d6,2g6
24:d=4,o=5,b=100:16e6,16e6,32p,8e6,16c6,8e6,8g6,8p,8g
24:d=8,o=6,b=200:b,e7
24:d=4,o=5,b=180:8e6,8d6,f#,g#,8c#6,8b,d,e,8b,8a,c#,e,2a
powerup:d=16,o=5,b=200:g,a,b,c6,d6,e6,f#6,g6,a6,b6,2c7
24:d=16,o=6,b=120:8c,p,c,p,8c,p,c,4p,8c,p,8c,p,c,p,8c,8p
Configure Buzzer
The buzzer is enabled by default. If you want to disable the buzzer, set Alert Message buzzer, Alert bell buzzer and Use PWM buzzer as shown in the following screenshot.

Configure Message Alert
Message Alert can be configured in External Notification.
- IOS
- Android
Nevigate to Setting -> External Notification
![]()
You can configure to buzzer off + vibra off.
![]()
Or buzzer on + vibra on.
![]()
Nevigate to Setting -> Module Configuration -> External Notification
![]()
Enable External notification enabled, then you can configure to buzzer only, vibra only or buzzer on + vibra on.
![]()
Disable External notification enabled, then you can configure to buzzer off + vibra off.
![]()
FAQ
How to check the device ID
- Check the device back
- Via Serial Tool
The last four digits of the MAC address is the device ID
For example, the device ID of the device below would be A0D4
![]()
Visit Meshtastic Web Flasher.
Click Open Serial Monitor, connect the device to your PC, check the serial log, keyword using nodenum.

![]()
How to reboot the device
Press and hold the button, then connect the charging cable, and release the button immediately.
Temperature Reading Accuracy
The temperature data is read from barometer, rather than reading from an independent temperature sensor.Device will generate heat while operation. So the measured temperature will be higher than the actual temperature.
Power Consumption
You can calculate the power consumption through the Power Consumption Table. This device is equipped with a high-voltage battery. When the battery power is low, it will accelerate the discharge process. This device is equipped with a high-voltage battery. When the battery power is low, it will accelerate the discharge process. So you will notice that the device consumes power very rapidly when it is on low battery.
Troubleshooting
Firmware Update Failed / OTA Recovery
If your SenseCAP MeshTracker X1 fails to start, becomes unresponsive, or the white ⚪️ LED stays solid on after a firmware update, the device may be stuck in DFU mode. Try the following:
- Force a reboot to exit DFU mode: disconnect the USB charging cable, press and hold the device button, connect the USB charging cable, and release the button immediately. Do not keep holding the button — holding it for more than 3 seconds after connecting the cable will force the device back into DFU mode.
- Check whether the device starts normally. If not, connect the device to your computer with a USB data cable and follow Step 1: Enter DFU mode, then perform Step 2: Flash Erase and Step 3: Flash Firmware to reinstall the Meshtastic firmware.
- If the device still cannot be recovered, follow Bootloader Installation to re-flash the bootloader, then reinstall the application firmware.
Do not force a reboot or unplug the USB cable while the firmware is being erased or flashed. If the device cannot enter DFU mode or be detected by your computer, please contact technical support.
Device never turns on
- The device may appear to be powered off when the LED indicator and buzzer are not activated. Before performing the above steps, it is recommended to
check the following parameters:

-
Use a known working USB cable to
charge the devicecontinuously for 1–2 hours to ensure the battery has sufficient power to wake up the system. -
If the device still does not respond after charging,
perform a hard resetas follows: Unplug the USB cable. Press and hold the button, then plug in the USB cable and then release the button immediately. -
If still no luck, Connect a USB cable to a computer. Hold the device button, then connect the device to the computer, then release the button, see whether or not the a disk pop out in your PC. If so, re-install the bootloader
Device stuck in boot loop
Description:
The device will restart repeatedly, and the serial port connects and disconnects repeatedly.
Solution:
- Step 1: Try to enter DFU mode manually: press and hold the device button, then quickly connect the device with the computer via USB cable, keep holding the button until a white ⚪️ LED turned on.
To successfully enter the DFU mode, you need to perform this operation quickly. You may need to try multiple times.
![]()
The device is in DFU mode if the white LED is solid on.
-
Step 2: Erase Flash
-
Step 3: Flash Firmware
Bootloader Installation
When you are flashing the bootloader, please make sure the cable connection is stable and DO NOT disconnect it during the flash process.
Step 1: Adafruit-nrfutil Installation
For Windows users, press the "Win" key and the "r" key, then enter "cmd" in the pop-out window, and click "Enter". This can open the command line.
For MAC users, press the "Command" key and the "Space" key, so that you can open Spotlight. Then enter "termial", click "Return". This can open the command line.
Prerequisites
Check in your command line whether or not Python and pip are installed successfully.
python --version
python -m pip --version
Then "Python xxx" and "pip xxx" should appear. If it does not, please try installing Python again.
This is the recommended method to install the latest version:
pip3 install --user adafruit-nrfutil
Check the installation path:
python -m pip show adafruit-nrfutil
This is the installation location:

For Windows users, you may need to add the path manually. Copy the installation location shown in the last step. Then add it as followed:

Step 2: Check your port number
Connect your device to your PC, and check the port number.
For Windows users, open your device manager, and go to port, the port number newly popped out after the device connection is the device port number.
For Mac users, for example:

For Windows users, for example:

Step 3: Flash the bootloader
In the terminal or command prompt, navigate to the directory where you downloaded the bootloader zip package and execute the following command, replacing the correct port for your device:
- For Windows:
adafruit-nrfutil --verbose dfu serial --package mesh_tracker_x1_bootloader-0.10.0-13.zip -p COMxx -b 115200 --singlebank --touch 1200
Please change COMXX to your COM number. For example, if your device is on com6, change the command to be:
adafruit-nrfutil --verbose dfu serial --package mesh_tracker_x1_bootloader-0.10.0-13.zip -p **COM6** -b 115200 --singlebank --touch 1200
Some of the devices will change their port number after you enter this command. So if the installation fails, check the port number again.
- For others:
adafruit-nrfutil --verbose dfu serial --package mesh_tracker_x1_bootloader-0.10.0-13.zip -p /dev/tty.SLAB_USBtoUART -b 115200 --singlebank --touch 1200

When you have completed the above steps, then you can follow this step to flash the application firmware.
2) Device can not enter DFU mode, but the serial port can be detected.
-
Open a serial port tool
-
Set the baud rate to
1200. -
Connect the device. The light will flash briefly when you connect it. Keep trying this until the light stays on, which means the device can go back to DFU mode, then flash bootloader -> erase flash -> flash the firmware.
3) Device can not enter DFU mode, and no serial port display
-
press and hold the device button, then connect the charging cable, then release the button immediately. After a disk pops out on your PC, you may see the serial port.
-
If still no luck, please disconnect the charging cable and leave the device for a few days until the battery is completely drained, then connect the charging cable and try to pair it again.
4) If none of the above steps work, please contact tech support: support@sensecapmx.com
Device automatically turns off
-
Phenomena Description
-
After the device turns on, it will turn off or reboot automatically after a while.
-
The serial port log ran for a while and then stopped.
This is possibly caused by manually and forcibly rebooting or turning off the device when the device is in the following states: not finishing the message transmission process, being configured......
- Troubleshoot
Click here to perform a flash-erase.
Factory Reset
If you want to restore to the default settings, you can do a factory reset. There are two methods for you to do the factory reset.
-
Click here to flash erase the device, and then re-flash the latest firmware.
-
Click the
Factory Resetbutton on the app. The device will reboot with the factory configuration automatically.
Direct Message Fail
NodeDB Reset
NodeDB is the local database that stores information about nodes discovered in the current Mesh network. If you encounter a situation where you can't communicate with a certain node, it might be because your nodeDB has stored outdated information for that node. You will need to update it.
Open the app and connect to the target device. Go to Settings->Device->Device Config->Reset NodeDB.
![]()
![]()
Exchange User Info
Each node will periodically send its own node information, enabling other nodes in the mesh to "see" and "recognize" it. Two nodes need to exchange their node information with each other in order to be able to communicate with each other. If you are unable to send or receive private messages with another node on the list, you can manually prompt them to exchange information in the app.

Regenerate Private Key
Each node keeps its private key to itself and never shares it. To communicate privately, two nodes exchange their public keys with each other over the mesh. If one node keeps failing in private message transmission, try regenerating the private key for it — this rotates its key pair, so other nodes need to re-sync with its new public key.

Reboot the faulty device to make the configuration function.
After the key regeneration, other devices need to reconnect with the node. So it is better to delete the node from the other device's node list.
Signal Quality
-
SNR reflects the quality of the communication link. A normal device usually operates above -7 dB. A device with a SNR lower than -10 dB indicates poor performance.
-
RSSI is determined jointly by the device and its surrounding environment. A normal device usually operates above -110 dBm. A device with an RSSI lower than -115 dBm is considered to have poor performance.
To achieve the best signal effect, please use the device in an open, unobstructed area with minimal interference for use.