Skip to main content

Getting Started with Seeed Studio XIAO ESP32-C5

Introduction

Seeed Studio XIAO ESP32-C5

Specification

ItemSeeed Studio XIAO ESP32-C5Seeed Studio XIAO ESP32-S3Seeed Studio XIAO ESP32-C3Seeed Studio XIAO ESP32-C6
ProcessorESP32-C5 RISC-V 32-bit @240 MHzESP32R8N8 32-bit Xtensa LX7 dual-core @240 MHzESP32-C3 32-bit RISC-V @160 MHzESP32-C6 32-bit RISC-V @160 MHz
Wireless Connectivity2.4 GHz & 5 GHz dual-band Wi-Fi 6 and Bluetooth 5 (LE)2.4 GHz Wi-Fi and Bluetooth 5 (LE)2.4 GHz Wi-Fi and Bluetooth 5 (LE) 2.4 GHz Wi-Fi 6, Bluetooth 5 (LE)
Memory8 MB PSRAM & 8 MB Flash8 MB PSRAM & 8 MB Flash400 KB SRAM, 4 MB Flash512KB SRAM , 4MB Flash
InterfacesI2C / UART / SPII2C / UART / SPII2C / UART / SPII2C / UART / SPI
PWM/Analog Pins11 / 511 / 911 / 411 / 7
Onboard ButtonsReset / Boot ButtonReset / Boot ButtonReset / Boot ButtonReset button / Boot button
Onboard LEDsCharge / USER LEDCharge / USER LEDCharge LEDCharge / USER LED
Battery Charge ChipSGM40567SGM40567ETA4054S2FSGM40567

Features

  • Powerful CPU: ESP32-C5, 32­bit RISC­-V single­core processor that operates at up to 240 MHz
  • Complete Wi­Fi subsystem: Dual-band Wi-Fi 6 subsystem (2.4 GHz and 5 GHz) compliant with IEEE 802.11 a/b/g/n/ac/ax, supporting Station, SoftAP, concurrent SoftAP+Station operation, and promiscuous (monitor) mode.
  • Bluetooth LE subsystem: Supports features of Bluetooth 5 and Bluetooth mesh
  • Better RF performance: External RF antenna included.
  • Battery charging chip: Supports lithium battery charge and discharge management.
  • Rich on-chip resources: 384 KB on-chip SRAM, 320 KB of ROM
  • Ultra small size: As small as a thumb(21x17.8mm) XIAO series classic form-factor for wearable devices and small projects
  • Reliable security features: Cryptographic hardware accelerators supporting AES-128/256, SHA family hashing, HMAC, a dedicated digital signature peripheral, and Secure Boot (V2).
  • Rich interfaces: 1×I2C, 1×SPI, 2×UART, up to 11×GPIO (PWM-capable), 5×ADC channels, and a JTAG(pads on the reverse side) bonding-pad interface.
  • Single-sided components, surface mounting design

Hardware overview

XIAO ESP32-C5 indication diagram
XIAO ESP32-C5 Pin List

Pin Map

XIAO PinFunctionChip PinAlternate FunctionsDescription
5VVBUSPower Input/Output
GND
3V33V3_OUTPower Output
D0AnalogGPIO1LP_UART_DSRN, LP_GPIO1GPIO, ADC
D1GPIO0LP_UART_DTRN, LP_GPIO0GPIO
D2GPIO25GPIO
D3GPIO7SDIO_DATA1GPIO
D4SDAGPIO23GPIO, I2C Data
D5SCLGPIO24GPIO, I2C Clock
D6TXGPIO11GPIO, UART Transmit
D7RXGPIO12GPIO, UART Receive
D8SCKGPIO8TOUCH7GPIO, SPI Clock
D9MISOGPIO9TOUCH8GPIO, SPI Data
D10MOSIGPIO10TOUCH9GPIO, SPI Data
MTDOGPIO5LP_UART_TXD, LP_GPIO5JTAG
MTDIGPIO3LP_I2C_SCL, LP_GPIO3JTAG, ADC
MTCKGPIO4LP_UART_RXD, LP_GPIO4JTAG, ADC
MTMSGPIO2LP_I2C_SDA, LP_GPIO2JTAG, ADC
ADC_BATGPIO6Read the BAT voltage value
ADC_CRLGPIO26Controls (enables/disables) the measurement circuit to save power.
ResetCHIP_ENEN
BootGPIO28Enter Boot Mode
U.FL-R-SMT1LNA_INUFL antenna
CHARGE_LEDVCC_3V3CHG-LED_Red
USER_LEDGPIO27User Light_Yellow

Getting Started

To enable you to get started with the XIAO ESP32-C5 faster, please read the hardware and software preparation below to prepare the XIAO.

Hardware

You need to prepare the following:

Seeed Studio XIAO ESP32-C5
tip

Some USB cables can only supply power and cannot transfer data. If you don't have a USB cable or don't know if your USB cable can transmit data, you can check Seeed USB Type-C support USB 3.1.

Software

The recommended programming tool for the XIAO ESP32-C5 is the Arduino IDE, so you need to complete the Arduino installation as part of the software preparation.

tip

If this is your first time using Arduino, we highly recommend you to refer to Getting Started with Arduino.

  • Step 1. Download and Install the stable version of Arduino IDE according to your operating system.


  • Step 2. Launch the Arduino application.

  • Step 3. Open BOARDS MANAGER -> Search esp32 -> Install version 3.3.5 or a higher version

Upload Progaram

Let's take a lighting program as an example below

Step 1. Select XIAO_ESP32C5 and PORT. If you don't know the PORT, you can reinsert and remove the XIAO_ESP3-2C5 to check.

Step 2. Paste Code in your Skecth

LED_BUILTIN corresponds to the L LED on the development board.

void setup() {
// put your setup code here, to run once:
pinMode(LED_BUILTIN, OUTPUT);
Serial.begin(9600);
}

void loop() {
// put your main code here, to run repeatedly:
digitalWrite(LED_BUILTIN, LOW);
Serial.print("LED ON \n");
delay(1000);
digitalWrite(LED_BUILTIN, HIGH);
Serial.print("LED OFF \n");
delay(1000);
}

Step 3. Click and Upload


Effect demonstration:

After you upload the program, you will see the L indicator light flashing at intervals of 1 second, and at the same time, the serial monitor will print LED ON and LED OFF.

Deep sleep mode

The XIAO ESP32-C5 features deep sleep and wake-up functions. This example utilizes a high-level trigger on pin D0 to wake the device from deep sleep.
It is important to note that this is a configurable option, as the hardware supports both high-level and low-level triggers to accommodate different circuit designs.

#define WAKEUP_PIN D0 // LP_GPIO1

RTC_DATA_ATTR int bootCount = 0;

void print_wakeup_reason(){
esp_sleep_wakeup_cause_t wakeup_reason = esp_sleep_get_wakeup_cause();

switch(wakeup_reason)
{
case ESP_SLEEP_WAKEUP_EXT0 : Serial.println("Wakeup caused by external signal using RTC_IO"); break;
case ESP_SLEEP_WAKEUP_EXT1 : Serial.println("Wakeup caused by external signal using RTC_CNTL"); break;
case ESP_SLEEP_WAKEUP_TIMER : Serial.println("Wakeup caused by timer"); break;
case ESP_SLEEP_WAKEUP_TOUCHPAD : Serial.println("Wakeup caused by touchpad"); break;
case ESP_SLEEP_WAKEUP_ULP : Serial.println("Wakeup caused by ULP program"); break;
case ESP_SLEEP_WAKEUP_GPIO : Serial.println("Wakeup caused by GPIO"); break;
default : Serial.printf("Wakeup was not caused by deep sleep: %d\n",wakeup_reason); break;
}
}

void setup(){
Serial.begin(115200);
delay(1000);

++bootCount;
Serial.println("Boot number: " + String(bootCount));
print_wakeup_reason();

pinMode(WAKEUP_PIN, INPUT_PULLUP);
pinMode(LED_BUILTIN, OUTPUT);

uint64_t mask = 1ULL << WAKEUP_PIN;
esp_deep_sleep_enable_gpio_wakeup(mask, ESP_GPIO_WAKEUP_GPIO_HIGH);

digitalWrite(LED_BUILTIN, LOW);
delay(100);
digitalWrite(LED_BUILTIN, HIGH);

delay(2000); //Delay time depends on the serial port / Give the PC time to stabilize
Serial.println("Going to sleep now");
esp_deep_sleep_start();
}

void loop(){}

If you are quick enough to turn on the serial monitor before the XIAO goes into deep sleep, then you can see the message output as shown below. This means that the XIAO is now asleep. Then you can also view and activate it by pressing the button.You can also observe the on-off state of the L LED to check if the device has been awakened. Once it is awakened, it will exhibit a flashing effect.

tip

After entering deep sleep mode, the XIAO's port will disappear and you'll need to wake it up to see its port number again!

caution

The XIAO ESP32-C5 supports GPIO wake-up and timer wake-up. To prevent the loss of hardware debugging capabilities and increased difficulty in firmware flashing during low-power development, it is strongly recommended that the JTAG (MTMS, MTDI, MTCK, MTDO) pins be reserved for dedicated use and not employed as wake-up sources for deep sleep mode.

Battery Usage

The XIAO ESP32-C5 is capable of using a 3.7V lithium battery as the power supply input. You can refer to the following diagram for the wiring method.

pir
caution

Please be careful not to short-circuit the positive and negative terminals and burn the battery and equipment when soldering.

Instructions on the use of batteries:

  1. Please use qualified batteries that meet the specifications.
  2. XIAO can be connected to your computer device via data cable while using the battery, rest assured that XIAO has a built-in circuit protection chip, which is safe.
  3. When XIAO ESP32-C5 is powered by a battery, the C LED will light up. You can use this as a basis for determining whether charging management has been carried out.

Check the battery voltage

The XIAO ESP32-C5 is equipped with the SGM40567 battery charging chip and the TPS22916CYFPR battery voltage acquisition chip. You can enable the BAT_VOLT_PIN_EN to activate the battery voltage acquisition function and read the battery voltage through the BAT_VOLT_PIN.

tip

On the XIAO ESP32C5, the pin corresponding to BAT_VOLT_PIN is GPIO6, and the pin corresponding to BAT_VOLT_PIN_EN is GPIO26.

#include <Arduino.h>

void setup() {
Serial.begin(115200);
pinMode(BAT_VOLT_PIN, INPUT); // Configure A0 as ADC input
pinMode(BAT_VOLT_PIN_EN , OUTPUT);
digitalWrite(BAT_VOLT_PIN_EN , HIGH);
}

void loop() {
uint32_t Vbatt = 0;
for(int i = 0; i < 16; i++) {
Vbatt += analogReadMilliVolts(BAT_VOLT_PIN ); // Read and accumulate ADC voltage
}
float Vbattf = 2 * Vbatt / 16 / 1000.0; // Adjust for 1:2 divider and convert to volts
Serial.println(Vbattf, 3); // Output voltage to 3 decimal places
delay(1000); // Wait for 1 second
}
  • analogReadMilliVolts(BAT_Voltage_Read)

    • This function is used to read the current analog voltage from the BAT_VOLT_PIN pin and return a calibrated voltage value in millivolts (mV).
    • Unlike the conventional analogRead(), which only provides a raw ADC value, analogReadMilliVolts() automatically applies the factory calibration parameters embedded in the chip. This results in higher accuracy, improved linearity in voltage measurement, and eliminates the need for manual ADC-to-voltage conversion.
    • During the voltage sampling process, a 16-times repeated sampling is performed through a for loop, and the results are accumulated. The purpose of multiple sampling is to suppress transient noise and discrete errors, thereby improving measurement stability. Finally, the accumulated value is divided by the number of samples (16) to obtain a smoother and more reliable averaged voltage value.
pir
tip

According to the datasheet, the effective measurement range of the ESP32-C5 covers 0~3300 mV. Therefore, the built-in battery voltage acquisition circuit of the XIAO ESP32-C5 is designed with two 100K resistors for voltage division, enabling accurate reading of values.

Resource

Hardware Design

Mechanical Design

Tech Support & Product Discussion

Thank you for choosing our products! We are here to provide you with different support to ensure that your experience with our products is as smooth as possible. We offer several communication channels to cater to different preferences and needs.

Loading Comments...