Seeed Studio XIAO nRF52840 with NuttX(RTOS)
Introduction
NuttX is a mature real-time operating system (RTOS) widely recognized for its standards compliance and small footprint. One of NuttX's main features is its scalability, which allows it to be used in environments ranging from 8-bit microcontrollers to 64-bit systems. This flexibility is achieved through adherence to POSIX and ANSI standards, enabling you to experiment with similar NuttX features across a wide range of chips from different architectures, families, and semiconductor vendors.
Additionally, NuttX offers many advanced and useful features, such as USB, Ethernet, Audio, and Graphics subsystems. These characteristics make NuttX an attractive choice for developers seeking a versatile, robust RTOS capable of operating on various types of hardware.
NuttX supports a vast and continually expanding number of boards. The official documentation provides a comprehensive list of supported boards, organized by architecture and System-on-Chip (SoC) series.
For instance, the Seeed Studio Xiao nRF52840 page in the NuttX documentation offers detailed descriptions of each supported feature and instructions on how to utilize them. Also there is a specific page in the NuttX documentation for Nordic Semiconductor nRF52 series chips.
Tools Setup
The first step to get started with NuttX on XIAO nRF52840 is to install UF2 Tools required to convert the hex file format to uf2, then download NuttX source code itself. The Nuttx provides a guide to different platforms. Follow these steps:
-
Download UF2 Tools:
git clone https://github.com/microsoft/uf2.git -
Create a workspace
mkdir nuttxspace -
Clone the repositories
cd nuttxspace
git clone https://github.com/apache/nuttx.git nuttx
git clone https://github.com/apache/nuttx-apps apps
The Apache Nuttx it's divided into two project:
- Nuttx: contains implemented the kernel, driver and subsystems.
- Apps: contains a collection of tools, shells, network utilities, libraries and interpreters.
Applications
To start an application it's necessary to load a configuration on NuttX, calling the command:
./tools/configurate.sh board_name:your_application
Also it's possible to check the list of board-supported a running the command:
./tools/configurate.sh -L
-
Build NuttX
cd nuttx
make distclean
./tools/configure.sh xiao-nrf52840:nsh
make V=1 -
Convert nuttx.hex to UF2 format using U2F Tools:
python3 uf2/utils/uf2conv.py -c -f 0xADA52840 -i nuttx.hex -o nuttx.uf2 -
Connect the Seeed Studio XIAO nRF52840, and enter bootloader mode by rapidly clicking it twice. The board will be detected as a USB Mass Storage Device. Then copy “nuttx.uf2” into the device.
Hands-on
It's time to explore NuttX practically. In this session, three applications are available: NSH, USBNSH, and JUMBO.
NSH
The NuttShell(NSH) is a shell system to be used in NuttX, similar to bash and other similar options. It supports a rich set of included commands, scripting and the ability to run your own applications as “builtin” (part of the same NuttX binary). The NSH configuration enables console at UART0 using 115200 bps.
We can start the build process clearing the previous configuration
cd ~/nuttxspace/nuttx
make distclean
Now we select the NSH configuration to the xiao-nrf5200 board:
./tools/configurate.sh xiao-nrf52840:nsh
Compile the source code.
make -j
Convert nuttx.hex to UF2 format using U2F Tools:
python3 uf2/utils/uf2conv.py -c -f 0xADA52840 -i nuttx.hex -o nuttx.uf2
Load the firmware into you board and connect the USB-to-Serial to TX and RX pins, then run a serial communication program such as minicon or picocom:
picocom -b 115200 /dev/ttyUSB0
Access the NuttShell console:
NuttShell (NSH) NuttX-12.8.0
nsh>
Typing ?, you will access the available options for commands and built-in applications.
nsh> ?
help usage: [-v] [<cmd>]
. cp exec ls reboot truncate
[ cmp exit mkdir rm uname
? dirname expr mkrd rmdir umount
alias date false mount set unset
unalias dd fdinfo mv sleep uptime
basename df free pidof source usleep
break dmesg help printf test xd
cat echo hexdump ps time
cd env kill pwd true
Builtin Apps:
getprime hello nsh ostest sh
Let's say hello to NuttX, type hello and then it executes the command:
nsh> hello
Hello, World!!
Congratulations, your first interation with NuttX was completed.
USBNSH
Similar to NSH configuration, but using CDC/ACM serial (console enabled in USB Port, at 115200 bps).
We can start the build process clearing the previous configuration
cd ~/nuttxspace/nuttx
make distclean
Now we select the NSH configuration to the xiao-nrf5200 board:
./tools/configurate.sh xiao-nrf52840:usbnsh
Compile the source code.
make -j
Convert nuttx.hex to UF2 format using U2F Tools:
python3 uf2/utils/uf2conv.py -c -f 0xADA52840 -i nuttx.hex -o nuttx.uf2
Load the firmware into you board, run a serial communication program such as minicon or picocom:
picocom -b 115200 /dev/ttyACM0
You must to press Enter 3 times, and then this message will show in the terminal.
NuttShell (NSH) NuttX-12.8.0
nsh>
JUMBO
This configuration enables two example applications, gpio and leds. The General Purpose Input/Output (GPIO) is a microcontroller's most fundamental part, allowing it to connect to the external world. This way we will use the NSH to access and configure those pins as we wish. But first, let's clear the previous configuration.
cd ~/nuttxspace/nuttx
make distclean
Select the jumbo configuration to the xiao-nrf52840 board.
./tools/configurate.sh xiao-nrf52840:jumbo
Compile de the source code.
make -j
Load the firmware into you board, run a serial communication program such as minicon or picocom:
picocom -b 115200 /dev/ttyACM0
You must to press Enter 3 times, and then this message will show in the terminal.
NuttShell (NSH) NuttX-12.8.0
nsh>
To check which options are accepted to interact with this application, type gpio -h, and it will return a list of parameters.
NuttShell (NSH) NuttX-12.8.0
nsh> gpio -h
USAGE: gpio [-t <pintype>] [-w <signo>] [-o <value>] <driver-path>
gpio -h
Where:
<driver-path>: The full path to the GPIO pin driver.
-t <pintype>: Change the pin to this pintype (0-10):
-w <signo>: Wait for a signal if this is an interrupt pin.
-o <value>: Write this value (0 or 1) if this is an output pin.
mation and exit.
Pintypes:
0: GPIO_INPUT_PIN
1: GPIO_INPUT_PIN_PULLUP
IO_INPUT_PIN_PULLDOWN
3: GPIO_OUTPUT_PIN
4: GPIO_OUTPUT_PIN_OPENDRAIN
5: GPIO_INTERRUPT_PIN
6: GPIO_INTERRUPT_HIGH_PIN
7: GPIO_INTERRUPT_LOW_PIN
8: GPIO_INTERRUPT_RISING_PIN
9: GPIO_INTERRUPT_FALLING_PIN
10: GPIO_INTERRUPT_BOTH_PIN
To confirm the GPIO device files were created, type ls/dev. After typing, you can see some gpios were declared define on xiao-nrf52840.h, which represent :
-
RGB LED On board:
- RGB_RED -> P0.26
- RGB_GREEN -> P0.30
- RGB_BLUE -> P0.06
-
GPIOs
- 1 Intput - P0.02(/dev/gpio0)
- 1 Interrupt Input - P0.03(/dev/gpio2)
- 1 Output - P0.28(/dev/gpio1)
nsh> ls /dev
/dev:
console
gpio0
gpio1
gpio2
null
ttyACM0
userleds
zero
nsh>
Following these commands to read gpio0 and gpio2 (with interruption) and write at gpio1.
nsh> gpio /dev/gpio0
Driver: /dev/gpio0
Input pin: Value=0
nsh> gpio /dev/gpio0
Driver: /dev/gpio0
Input pin: Value=1
nsh> gpio -o 0 /dev/gpio1
Driver: /dev/gpio1
Output pin: Value=1
Writing: Value=0
Verify: Value=0
nsh> gpio -w 1 /dev/gpio2
Driver: /dev/gpio2
Interrupt pin: Value=0
Verify: Value=1
The USERLEDS is a subsystem that allows to control of the LEDs with single operation. Also, you can use commands-line like the printf. In this demo we will turn on and turn off the RGB LED on-board each 1 seconds.
Typing leds, you observe the LEDs blinky same time.
NuttShell (NSH) NuttX-12.8.0
nsh> leds
leds_main: Starting the led_daemon
leds_main: led_daemon started
led_daemon (pid# 3): Running
led_daemon: Opening /dev/userleds
led_daemon: Supported LEDs 0x07
led_daemon: LED set 0x01
nsh> led_daemon: LED set 0x02
led_daemon: LED set 0x03
led_daemon: LED set 0x04
led_daemon: LED set 0x05
led_daemon: LED set 0x06
led_daemon: LED set 0x07
Check the video below with the demo for gpio and leds example:
For more information about NuttX RTOS, please visit NuttX Documentation
✨ Contributor Project
- This project is supported by the Seeed Studio Contributor Project.
- A special thanks to Rodrigo for his dedicated efforts. Your work will be exhibited.
Tech Support & Product Discussion
Thank you for choosing our products! We are here to provide you with different support to ensure that your experience with our products is as smooth as possible. We offer several communication channels to cater to different preferences and needs.