Sensing and Network Connectivity
This topic here introduces the Seeed Studio product documentation regarding the very first step of digitized data from physical world, that is, delopying information infrastructures in a dynamic sensing framework, to lay the groundwork for society monitoring and understanding the physical and natural environments.
You can discover this page with two large portions.
- Industrial Sensors with Network Devices
- Entry-level Sensors and Network Modules
Industrial Sensors and Network Devices
We launched industrial grade sensors with long range connectivity and intelligence, generating digitized data from physical world in instrumental-level precision. You can find in this portion with:- Sensors & Probes for various industrial-grade environmental data sensing
- AI-based Sensors for reday-to-deploy intelligent scenarios
- Data Logger for remote environmental data monitoring
- Gateway for long-range, high-security, indoor and outdoor data transmission
- Other network infrastructures for data transmission, such as routers.
Industrial Sensors and Probes
SenseCAP Sensors & Probes
SenseCAP sensors and probes offer multiple ambient data sensing, with industrial hardware design.
SenseCAP S210X Series Sensors
PDF Download of SenseCAP S210X Sereis User GuideSenseCAP S2101 - Temperature and Humidity
SenseCAP S2102 - Wireless Light Intensity
SenseCAP S2103 - Temperature, Humidity and CO2
SenseCAP S2104 - Soil Moisture and Temperature
SenseCAP S2105 - Soil Moisture, Temperature and EC
SenseCAP Multi-in-one Sensors
SenseCAP ORCH S4 - Temperature, Humidity, Atmospheric Pressure, and LightPDF Download of SenseCAP ONE Weather Sensor Sereis User Guide
SenseCAP ONE S500 - Temperature, Humidity, Barometric Pressure, Wind Speed, and Wind Direction
SenseCAP ONE S700 - Temperature, Humidity, Wind Speed/Direction, Barometric Pressure, Light Intensity, Precipitation Intensity
SenseCAP ONE S900 - 9-in-1 sensor, capable of sensing PM2.5 and PM10
SenseCAP ONE S1000 - 10-in-1 sensor, capable of sensing CO2, PM2.5 and PM10
Industrial AI-based Sensors
SenseCAP AI-based Sensors
Built for reday-to-deploy intelligent scenarios, SenseCAP A1101 with intelligent vision is really.
SenseCAP A1101 Vision AI
Getting Started with SenseCAP A1101 Vision AITrain and Deploy Your Own AI Model Into SenseCAP A1101
One Stop Model Training with Edge Impulse
More Coming Soon
Data Logger with Configuration Guide
SenseCAP Data Logger
SenseCAP Data Logger can connect to MODBUS-RTU RS485/Analog/GPIO sensors and transmit data from sensors to the LoRaWAN® / 4G network
SenseCAP S2100 Data Logger
Introduction of SenseCAP S2100 LoRaWAN® Data LoggerConfigure the 12V RS485 Sensor for S2100 Data Logger
Configure the Analog Sensor for S2100 Data Logger
Configure the Counter & GPIO Sensor for S2100 Data Logger
Build LoRaWAN® Sensors with SenseCAP S2110 Sensor Builder and SenseCAP Data Logger
Gateway for Multiple Platform
SenseCAP Gateway
SenseCAP Gateway provides miles of wireless network coverage and data transmission capacity for Long Range / LoRaWAN® devices
Flux-Platform Gateway
SenseCAP M4 Square OverviewSenseCAP M4 Square Quick Start
SenseCAP M4 Square FAQ
Routers for Other Network Infrastructure
Routers
The routers can connect a local network to the Internet, enabling devices communicate with each other.
Entry-level Sensors and Network Modules
Without complicated instruments, we can sense and monitor the physical world just using microcontrollers and simple functional elecrtricals. That is, in this portion you can find:- Grove ecosystem sensors
- Grove communication modules
- Other sensors and communcation modules
Grove Ecosystem Sensors
Grove Sensors
This is the introduction of Grove Sensors.
Grove Communication Modules
Grove Sensor Network
This is the introduction of Grove Sensor Network, the transmittion methods offered to sensors.
Other Sensors and Communication Modules
Sensing Nodes
This is the introduction of Sensing Nodes, other sensors besides Grove ecosystem.
mmWave Radar Sensor
24GHz mmWave Human Static Presence Module Lite - Configurable Parameter24GHz mmWave Fall Detection Sensor , 24GHz mmWave Human Static Presence Sensor
60GHz mmWave Sleep Breathing Monitoring Module
60GHz mmWave Breathing and Heartbeat Module
60GHz mmWave Fall Detection Module Pro
Microwave Sensor - 24GHz Doppler Radar Motion Sensor - MW2401TR11
Beyond Grove / Retired Product
This is the introduction of Seeed Studio ageful sensors and communication modules.
Click HERE to see the full picture.From entry-level to industrial-grade Sensors
- Imagining how quickly you can build industrial-graded IoT sensors and applications in minutes, as well as develop custom open source LoRaWAN devices at low cost.
SenseCAP S2110 Sensor Builder
SenseCAP S2110 Sensor Builder
🔧 An open-source tool to build RS485 sensors with Grove ecosystem > Build LoRaWAN Sensors with SenseCAP S2110 Sensor Builder and SenseCAP Data Logger
From Simple to Sophisticated
- Developing industrial solutions with entry-level sensor hardware.
SenseCAP K1100
SenseCAP K1100
☁️ LoRaWAN®-Network Application > SenseCAP & Node-Red for Cloud Services
Integrated Azure IoT, Power BI, InfluxDB
> Helium Cloud Services
Integrated Azure IoT, Google Sheets, AWS IOT
> TTN Cloud Services
SenseCAP K1100
☁️ WiFi-Network Application > Quick Start With Blynk
> Quick Start With Google Cloud IoT
> Develop in Microsoft Azure IoT Central
> Data visualisation with Power BI
> Advanced WiFi Usage