edit

Debugging with OpenOCD and gdb

Please use openocd 4.0 or newer.

This example assumes you have a Segger J-Link compatible JTAG adapter between your computer and the device (or dev board) you are debugging. It is possible to use an SWD (ST-Link) adapter instead, for this use openocd 0.7 or newer.

Start the openocd server with configuration files matching your hardware:

1
openocd -f interface/jlink.cfg -f target/stm32.cfg

Or, if you are using SWD:

1
openocd -f interface/stlink-v2.cfg -f target/stm32f1x_stlink.cfg

In a second window, start an interactive session with openocd:

1
telnet localhost 4444

This seems to be necessary to avoid "target is not halted" errors and other trouble later:

1
reset_config trst_and_srst

Stop the target (the arm processor):

1
reset halt

If you have not already flashed the binary, using for instance dfu-util, you can do it over JTAG like this:

1
2
3
reset init
flash write_image erase dso-lib.hex 0 ihex
reset halt

In a third window, start gdb or gdbtui:

1
2
3
4
arm-none-eabi-gdb
(gdb) file dso-lib.elf
(gdb) target remote localhost:3333"
(gdb) load dso-lib.elf

You should now be able to run and debug:

1
2
3
(gdb) set $pc = Reset_Handler
(gdb) display/i $pc
(gdb) stepi

Tech Support

Please submit any technical issue into our forum or drop mail to techsupport@seeed.cc.