Skip to main content

Grove - 125KHz RFID Reader

This Grove-125KHz RFID Reader is a module used to read uem4100 RFID card information with two output formats: Uart and Wiegand. It has a sensitivity with maximum 7cm sensing distance. There is also the electronic brick version of this module. It can help you with project like internet of thing and access control system.

And you should use the module below while using RFID reader:

Version

Product VersionChangesReleased Date
Grove - 125KHz RFID Reader V1.0InitialOct 2015

Specifications

ParameterValue/Range
Voltage4.75-5.25V
Working Frequency125 KHz
Sensing Distance(Max)70mm
TTL Output9600 baudrate, 8 data bits, 1 stop bit, and no verify bit
Wiegand Output26 bits Wiegand format, 1 even verify bit, 24 data bits, and 1 odd verify bit
tip
More details about Grove modules please refer to [Grove System](https://wiki.seeedstudio.com/Grove_System/)

Platforms Supported

ArduinoRaspberry Pi
caution
The platforms mentioned above as supported is/are an indication of the module's software or theoritical compatibility. We only provide software library or code examples for Arduino platform in most cases. It is not possible to provide software library / demo code for all possible MCU platforms. Hence, users have to write their own software library.

Getting Started

note
If this is the first time you work with Arduino, we firmly recommend you to see [Getting Started with Arduino](https://wiki.seeedstudio.com/Getting_Started_with_Arduino/) before the start.

Play With Arduino

Hardware

  • Step 1. Prepare the below stuffs:
Seeeduino V4.2Base ShieldGrove - 125KHz RFID Reader
enter image description hereenter image description hereenter image description here
Get One NowGet One NowGet One Now
  • Step 2. Connect Grove - 125KHz RFID Reader to port D2 of Grove-Base Shield.
  • Step 3. Plug Grove - Base Shield into Seeeduino.
  • Step 4. Connect Seeeduino to PC via a USB cable.

note

If we don't have Grove Base Shield, We also can directly connect Grove_Ultrasonic_Ranger to Seeeduino as below.

SeeeduinoGrove - 125KHz RFID Reader
5VRed
GNDBlack
D3White
D2Yellow

Software

  • Step 1. Copy the code into Arduino IDE and upload. If you do not know how to upload the code, please check how to upload code.
/*
link between the computer and the SoftSerial Shield
at 9600 bps 8-N-1
Computer is connected to Hardware UART
SoftSerial Shield is connected to the Software UART:D2&D3
*/
 
#include <SoftwareSerial.h>
 
SoftwareSerial SoftSerial(2, 3);
unsigned char buffer[64]; // buffer array for data receive over serial port
int count = 0; // counter for buffer array
 
void setup()
{
SoftSerial.begin(9600); // the SoftSerial baud rate
Serial.begin(9600); // the Serial port of Arduino baud rate.
}
 
void loop()
{
// if date is coming from software serial port ==> data is coming from SoftSerial shield
if (SoftSerial.available())
{
while(SoftSerial.available()) // reading data into char array
{
buffer[count++] = SoftSerial.read(); // writing data into array
if(count == 64)break;
}
Serial.write(buffer, count); // if no data transmission ends, write buffer to hardware serial port
clearBufferArray(); // call clearBufferArray function to clear the stored data from the array
count = 0; // set counter of while loop to zero
}
if (Serial.available()) // if data is available on hardware serial port ==> data is coming from PC or notebook
SoftSerial.write(Serial.read()); // write it to the SoftSerial shield
}
void clearBufferArray() // function to clear buffer array
{
// clear all index of array with command NULL
for (int i=0; i<count; i++)
{
buffer[i]=NULL;
}
}
  • Step 2. Open the Serial Monitor, the card information can be displayed as shown below:

Wiegand Mode

(Jumper Set to the Right two Pins) You would need to select the jumper to "W" to enter this mode. The Wiegand demo code for Seeeduino is designed to read Wiegand data in interrupt mode.

In Wiegand Mode, output data is formatted with 26bits including 24bits card info and 2 bits parity.

bit012345678910111213141516171819202122232425
-PEDP0
--E0-
--D2[7..0]D1[7..0]D0[7..0]-
  • PE is even bit, PO is odd bit;
  • E is the data bit which was involved in even, O is the data bit which was involved in odd;
  • DX[7..0] is the data bit which correspond to Mifare@ Standard & Light card read only ID;

FAQs

Q1: How to convert the output to Card Number?

A1: Please follow below steps.

  • Take ID: 0009776930 for example:
  • Card Number ID: 0009776930 ------- Decimalism [Start Bit(00) + Card Number(8 numbers)]
  • Output: 0700952F229F ------------- Hex [[Start Bit(07h) + Card Number(8 numbers) + Checksum]
  • The calculator for decimal and hex numbers is available online.

Q2: How to read tags continuously?

A2: The RFID reader can read tags continuously without any setting. Keep the tag 2.5-4 cm from the antenna, and the reader can read data continuously. And if the distance is below 2.5cm, the reader reads data once if not moving tags away.

Resources

Projects

Arduino Based Security Project Using Cayenne: Arduino based Home Security Project. SMS/email alerts when intruder detected. Personalized messages for authorized personnel.

Tech Support & Product Discussion

Thank you for choosing our products! We are here to provide you with different support to ensure that your experience with our products is as smooth as possible. We offer several communication channels to cater to different preferences and needs.

Loading Comments...