edit

LCD 16*2 Characters- Green Yellow back light

Cautions


  1. The LCD panel is made by glass. Any mechanical shock (eg. dropping from high place) will damage the LCD module.

  2. Do not add excessive force on the surface of the display, which may cause the Display color change abnormally.

  3. The polarizer on the LCD is easily get scratched. If possible, do not remove the lCD protective film until the last step of installation.

  4. Never attempt to disassemble or rework the LCD module.

  5. Only Clean the LCD with Isopropyl Alcohol or Ethyl Alcohol. Other solvents(eg.water) may damage the LCD.

  6. When mounting the LCD module, make sure that it is free form twisting, warping and distortion.

  7. Ensure to provide enough space(with cushion) between case and LCD panel to prevent external force adding on it, or it may cause damage to the LCD or degrade the display result.

  8. Only hold the lCD module by its side. Never hold LCD module by add force on the heat seal ot TAB.

  9. Never add force to component of the LCD module. It may cause invisible damage or degrade of the reliability.

  10. LCD module could be easily damaged by static electricity. Be careful to maintain an optimum anti-static work environment to protect the LCD module.

  11. When peeling off the protective film from LCD, static charge may cause abnormal display pattern. It is normal and will resume to nomal in a short while.

  12. Take care and prevent get hurt by the LCD panel sharp edge.

  13. Never operate the LCD module exceed the absolute maximum ratings.

  14. Keep the signal line as short as possible to prevent noisy signal applying to LCD module.

  15. Never apply signal to the LCD module without power supply.

  16. IC chip(eg. TAB or COG) is sensitive to the light. Strong lighting environment could possibly cause malfunction. Light sealing structure casing is recommend.

  17. LCD module reliability may be reduced by temperature shock.

  18. When storing the lCD module, avoid exposure to the direct sunlight, high humidity, high temperature or low temperature. They may damage or degrade the LCD module.

Schematic


Block Diagram

Specification


  • LCD Display Mode: STN, Positive, Transflective

  • Display Color: Deep Blue/ Yellow Green

  • Viewing Angle: 6H

  • Driving Method : 1/16 duty, ⅕ bias

  • Back Light : Yellow-Green LED backlight

  • Outline Dimension: 80*36*15.8 MAX

Note

  1. Color tone may slightly change by Temperature and Driving Condition.
  2. The Color is defined as the inactive/background color

AC Characteristics

Vss=0V,VDD=5V,TOP=25℃

Item Symbol MIN TYP MAX Unit
E cycle time tc 1500 - - ns
E high level width twh 700 - - ns
E low level width twl 700 - - ns
E rise time tr - - 18 ns
E fall time tf - - 18 ns
Address set-up time tas 5 - - ns
Address set-up time tasu 210 - - ns
Address hold time tah 15 - - ns
Data set-up time tdsw 300 - - ns
Data delay time td - - 480 ns
Data hold time(write) tdhw 15 - - ns
Data hold time(read) tdhr 30 - - ns
![](https://github.com/SeeedDocument/LCD_16-2_Characters-Green_Yellow_back_light/raw/master/img/LCD-module-WTiming.jpg) ![](https://github.com/SeeedDocument/LCD_16-2_Characters-Green_Yellow_back_light/raw/master/img/LCD-module-RTiming.jpg)
**Host Writing Timing Diagram** **Host Read Timing Diagram**

Pin definition and Rating


Pin No Pin Name I/O Descriptions
1 VSS Power Negative Power supply, Ground(0V)
2 VDD Power Positive power supply
3 V0 Power LCD contrast reference
4 RS Input

  • RS=HIGH:DB0-DB7=Display RAM data

  • RS=LOW:DB0-DB7=Instruction data

5 R/W Input

In read mode

R/W=HIGH

Data read form the LCD module,

data appears at DB0-DB7 and can be read by the host while, E=H and the device is being selected

In write mode

R/W=LOW;

Data write to the LCD module,

data appears at DB0-DB7 will be written into the LCD module at E=H->L and device is being selected.

6 E Input
7 DB0 I/O Data bus;

Three state I/O terminal for display data or instruction data

.. .. ..
14 DB7 I/O
15 CS1 input Chip Selection,

When CS1=1(*1)

Enable access to the Left Side (64column) of the LCD module

16 CS2 Input Chip Selection,

When CS2=1(*1)

Enable access to the Right Side (64column) of the LCD module

17 /RST Input Reset signal

/RST = L,

Display off

display start line register becomes 0

no command or instruction data could be accepted

/RST = H

Normal running

18 VOUT Output Power Booster output for V0
19 BLA Power Positive Power for LED backlight
20 BLK Power Negative Power for LED backlight

Note:

Display or instruction data could write into the LCD mudule's driver/controllers individually or at the same time.

Only read display or instruction data form one of the driver/controller in the LCD module at a time, otherwise unexpected data collision may occur.

Mechanic Dimensions


Outline Dimension:98.0*60.0*13.7MAX (See attached outline Drawing for details)

Usage


Internal Registers

There are three registers in each section of LCD module. Each of them could be controlled independently.

Page(X) Address Register

X address register designates pages of the internal display data RAM. Count function is not available. The address should set by instruction.

Column(Y) Address Counter

Y address counter designates address of the internal display data RAM. It could be set by instruction and is increased by 1 automatically by read or write display data operations.

Display Start Line (Z) Register

Z address register indicates of display data RAM to LCD top line. It may be used for scrolling display pattern on the LCD.

Programming


Basic Setting

To drive the LCD module correctly and provide normally display, please use the following setting

  • Display start line(Z address )=0

  • LCD Display = on

Note

  1. These setting/commands should issue to the LCD module while start up.
  2. See the Display Commands section for details.

Adjusting the LCD display contrast

A Variable-Resistor must be connected to the LCD module for providing a reference to V0. Adjusting the VR will result the change of LCD display contrast. The recommended value of VR is 25k to 50k.

Resetting the LCD module

The LCD module should be initialized by setting /RST terminal at low level when turning the power on.

When /RST pull low, the LCD mudule will:

  • Display off

  • Display start line register becomes 0. (Z-address=0)

While /RST is low, no instruction can be accepted except status read. Therefore, execute other instructions after making sure that DB4=0(cleat /RST) and DB7=0(ready) by status read instruction. The conditions of power supply at initial power up are as follow:

Item Symbol Min Tpy Max Unit
Reset time trs 2.0 - - us
Rise time tr - - 150 ns

Resources

Tech Support

Please submit any technical issue into our forum or drop mail to techsupport@seeed.cc.