Skip to main content

Quick Start

POE connection

SenseCAP M2 supports PoE (Power on Ethernet) and is compatible with IEEE 802.3 af standard.

tip

You will need to have an extra PoE switch that provides 40V-57V DC power as a PSE (Power Sourcing Equipment) if your modem/router does not support PoE.

pir

Gateway Network Configuration

Connect the antenna and power adaptor to the gateway. The power LED will show in red, and in about 15s, the indicator on the top will flash green, indicating that the gateway is booting.

pir

There are two ways to connect to the Internet. Choose the one that works for you.

Ethernet Connection

Connect the Ethernet cable to the Ethernet port, and the indicator on the top will show solid green if the gateway is successfully connected to the internet.

WIFI Connection

There are two ways for users to login Luci configuration page.

Access via router

  • Step 1: Connect your device to a Ethernet cable, and connect your PC to the same router.
Your PC and device should be connected to the same router/network.

pir

  • Step 2: Get IP Address of your device

Check the IP Address of your device on your router admin page.

  • Step 3: Get your device Username and Password

You can find the Username and Password on your device label.

pir

  • Step 4: Login Luci

Input the IP Address of your device in a browser to enter the Luci page. Then input your device username and password to login.

pir

Access via device AP hotspot

  • Step 1: Turn on the device AP hotspot.

Press the button for 5s until the blue indicator flashes slowly to enter the configuration mode.

  • Step 2: Connect to the AP hotspot. AP hotspot name is SenseCAP_XXXXXX (6-figure MAC address),default password is 12345678; connect your computer to this AP hotspot.

pir

  • Step 3: Get your device Username and Password

You can find the Username and Password on your device label.

pir

  • Step 4: Log in to the Local Console

Input the IP Address (192.168.168.1) in your browser to enter the Local Console. Then input your device username and password, and click the Login button.

pir

Connect to a WIFI

  • Step 1: Click on Network - Wireless

pir

  • Step 2: Click on the Scan button to scan the WIFI.

pir

  • Step 3: Select your WI-FI to join the network.

pir

  • Step 4: Submit the Wi-Fi password, and then click Submit and Save.

pir

Then click Save and Apply to apply your settings.

The indicator on the top will show solid green if the gateway is successfully connected to the WIFI.

Cellular Connection (for 4G version)

  • Step 1: Plug your SIM card into the Nano-SIM card slot

pir

  • Step 2: Login the Luci page, and click on Network - Cellular

pir

  • Step 3: Setup the APN info, and click Save and Apply to apply your settings.

pir

Channel Plan Settings

Navigate to LoRaChannel Plan

pir

Select the Region and Frequency plan.

pir

After setting, click Save&Apply.

Checking the Gateway Connection Status

After powering on the gateway, there are two ways for you to check the gateway working status:

LED Indicator

ModeDescription

Green

SolidGateway is healthy and the internet is well connected.
Slow blinkingGateway is booting, please wait.

Blue

Solid

The gateway is ready for internet connection.

Further configuration is needed.

Slow blinkingConfiguration mode, and will auto exit after 5 mins if no activity.

Fast blinking

Press the button for 30s until the indicator show fast flash will trigger the factory reset.

Orange

Slow blinking

Firmware is updating, and please do not power off the gateway or
disconnect the internet.

White

Solid

Gateway is only with a factory firmware, and will be updated to the latest firmware automatically
when it is connected to the internet.

Red

SolidHardware issue or internet connection failure.
Slow blinkingGateway not connected to the LNS.

SenseCAP Mate APP

In the SenseCAP Mate App, Online status indicates Online when the gateway is connected to the network. Please refer to the next chapter for obtaining the SenseCAP App.

Bind the gateway

SenseCAP Mate APP supports device configuration and remote management.

  • Step 1: Download the SenseCAP Mate APP

pir

  • Step 2: Login the APP If it is your first time to use the SenseCAP platform, please register an account first.
tip

Please select Global of Server Location.

pir

  • Step 3: Add device

Click the + in the upper right corner and select Add device Then scan the QR code on your gateway label.

pir

Set up your device name and location. Then confirm your settings. After successful binding, you will see your gateway in the Device directory.

pir

Connect the SenseCAP Sensors

  • Step 1: Add device

Click the + in the upper right corner and select Add device Then scan the QR code on your gateway label.

pir

  • Step 2: Select the frequency plan

Click on Settings, set the platform and frequency, the frequency should match your gateway frequency.

eg: If your gateway is US915 version , then you need to set your sensor to US915 frequency.

pir

tip

SenseCAP M2 Multi-Platform Gateway can’t connect to Helium network.

For more configurations about SenseCAP sensors, please refer to: SenseCAP Sensors

SenseCAP Portal and Mate APP

SenseCAP Mate APP and SenseCAP Portal can be used to check your device status and device management.

Gateway Info

Check the gateway info on the SenseCAP Portal and SenseCAP Mate APP

pir

Sensor data

Check the sensor data on the SenseCAP Portal and SenseCAP Mate APP

pir

Loading Comments...