edit

Grove - Adjustable PIR Motion Sensor

Grove - Adjustable PIR Motion Sensor is an easy to use Passive Infrared motion sensor, which can detect infrared object motion up to 3 meters. Any infrared object moves in its detecting range, the sensor outputs HIGH on its SIG pin. And you can adjust the SIG HIGH time up to 130s via the potentiometer, moreover, you can adjust the detect range via the other potentiometer.

Features

  • Built-in filter, high immunity to RFI
  • Output time, sensitivity and detect range adjustable
  • Low voltage, low power consumption

Specification

Item Value
Operating Voltage 3.3V / 5V
Operating Temperature -30℃ ~ 70℃
Viewing Angel Horizontal placement 80°
Vertical placement 55°
Detction Spectral Response(λ) 5nm ~ 14nm
Detction Distance 0 ~ 3m
High Level On Time <130s
Interface Digital

Typical applications

  • PIR motion detection
  • Intruder detection
  • Occupancy detection
  • Motion sensor lights
  • Security system
  • Automatic control

Hardware Overview

Pin Out

Warning

The Fresnel lens equipped with the module is a plastic piece and is prohibited from approaching high temperatures or open flames.

Schemaitc

Power

The typical voltage of L221D is 3.3V, so we use the XC6206P332MR chip to provide a stable 3.3V. The input of XC6206P33 ranges from 1.8V to 6.0V, so you can use this module with your Arduino both in 3.3V and 5V.

Platforms Supported

Arduino Raspberry Pi BeagleBone Wio LinkIt ONE

Caution

The platforms mentioned above as supported is/are an indication of the module's software or theoritical compatibility. We only provide software library or code examples for Arduino platform in most cases. It is not possible to provide software library / demo code for all possible MCU platforms. Hence, users have to write their own software library.

Getting Started

Play With Arduino

Hardware

Materials required

Seeeduino V4.2 Base Shield Adjustable PIR Motion Sensor Grove - Blue LED
enter image description here enter image description here enter image description here
Get One Now Get One Now Get One Now Get One Now

Note

1 Please plug the USB cable gently, otherwise you may damage the port. Please use the USB cable with 4 wires inside, the 2 wires cable can't transfer data. If you are not sure about the wire you have, you can click here to buy

2 Each Grove module comes with a Grove cable when you buy. In case you lose the Grove cable, you can click here to buy.

  • Step 1. Connect the Grove - Adjustable PIR Motion Sensor to port D2 of Grove-Base Shield, connect the Grobe - Blue LED to the D4 port of the Grove-Base Shield.

  • Step 2. Plug Grove - Base Shield into Seeeduino.

  • Step 3. Connect Seeeduino to PC via a USB cable.

Note

If we don't have Grove Base Shield, We also can directly connect this module to Seeeduino as below.

Seeeduino Grove Cable Grove - Adjustable PIR Motion Sensor
GND Black GND
5V or 3.3V Red VCC
NO connection White NC
D2 Yellow SIG
Seeeduino Grove Cable Grove - Blue LED
GND Black GND
5V or 3.3V Red VCC
NO connection White NC
D4 Yellow SIG

Software

Attention

If this is the first time you work with Arduino, we strongly recommend you to see Getting Started with Arduino before the start.

  • Step 1. Just click the icon in upper right corner of the code block to copy the following code into a new sketch in the Arduino IDE.
 1
 2
 3
 4
 5
 6
 7
 8
 9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
/*macro definitions of PIR motion sensor pin and LED pin*/
#define PIR_MOTION_SENSOR 2//Use pin 2 to receive the signal from the module 
#define LED 4//the Grove - LED is connected to D4 of Arduino

void setup()
{
    pinsInit();
}

void loop() 
{
    if(isPeopleDetected())//if it detects the moving people?
        turnOnLED();
    else
        turnOffLED();
}
void pinsInit()
{
    pinMode(PIR_MOTION_SENSOR, INPUT);
    pinMode(LED,OUTPUT);
}
void turnOnLED()
{
    digitalWrite(LED,HIGH);
}
void turnOffLED()
{
    digitalWrite(LED,LOW);
}
/***************************************************************/
/*Function: Detect whether anyone moves in it's detecting range*/
/*Return:-boolean, ture is someone detected.*/
boolean isPeopleDetected()
{
    int sensorValue = digitalRead(PIR_MOTION_SENSOR);
    if(sensorValue == HIGH)//if the sensor value is HIGH?
    {
        return true;//yes,return ture
    }
    else
    {
        return false;//no,return false
    }
}
  • Step 2. Upload the demo. If you do not know how to upload the code, please check How to upload code.

Success

If every thing goes well, When someone approaches this sensor or when you approach this sensor with your hand, the LED will light up.

Resources

Tech Support

Please do not hesitate to submit the issue into our forum