Grove - Gas Sensor
The Grove - Gas Sensor module is useful for gas leakage detecting(in home and industry). It can detect LPG, i-butane, methane, alcohol, Hydrogen, smoke and so on. Measurements can be taken as soon as possible based on its fast response time. Also the sensitivity can be adjusted by the potentiometer.
Each Grove - Gas Sensor Kit consists of one gas sensor base and four detectors. You can switch the detector on the base according to specific target gases.
- Grove - Gas Sensor(MQ2):Combustible Gas, Smoke
- Grove - Gas Sensor(MQ3):Alcohol Vapor
- Grove - Gas Sensor(MQ5):LPG, Natural Gas, Town Gas
- Grove - Gas Sensor(MQ9):Carbon Monoxide, Coal Gas, Liquefied Gas
Specification
- Working Voltage: 4.9-5.1V
- Heating consumption: 0.5-800mW
- Load resistance: can adjust
- Heater resistance: 33Ω
- Sensing Resistance: 3-30kΩ
- Working Temperature: -25~70 ℃
More details about Grove modules please refer to [Grove System](https://wiki.seeedstudio.com/Grove_System/)
Getting Started
Connect the module with Grove Shield using A0 like following picture and use the program below to gain the voltage. The higher the concentration of the gas is, the bigger the output voltage of the SIG pin gets. Sensitivity can be regulated by rotating the potentiometer. Please note that the best preheat time of the sensor is about 24 hours. For the detailed information about the sensor, please refer to the datasheet.s
Resources
This Markdown file was created from https://www.seeedstudio.com/wiki/Grove_-_Gas_Sensor
Tech Support & Product Discussion
Thank you for choosing our products! We are here to provide you with different support to ensure that your experience with our products is as smooth as possible. We offer several communication channels to cater to different preferences and needs.