Skip to main content

Grove - RJ45 Adapter

The Grove-RJ45 Adapter is a module which can convert a standard Grove connector to a RJ45 connector. Universal 4-Pin Grove cables can not meet the requirements when Arduino remote connect and control Grove module. Through two RJ45 adapter and a cable, It is able to achieve communication between Arduino and Grove module. This help solve the problem that Arduino and Grove are not convenient to connect because of the distance issue.

Feature


  • Standard Grove Connector and RJ45 Connector

  • Applications Widely

  • Easy to use

Interface Function


Grove Connecter R45 Connector
VCC A7
GND A8
D1 A5
D2 A4

Usage


If you want to use the Moisture Sensor to real-time detect the moisture of soil in your garden, but you do not want to go to the garden personally. How to do it? Using two RJ45 adapter and a long network cable, you can solve this problem. The Hardware Installation should be:

You may need to write the code by yourself for the special applications. But we can guarantee that you can always know the soil moisture of plants by observing the output data of the moisture sensor.

You may want to ask why not use a long Grove cable instead of two Grove - RJ45 and a network cable, the reason is the network cable has a weak attenuation.

Schematic Online Viewer

Resource


Tech Support & Product Discussion

Thank you for choosing our products! We are here to provide you with different support to ensure that your experience with our products is as smooth as possible. We offer several communication channels to cater to different preferences and needs.

Loading Comments...