edit

Overview

This repo introduce how to install the File System library used on Wio Terminal. It provides basic functionality of File operating with the SD card, allowing to Read/Write in or from the SD card using SPI interface.

Installing the File System Library For Wio Terminal

  1. Visit the Seeed_Arduino_FS repositories and download the entire repo to your local drive.

  2. Now, the TFT LCD library can be installed to the Arduino IDE. Open the Arduino IDE, and click sketch -> Include Library -> Add .ZIP Library, and choose the Seeed_Arduino_LCD file that you've have just downloaded.

InstallLibrary