edit

Reading/Writing from the SD Card

This repo describes how to Read/Write from or to the SD Card. With this, you are able to load data from the SD Card, a simple demonstration will be storing sensor reading to the SD Card.

Initializing the SD Card on ResScreen

Include theSeeed_FS libraries as follow. And initializing the SD Card using: SD.begin(SDCARD_SS_PIN, SDCARD_SPI), where SPI is used to communicate in Wio Terminal for SD Card.

 1
 2
 3
 4
 5
 6
 7
 8
 9
10
11
12
13
14
15
16
17
#include <SPI.h>
#include <Seeed_FS.h>
#include "SD/Seeed_SD.h"

File myFile; //Intialise the file Class and named it myFile

void setup() {
  Serial.begin(115200);
  while (!Serial) {
  }

  Serial.print("Initializing SD card...");
  if (!SD.begin(SDCARD_SS_PIN, SDCARD_SPI)) {
    Serial.println("initialization failed!");
    while (1);
  }
  Serial.println("initialization done.");

Writing to the SD Card

To write in the SD Card, need to first open the file. There are different modes for the file system so need to state what mode to use while opening the file, modes are as follow:

FILE MODE Name Defined
WRITE FILE_WRITE
READ FILE_READ
APPEND FILE_APPEND

To open the file, the open File Class member function is used and takes 2 parameters as follow:

1
open(const char *filepath, uint8_t mode = FILE_READ) //default mode is READ

In this case, open a txt file name test.txt and FILE_WRITE is used. To write inside a txt file can use println function(File Class):

 1
 2
 3
 4
 5
 6
 7
 8
 9
10
11
12
13
14
15
  // open the file. note that only one file can be open at a time,
  // so you have to close this one before opening another.
  myFile = SD.open("test.txt", FILE_WRITE); //Writing Mode

  // if the file opened okay, write to it:
  if (myFile) {
    Serial.print("Writing to test.txt...");
    myFile.println("testing 1, 2, 3."); //Writing this to the txt file
    // close the file:
    myFile.close();
    Serial.println("done.");
  } else {
    // if the file didn't open, print an error:
    Serial.println("error opening test.txt");
  }

Note: One file at the time, so close a file when done.

Reading from the SD Card

To read a file from SD Card, also needs to open the file. This time, using FILE_READ mode to only read the file.

Using the File member function availble() to check the availablity of the file and read() to print out things inside the file .

 1
 2
 3
 4
 5
 6
 7
 8
 9
10
11
12
13
14
15
myFile = SD.open("test.txt", FILE_READ); //Read Mode
  if (myFile) {
    Serial.println("test.txt:");

    // read from the file until there's nothing else in it:
    while (myFile.available()) {
      Serial.write(myFile.read());
    }
    // close the file:
    myFile.close();
  } else {
    // if the file didn't open, print an error:
    Serial.println("error opening test.txt");
  }
}

Complete Code

 1
 2
 3
 4
 5
 6
 7
 8
 9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
#include <SPI.h>
#include <Seeed_FS.h>
#include "SD/Seeed_SD.h"

File myFile;

void setup() {
  Serial.begin(115200);
  while (!Serial) {
  }
  Serial.print("Initializing SD card...");
  if (!SD.begin(SDCARD_SS_PIN, SDCARD_SPI)) {
    Serial.println("initialization failed!");
    while (1);
  }
  Serial.println("initialization done.");

  // open the file. note that only one file can be open at a time,
  // so you have to close this one before opening another.
  myFile = SD.open("test.txt", FILE_WRITE);

  // if the file opened okay, write to it:
  if (myFile) {
    Serial.print("Writing to test.txt...");
    myFile.println("testing 1, 2, 3.");
    // close the file:
    myFile.close();
    Serial.println("done.");
  } else {
    // if the file didn't open, print an error:
    Serial.println("error opening test.txt");
  }

  // re-open the file for reading:
  myFile = SD.open("test.txt", FILE_READ);
  if (myFile) {
    Serial.println("test.txt:");

    // read from the file until there's nothing else in it:
    while (myFile.available()) {
      Serial.write(myFile.read());
    }
    // close the file:
    myFile.close();
  } else {
    // if the file didn't open, print an error:
    Serial.println("error opening test.txt");
  }
}

void loop() {
  // nothing happens after setup
}