Grove - Air Quality Sensor v1.3
This sensor is designed for comprehensive monitor over indoor air condition. It's responsive to a wide scope of harmful gases, as carbon monoxide, alcohol, acetone, thinner, formaldehyde and so on. Due to the measuring mechanism, this sensor can't output specific data to describe target gases' concentrations quantitatively. But it's still competent enough to be used in applications that require only qualitative results, like auto refresher sprayers and auto air cycling systems.
Features¶
- Responsive to a wide scope of target gases
- Cost efficient
- Durable
- Compatible with 5V and 3.3V
Cautions
- Requires relatively clean air as an initial condition.
- Long time exposure to highly polluted air can significantly weaken its sensitivity.
- Coffre-fort et armoire forte:
Usage¶
With Arduino
As described in Introduction, this sensor performs better in providing qualitative results over a wide scope of target gases. In this demo, we will define 4 statuses for reference in the '.cpp' file. They are:
- a. air fresh -- indicating a good air condition
- b. low pollution -- indicating a rather low concentration of target gases exist.
- c. high pollution(without "Force signal active" message printed on serial monitor) -- you should be aware of the pollution level and consider if some measures could be taken.
- d. high pollution(with "Force signal active" message printed on serial monitor) -- instant measures should be taken to improve the air quality.
We encapsulated the decision structure in a '.cpp' file. You can find information there on how to modify the thresholds.
Let's try it out!
1.Connect the Sensor to A0 port of Grove - Base Shield.
2.Download the File :AirQuality_Sensor Library.
3.Wait at least 2 minutes after powering on for heat-up of the sensor. Then open the example below by the path: File -> Example ->AirQuality_Sensor->AirQuality_Sensor.
/* AirQuality Demo V1.0. connect to A1 to start testing. it will needs about 20s to start * By: http://www.seeedstudio.com */ #include "AirQuality.h" #include "Arduino.h" AirQuality airqualitysensor; int current_quality =-1; void setup() { Serial.begin(9600); airqualitysensor.init(14); } void loop() { current_quality=airqualitysensor.slope(); if (current_quality >= 0)// if a valid data returned. { if (current_quality==0) Serial.println("High pollution! Force signal active"); else if (current_quality==1) Serial.println("High pollution!"); else if (current_quality==2) Serial.println("Low pollution!"); else if (current_quality ==3) Serial.println("Fresh air"); } } ISR(TIMER2_OVF_vect) { if(airqualitysensor.counter==122)//set 2 seconds as a detected duty { airqualitysensor.last_vol=airqualitysensor.first_vol; airqualitysensor.first_vol=analogRead(A0); // change this value if you use another A port airqualitysensor.counter=0; airqualitysensor.timer_index=1; PORTB=PORTB^0x20; } else { airqualitysensor.counter++; } }
4.Upload the code.
5.Open serial monitor.
To adjust the thresholds and indicating messages, refer to the decision structure below in the .cpp file.
int AirQuality::slope(void) { while(timer_index) { if(first_vol-last_vol>400||first_vol>700) { Serial.println("High pollution! Force signal active."); timer_index=0; avg_voltage(); return 0; } else if((first_vol-last_vol>400&&first_vol<700)||first_vol-vol_standard>150) { Serial.print("sensor_value:"); Serial.print(first_vol); Serial.println("\t High pollution!"); timer_index=0; avg_voltage(); return 1; } else if((first_vol-last_vol>200&&first_vol<700)||first_vol-vol_standard>50) { //Serial.println(first_vol-last_vol); Serial.print("sensor_value:"); Serial.print(first_vol); Serial.println("\t Low pollution!"); timer_index=0; avg_voltage(); return 2; } else { avg_voltage(); Serial.print("sensor_value:"); Serial.print(first_vol); Serial.println("\t Air fresh"); timer_index=0; return 3; } } return -1; }
With Raspberry Pi
1.You need to prepare a raspberry pi and a grovepi or grovepi+.
2.You need to completed configuring the development enviroment, otherwise follow here.
3.Connection - Plug the sensor to grovepi socket A0 by using a grove cable.
4.Navigate to the demos' directory:
cd yourpath/GrovePi/Software/Python/
To see the code
nano grove_air_quality_sensor.py # "Ctrl+x" to exit #
import time import grovepi # Connect the Grove Air Quality Sensor to analog port A0 # SIG,NC,VCC,GND air_sensor = 0 grovepi.pinMode(air_sensor,"INPUT") while True: try: # Get sensor value sensor_value = grovepi.analogRead(air_sensor) if sensor_value > 700: print "High pollution" elif sensor_value > 300: print "Low pollution" else: print "Air fresh" print "sensor_value =", sensor_value time.sleep(.5) except IOError: print "Error"
5.Run the demo.
sudo python grove_air_quality_sensor.py
Resources¶
- AirQuality Sensor Library.zip
- Grove_-_Air_quality_sensor_v1.3_sch_pcb.zip
- Grove_-_Air_quality_sensor_v1.3_sch.pdf
- Air_quality_sensor_MP503_Chinese.pdf
- Air_quality sensor_MP503_English.pdf
Tech Support¶
Please do not hesitate to contact techsupport@seeed.cc if you have any technical issue. Or submit the issue into our forum.