edit

Grove - 4-Digit Display

Grove - 4-Digit Display module is a 12-pin module. In this module, we utilise a TM1637 to scale down the number of controlling pins to 2. That is to say, it controls both the content and the luminance via only 2 digital pins of Arduino or Seeeduino. For projects that require alpha-numeric display, this can be a nice choice.

Version

Product Version Changes Released Date
Grove - 4-Digit Display V1.0 Initial May 2012

Features

  • 4 digit red alpha-numeric display
  • Grove compatible interface (3.3V/5V)
  • 8 adjustable luminance levels

Tip

More details about Grove modules please refer to Grove System

Specifications

Item Min Typical Max Unit
Voltage 3.3 5.0 5.5 VDC
Current 0.2 27 80 mA
Dimensions 42x24x14 mm
Net Weight 7±1 g

Application Ideas

  • Time display
  • Stopwatch
  • Sensors' input display

Platforms Supported

Arduino Raspberry Pi BeagleBone Wio LinkIt ONE

Caution

The platforms mentioned above as supported is/are an indication of the module's software or theoritical compatibility. We only provide software library or code examples for Arduino platform in most cases. It is not possible to provide software library / demo code for all possible MCU platforms. Hence, users have to write their own software library.

Getting Started

Note

If this is the first time you work with Arduino, we firmly recommend you to see Getting Started with Arduino before the start.

Play With Arduino

Hardware

  • Step 1. Prepare the below stuffs:
Seeeduino V4.2 Base Shield Grove-4-Digit Display
enter image description here enter image description here enter image description here
Get One Now Get One Now Get One Now
  • Step 2. Connect Grove-4-Digit Display to D2 port of Grove-Base Shield.
  • Step 3. Plug Grove - Base Shield into Seeeduino.
  • Step 4. Connect Seeeduino to PC via a USB cable.

Note

If we don't have Grove Base Shield, We also can directly connect Grove-4-Digit Display to Seeeduino as below. We also can plug Grove-4-Digit Display to other Grove digital port.

Seeeduino Grove-4-Digit Display
5V Red
GND Black
D3 White (DIO)
D2 Yellow(CLK)

Warning

The Grove-4-Digit Display includes 4 pins, GND, VCC, DIO, CLK. We can connect DIO and CLK to any digital pin. It is not I2C protocol.

Software

  • Step 4. We will see the Grove-4-Digit Display being turned on.

Play With Raspberry Pi (With Grove Base Hat for Raspberry Pi)

Hardware

  • Step 1. Things used in this project:
Raspberry pi Grove Base Hat for RasPi Grove - 4 Digit Display
enter image description here enter image description here enter image description here
Get ONE Now Get ONE Now Get ONE Now
  • Step 2. Plug the Grove Base Hat into Raspberry Pi.
  • Step 3. Connect the 4-digit display to port 12 of the Base Hat.
  • Step 4. Connect the Raspberry Pi to PC through USB cable.

Note

For step 3 you are able to connect the digit to any GPIO Port but make sure you change the command with the corresponding port number.

Software

  • Step 1. Follow Setting Software to configure the development environment.
  • Step 2. Download the source file by cloning the grove.py library.
1
2
cd ~
git clone https://github.com/Seeed-Studio/grove.py
  • Step 3. Excute below commands to run the code.
1
2
cd grove.py/grove
python grove_4_digit_display.py 12 13

Following is the grove_4_digit_display.py code.

  1
  2
  3
  4
  5
  6
  7
  8
  9
 10
 11
 12
 13
 14
 15
 16
 17
 18
 19
 20
 21
 22
 23
 24
 25
 26
 27
 28
 29
 30
 31
 32
 33
 34
 35
 36
 37
 38
 39
 40
 41
 42
 43
 44
 45
 46
 47
 48
 49
 50
 51
 52
 53
 54
 55
 56
 57
 58
 59
 60
 61
 62
 63
 64
 65
 66
 67
 68
 69
 70
 71
 72
 73
 74
 75
 76
 77
 78
 79
 80
 81
 82
 83
 84
 85
 86
 87
 88
 89
 90
 91
 92
 93
 94
 95
 96
 97
 98
 99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
130
131
132
133
134
135
136
137
138
139
140
141
142
143
144
145
146
147
148
149
150
151
152
153
154
155
156
157
158
159
160
161
162
163
164
165
166
167
168
169
170
171
172
173
174
175
176
177
178
179
180
181
182
183
184
185
186
187
188
189
190
191
192
193
194
195
196
197
198
199
200
201
202
203
204
205
206
207
208
209
210
211
212
213
214
215
216
217
218
219
220
221
222
import sys
import time
from grove.gpio import GPIO


charmap = {
    '0': 0x3f,
    '1': 0x06,
    '2': 0x5b,
    '3': 0x4f,
    '4': 0x66,
    '5': 0x6d,
    '6': 0x7d,
    '7': 0x07,
    '8': 0x7f,
    '9': 0x6f,
    'A': 0x77,
    'B': 0x7f,
    'b': 0x7C,
    'C': 0x39,
    'c': 0x58,
    'D': 0x3f,
    'd': 0x5E,
    'E': 0x79,
    'F': 0x71,
    'G': 0x7d,
    'H': 0x76,
    'h': 0x74,
    'I': 0x06,
    'J': 0x1f,
    'K': 0x76,
    'L': 0x38,
    'l': 0x06,
    'n': 0x54,
    'O': 0x3f,
    'o': 0x5c,
    'P': 0x73,
    'r': 0x50,
    'S': 0x6d,
    'U': 0x3e,
    'V': 0x3e,
    'Y': 0x66,
    'Z': 0x5b,
    '-': 0x40,
    '_': 0x08,
    ' ': 0x00
}

ADDR_AUTO = 0x40
ADDR_FIXED = 0x44
STARTADDR = 0xC0
BRIGHT_DARKEST = 0
BRIGHT_DEFAULT = 2
BRIGHT_HIGHEST = 7


class Grove4DigitDisplay(object):
    colon_index = 1

    def __init__(self, clk, dio, brightness=BRIGHT_DEFAULT):
        self.brightness = brightness

        self.clk = GPIO(clk, direction=GPIO.OUT)
        self.dio = GPIO(dio, direction=GPIO.OUT)
        self.data = [0] * 4
        self.show_colon = False

    def clear(self):
        self.show_colon = False
        self.data = [0] * 4
        self._show()

    def show(self, data):
        if type(data) is str:
            for i, c in enumerate(data):
                if c in charmap:
                    self.data[i] = charmap[c]
                else:
                    self.data[i] = 0
                if i == self.colon_index and self.show_colon:
                    self.data[i] |= 0x80
                if i == 3:
                    break
        elif type(data) is int:
            self.data = [0, 0, 0, charmap['0']]
            if data < 0:
                negative = True
                data = -data
            else:
                negative = False
            index = 3
            while data != 0:
                self.data[index] = charmap[str(data % 10)]
                index -= 1
                if index < 0:
                    break
                data = int(data / 10)

            if negative:
                if index >= 0:
                    self.data[index] = charmap['-']
                else:
                    self.data = charmap['_'] + [charmap['9']] * 3
        else:
            raise ValueError('Not support {}'.format(type(data)))
        self._show()

    def _show(self):
        with self:
            self._transfer(ADDR_AUTO)

        with self:
            self._transfer(STARTADDR)
            for i in range(4):
                self._transfer(self.data[i])

        with self:
            self._transfer(0x88 + self.brightness)

    def update(self, index, value):
        if index < 0 or index > 4:
            return

        if value in charmap:
            self.data[index] = charmap[value]
        else:
            self.data[index] = 0

        if index == self.colon_index and self.show_colon:
            self.data[index] |= 0x80

        with self:
            self._transfer(ADDR_FIXED)

        with self:
            self._transfer(STARTADDR | index)
            self._transfer(self.data[index])

        with self:
            self._transfer(0x88 + self.brightness)


    def set_brightness(self, brightness):
        if brightness > 7:
            brightness = 7

        self.brightness = brightness
        self._show()

    def set_colon(self, enable):
        self.show_colon = enable
        if self.show_colon:
            self.data[self.colon_index] |= 0x80
        else:
            self.data[self.colon_index] &= 0x7F
        self._show()

    def _transfer(self, data):
        for _ in range(8):
            self.clk.write(0)
            if data & 0x01:
                self.dio.write(1)
            else:
                self.dio.write(0)
            data >>= 1
            time.sleep(0.000001)
            self.clk.write(1)
            time.sleep(0.000001)

        self.clk.write(0)
        self.dio.write(1)
        self.clk.write(1)
        self.dio.dir(GPIO.IN)

        while self.dio.read():
            time.sleep(0.001)
            if self.dio.read():
                self.dio.dir(GPIO.OUT)
                self.dio.write(0)
                self.dio.dir(GPIO.IN)
        self.dio.dir(GPIO.OUT)

    def _start(self):
        self.clk.write(1)
        self.dio.write(1)
        self.dio.write(0)
        self.clk.write(0)

    def _stop(self):
        self.clk.write(0)
        self.dio.write(0)
        self.clk.write(1)
        self.dio.write(1)

    def __enter__(self):
        self._start()

    def __exit__(self, exc_type, exc_val, exc_tb):
        self._stop()


Grove = Grove4DigitDisplay


def main():
    if len(sys.argv) < 3:
        print('Usage: {} clk dio'.format(sys.argv[0]))
        sys.exit(1)

    display = Grove4DigitDisplay(int(sys.argv[1]), int(sys.argv[2]))

    count = 0
    while True:
        t = time.strftime("%H%M", time.localtime(time.time()))
        display.show(t)
        display.set_colon(count & 1)
        count += 1
        time.sleep(1)


if __name__ == '__main__':
    main()

Success

If everything goes well, the 4-digit display will show the current time.

You can quit this program by simply press Ctrl+C.

Play With Raspberry Pi (with GrovePi_Plus)

Hardware

  • Step 1. Prepare the below stuffs:
Raspberry pi GrovePi_Plus Grove-4-Digit Display
enter image description here enter image description here enter image description here
Get One Now Get One Now Get One Now
  • Step 2. Plug the GrovePi_Plus into Raspberry.
  • Step 3. Connect Grove-4-Digit Display to D5 port of GrovePi_Plus.
  • Step 4. Connect the Raspberry to PC through USB cable.

Software

  • Step 1. Follow Setting Software to configure the development environment.
  • Step 2. Git clone the Github repository.
1
2
cd ~
git clone https://github.com/DexterInd/GrovePi.git
  • Step 3. Excute below commands to monitor the loudness.
1
2
cd ~/GrovePi/Software/Python
python grove_4_digit_display.py

Here is the grove_4_digit_display.py code.

  1
  2
  3
  4
  5
  6
  7
  8
  9
 10
 11
 12
 13
 14
 15
 16
 17
 18
 19
 20
 21
 22
 23
 24
 25
 26
 27
 28
 29
 30
 31
 32
 33
 34
 35
 36
 37
 38
 39
 40
 41
 42
 43
 44
 45
 46
 47
 48
 49
 50
 51
 52
 53
 54
 55
 56
 57
 58
 59
 60
 61
 62
 63
 64
 65
 66
 67
 68
 69
 70
 71
 72
 73
 74
 75
 76
 77
 78
 79
 80
 81
 82
 83
 84
 85
 86
 87
 88
 89
 90
 91
 92
 93
 94
 95
 96
 97
 98
 99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
# NOTE: 4x red 7 segment display with colon and 8 luminance levels, but no decimal points

import time
import grovepi

# Connect the Grove 4 Digit Display to digital port D5
# CLK,DIO,VCC,GND
display = 5
grovepi.pinMode(display,"OUTPUT")

# If you have an analog sensor connect it to A0 so you can monitor it below
sensor = 0
grovepi.pinMode(sensor,"INPUT")

time.sleep(.5)

# 4 Digit Display methods
# grovepi.fourDigit_init(pin)
# grovepi.fourDigit_number(pin,value,leading_zero)
# grovepi.fourDigit_brightness(pin,brightness)
# grovepi.fourDigit_digit(pin,segment,value)
# grovepi.fourDigit_segment(pin,segment,leds)
# grovepi.fourDigit_score(pin,left,right)
# grovepi.fourDigit_monitor(pin,analog,duration)
# grovepi.fourDigit_on(pin)
# grovepi.fourDigit_off(pin)

while True:
    try:
        print ("Test 1) Initialise")
        grovepi.fourDigit_init(display)
        time.sleep(.5)

        print ("Test 2) Set brightness")
        for i in range(0,8):
            grovepi.fourDigit_brightness(display,i)
            time.sleep(.2)
        time.sleep(.3)

        # set to lowest brightness level
        grovepi.fourDigit_brightness(display,0)
        time.sleep(.5)

        print ("Test 3) Set number without leading zeros")
        leading_zero = 0
        grovepi.fourDigit_number(display,1,leading_zero)
        time.sleep(.5)
        grovepi.fourDigit_number(display,12,leading_zero)
        time.sleep(.5)
        grovepi.fourDigit_number(display,123,leading_zero)
        time.sleep(.5)
        grovepi.fourDigit_number(display,1234,leading_zero)
        time.sleep(.5)

        print ("Test 4) Set number with leading zeros")
        leading_zero = 1
        grovepi.fourDigit_number(display,5,leading_zero)
        time.sleep(.5)
        grovepi.fourDigit_number(display,56,leading_zero)
        time.sleep(.5)
        grovepi.fourDigit_number(display,567,leading_zero)
        time.sleep(.5)
        grovepi.fourDigit_number(display,5678,leading_zero)
        time.sleep(.5)

        print ("Test 5) Set individual digit")
        grovepi.fourDigit_digit(display,0,2)
        grovepi.fourDigit_digit(display,1,6)
        grovepi.fourDigit_digit(display,2,9)
        grovepi.fourDigit_digit(display,3,15) # 15 = F
        time.sleep(.5)

        print ("Test 6) Set individual segment")
        grovepi.fourDigit_segment(display,0,118) # 118 = H
        grovepi.fourDigit_segment(display,1,121) # 121 = E
        grovepi.fourDigit_segment(display,2,118) # 118 = H
        grovepi.fourDigit_segment(display,3,121) # 121 = E
        time.sleep(.5)

        grovepi.fourDigit_segment(display,0,57) # 57 = C
        grovepi.fourDigit_segment(display,1,63) # 63 = O
        grovepi.fourDigit_segment(display,2,63) # 63 = O
        grovepi.fourDigit_segment(display,3,56) # 56 = L
        time.sleep(.5)

        print ("Test 7) Set score")
        grovepi.fourDigit_score(display,0,0)
        time.sleep(.2)
        grovepi.fourDigit_score(display,1,0)
        time.sleep(.2)
        grovepi.fourDigit_score(display,1,1)
        time.sleep(.2)
        grovepi.fourDigit_score(display,1,2)
        time.sleep(.2)
        grovepi.fourDigit_score(display,1,3)
        time.sleep(.2)
        grovepi.fourDigit_score(display,1,4)
        time.sleep(.2)
        grovepi.fourDigit_score(display,1,5)
        time.sleep(.5)

        print ("Test 8) Set time")
        grovepi.fourDigit_score(display,12,59)
        time.sleep(.5)

        print ("Test 9) Monitor analog pin")
        seconds = 10
        grovepi.fourDigit_monitor(display,sensor,seconds)
        time.sleep(.5)

        print ("Test 10) Switch all on")
        grovepi.fourDigit_on(display)
        time.sleep(.5)

        print ("Test 11) Switch all off")
        grovepi.fourDigit_off(display)
        time.sleep(.5)

    except KeyboardInterrupt:
        grovepi.fourDigit_off(display)
        break
    except IOError:
        print ("Error")
  • Step 4. We will see the Grove-4-Digit Display as below.
 1
 2
 3
 4
 5
 6
 7
 8
 9
10
11
12
pi@raspberrypi:~/GrovePi/Software/Python $ python grove_4_digit_display.py 
Test 1) Initialise
Test 2) Set brightness
Test 3) Set number without leading zeros
Test 4) Set number with leading zeros
Test 5) Set individual digit
Test 6) Set individual segment
Test 7) Set score
Test 8) Set time
Test 9) Monitor analog pin
Test 10) Switch all on
Test 11) Switch all off

Play with TI LaunchPad

Displaying the Numbers (4-Digital-Display)

This example demonstrates how to display some digital numbers using a Grove-4-Digital Display.

 1
 2
 3
 4
 5
 6
 7
 8
 9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
/*
 * TM1637.cpp
 * A library for the 4 digit display
 */
#include "TM1637.h"
#define CLK 39 //pins definitions for TM1637 and can be changed to other ports
#define DIO 38
TM1637 tm1637(CLK,DIO);
void setup()
{
    tm1637.init();
    tm1637.set(BRIGHT_TYPICAL);//BRIGHT_TYPICAL = 2,BRIGHT_DARKEST = 0,BRIGHTEST = 7;
}
void loop()
{
    int8_t NumTab[] = {0,1,2,3,4,5,6,7,8,9,10,11,12,13,14,15};//0~9,A,b,C,d,E,F
    int8_t ListDisp[4];
    unsigned char i = 0;
    unsigned char count = 0;
    delay(150);
    while(1)
    {
        i = count;
        count ++;
        if(count == sizeof(NumTab)) count = 0;
        for(unsigned char BitSelect = 0;BitSelect < 4;BitSelect ++)
        {
            ListDisp[BitSelect] = NumTab[i];
            i ++;
            if(i == sizeof(NumTab)) i = 0;
        }
        tm1637.display(0,ListDisp[0]);
        tm1637.display(1,ListDisp[1]);
        tm1637.display(2,ListDisp[2]);
        tm1637.display(3,ListDisp[3]);
        delay(300);
    }
}

Resources

Inspired by OVERWATCH, we have made a very cool Wooden Laser Gun toy for fun these day!

The Wooden Laser Gun and the Gun Target are all based on an Arduino board called Seeeduino Lotus. The laser emitter on the Laser Gun is controlled to fire laser pulse to "activate" the Gun Target. And there are 3 light sensors on the Gun Target to detect the laser pulse. It seems very simple right? If you are interested in our project, please make one for yourself or your child! It's worth to spend one day DIY it as a Xmas present.

Projects

MSP430 Alarm Clock with Grove Modules: Create your own alarm clock using the MSP430F5529 LaunchPad and the SeeedStudio Grove Modules.

Clock - Grove 4-digit Display Using Photon: Your first clock with 4 components, based on Grove and TM1637

Tech Support

Please submit any technical issue into our forum.